This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Boot TDA with no Gel Scripts

Part Number: TDA4VM

Hello, 

I want to boot the TDA on CCS without the use gel scripts. This is so I can replicate this on custom boards (with customer's boot loader) and bring the TDA to a state where I can connect and load binaries with through an emulator.

Set-up

- No boot mode 

- on board XDS110 and using CCS IDE 

- Using the J721e EVM and SBL from the PDK 

What Binaries or process  (if any) do I need to run on the DMSC to run the SBL on the R5F?