This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Requesting the BSDL file for the AMC package. The BSDL currently available in the downloads section is for the ALW package only.
Hello Stan DeVault
Thank you for the query.
Let me check the availability or planned schedule and update you.
Can you help us understand the use case.
Regards,
Sreenivasa
The use case is to be able to perform boundary scan test (aka JTAG test) with the component in circuit. To do this I need the BSDL (Boundary Scan Description Language) file. Every chip equipped with JTAG test capability (IEEE 1149.1 capable) will have a BSDL file describing its internal boundary scan circuitry/structure.
Hello Stan DeVault
Thank you for the inputs.
Can you please help me confirm if you are working with TI sales/support. As i understand internally we will need to have an NDA in place and additionally need to enable access permission.
Regards,
Sreenivasa
Hello Stan DeVault
I will close the thread since i have not heard from you.
Regards,
Sreenivasa