Part Number: TDA4VM
TDA4VM
boot mode : SBL
About one boot failure in a hundred times


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can you please share more details on the issue?
Which SDK version you are using and what is the failure you are seeing. Can you please share the SBL logs?
Regards,
Parth
/*****************************************************************/ 板卡启动成功时的MCU1_0的log SBL Revision: 01.00.10.00 (Feb 19 2023 - 20:39:49) SBL_ReadSysfwImage in [330] Getting eMMC parameters eMMC: BlockCount = 0x3a40000 eMMC: part_support = 7,part_config =2 TIFS ver: 21.1.1--v2021.01a (Terrific Lla SBL_MMCBootImage in [520] Getting eMMC parameters eMMC: BlockCount = 0x3a40000 eMMC: part_support = 7,part_config =2 [ads] start mcu0_0 version ++++++A2+++++++ IPC Profile App: IPC Profile App: IPC Profile Application - STARTS !!! [ads] start mcu0_0 --> 1 [ads] start mcu0_0 --> 2 [ads] start mcu0_0 --> 3 create IpcSpiMasterApp_TaskFxn IPC_SPI Master Demo App:Transmitted Message of size 4 bytes, 1000 times in 0 usecs IPC_SPI Master Demo App:Average of 0.00 usecs per transmit IPC Profile App: CDD IPC MCAL Version Info cs per transmit IPC_SPI Master Demo App:Measured Load: Total CPU: 100.000000%, HWI: 0.000000%, SWI:0.000000% TSK: 0.000000% IPC Profile App: --------------------- otal CPU: 100.000000%, HWI: 0.000000%, SWI:0.000000% TSK: 0.000000% IPC_SPI Master Demo App:SPI Test Passed!!! IPC Profile App: Vendor ID : 44 [ads] start gpt_test [PC Profile App: ModuGPT_APP: Building Interrupt List !!! GPC Profile App: SW Major Version GPT_APP: Variant - Post Build being used !!! GPC Profile App: SW Minor Version : 3 ! GPT_APP: Interrupt List Completed !!! GPC Profile App: SW Patch Version GPT_APP: Variant - Post Build being used !!! G _APP: Variant - Post Build being used !!! PGPT_APP GPT MCAL Version Info GPT_APP GPT MCAL Version Info GPT_APP--------------------- GPT_APP Vendor ID : 44 GPT_APP Module ID : 100 GPT_APP SW Major Version : 1 GPT_APP SW Minor Version : 3 GPT_APP SW Patch Version : 2 ------------------------------------------ GPT_APP: Running GPT Test for channel 6 ------------------------------------------ GPT_APP: Enabled notification for channel [6] is GPT_CH_MODE_CONTINUOUS GPT_APP: Enabled notification for channel [6] GPT_APP: Started Timer Channel [6] GPT_APP: Elapsed Time Value = a8bce GPT_APP: GPT Stack Usage 8192 bytes GPT_APP: GPT Stack/section corruption!!! [ads] start while(1) PMIC App:0X31 WR = 0x0,ret=0 PMIC App:0X32 WR = 0x0,ret=0 PMIC App:0X09 RD0 = 0xff,ret=0 PMIC App:0X09 WR = 0xbf,ret=0 PMIC App:0X09 RD1 = 0xbf,ret=0 IPC Profile App: Sync with MASTER1 CPU done... IPC-Service: INFO: Register service '[ID: 0]: com.mcu10.info' finished! IPC Profile App: Announce Service: ti.ipc4.mcu_pmic IPC Profile App: IPC Profile App: Starting MCU2_1 to MCU1_0 IPC receive task IPC Profile App: failed to receive from comm[2] IPC Profile App: MCU1_0 INFO: go to sleep /*****************************************************************/ 板卡启动失败时的MCU1_0的log SBL Revision: 01.00.10.00 (Feb 19 2023 - 20:39:49) SBL_ReadSysfwImage in [330] Getting eMMC parameters eMMC: BlockCount = 0x3a40000 eMMC: part_support = 7,part_config =2 TIFS ver: 21.1.1--v2021.01a (Terrific Lla SBL_MMCBootImage in [520] Getting eMMC parameters eMMC: BlockCount = 0x3a40000 eMMC: part_support = 7,part_config =2 [ads] start mcu0_0 version ++++++A2+++++++ IPC Profile App: IPC Profile App: IPC Profile Application - STARTS !!! [ads] start mcu0_0 --> 1 [ads] start mcu0_0 --> 2 [ads] start mcu0_0 --> 3 create IpcSpiMasterApp_TaskFxn
You can refer to the link below for more detailed information
(+) TDA4VM: uboot fails to start - Processors forum - Processors - TI E2E support forums
Hi,
You can refer to the link below for more detailed information
(+) TDA4VM: uboot fails to start - Processors forum - Processors - TI E2E support forums
Is this the same issue being discussed in the thread you mentioned above? If yes, let's continue the discussion on that thread itself so that it is easy to track.
Regards,
Parth
yes, That thread started with the A72 bootloader, this thread started with the MCU1_0 bootloader, and now I've synced this post to the other one
Okay, closing this one. Please continue the discussion on the other thread.
Regards,
Parth