Part Number: PROCESSOR-SDK-C6748
I know this hardware/software is not supported anymore, but this may be a general CCS question.
How can I specify the program entry point? In other projects, I can set this in the linker.cmd file.
But in the LED example program, the linker.cmd file is generated and I can't figure out where the generated file is getting it's data.
Background:
I'm working on booting the C6748 DSP from an SD card.
I can flash the bootloader to the SD card and I get a UART response indicating that the app program will be loaded.
However, it runs into an error.
I suspect that the problem is the requirement for the program entry point as specified in the docs:

I have the LED example program loaded, but I can't find where the entry point is 1k aligned.
Where is that set?