Hi Experts
Our customer is developing minor-change model at this time, and they updated SDK (ver. 4.2.0.9 )to the latest Linux SDK version (ver. 08.02.00.24), as well. As the result, customer is encountering missing-commutation issue now. Customer is using omap-serial.c file, when they replaced omap-serial.c (ver. 08.02.00.24) with omap-serial.c (ver. 4.2.0.9 ), it seemed this issue was resolved.
Since I found out there is similar issue report thread in E2E forum, I share this URL with customer. After that, I receive the following questions.
- Customer understood omap-serial.c has not been maintained for a long time, but, customer is asking TI if it is possible to use omap-serial.c (ver. 4.2.0.9 ). I believe it is difficult to answer it.. however, can I have your expert’s advice/comments on them, please?
- Regarding 8250-omap.c, customer understand it is a new UART driver… customer wants to do RS-485 commutation. In this case, customer is considering that they need to control RTS/CTS. They mean, they need to set “High” to RTS when customer wants to transfer data, and then, they need to set “Low” to RTS when customer wants to receive data. but, it seems it is impossible to control RTS signal. so, customer is asking if there is any solution for this behavior.
can I have your expert’s advice/comments on them, please?
Best regards,
Miyazaki