Hi,
We decided to go with 2Gb (4 die part) from Micron and the part# is MT35XU02GCBA1G12-0AUT. I have the below questions.
- From our understanding, there will not be any timing information, other Electrical characteristics and software requirements changes, if Single die /quad die devices operating in SDR mode.
- As per our timing analysis, the maximum frequency we can achieve as 100MHz for read and 125MHz for write to meet the set up and hold margin.
Read Command
- .

Write Command

- Does TDA4VM has the below feature for SPI. it will help to improve the set-up requirement.

Can you pls confirm that the OSPI implementation in SDK is internal loop back or external loop back?
What is the driver for OSPI, Internal loopback VS. External loopback? How it is used TI EVM