Dear Sir
I find the red line in a image has aliasing effect after converting RGBX to YUV422 through M2M.
This aliasing effect is increased significantly . Is there any way to optimize the aliasing effect?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir
I find the red line in a image has aliasing effect after converting RGBX to YUV422 through M2M.
This aliasing effect is increased significantly . Is there any way to optimize the aliasing effect?
Thanks.
Hi Cao,
Can you explain bit about the attached images? Is the left side image with the old coefficients and right side image with the latest coefficients? I see good improvement on the right side image. The red line has very less artifacts.. So it is improved..
Can you now copy these coefficients to all phases?
static const CSL_DssWbPipeScalerCoeff gScalerCoefDownScaleM14[ CSL_DSS_WB_PIPE_NUM_SCALER_PHASES] = { { 12, 128, 232}, { 12, 128, 232}, { 12, 128, 232}, { 12, 128, 232}, { 12, 128, 232}, { 12, 128, 232}, { 12, 128, 232}, { 12, 128, 232}, { 12, 128, 232}, { 12, 128, 232}, { 12, 128, 232}, { 12, 128, 232}, { 12, 128, 232}, { 12, 128, 232}, { 12, 128, 232}, { 12, 128, 232}, };
Regards,
Brijesh
HI,Brijesh
The left side image is the RGB image and right side image is the UYVY image converted from RGB image. The red line has aliasing effect after converting as before.
Hi,
Did you try the experiment that i have suggested? If not, can you please try and check the output?
Regards,
Brijesh
Hi,Brijesh
I have tried what you have suggested. The code diff and registers are below
diff --git a/pdk_jacinto/packages/ti/csl/src/ip/dss/V4/priv/csl_dssWbPipe.c b/pdk_jacinto/packages/ti/csl/src/ip/dss/V4/priv/csl_dssWbPipe.c
index a34ea0676c..8170ff8153 100755
--- a/pdk_jacinto/packages/ti/csl/src/ip/dss/V4/priv/csl_dssWbPipe.c
+++ b/pdk_jacinto/packages/ti/csl/src/ip/dss/V4/priv/csl_dssWbPipe.c
@@ -260,22 +260,22 @@ static const CSL_DssWbPipeScalerCoeff gScalerCoefDownScaleM10[
static const CSL_DssWbPipeScalerCoeff gScalerCoefDownScaleM14[
CSL_DSS_WB_PIPE_NUM_SCALER_PHASES] =
{
- {- 8, 120, 288},
- {- 6, 134, 286},
- {- 4, 148, 284},
- {- 2, 164, 280},
- { 0, 180, 276},
- { 6, 194, 266},
- { 12, 208, 256},
- { 18, 220, 244},
- { 0, 24, 232},
- {- 2, 32, 244},
- {- 4, 40, 256},
- {- 6, 52, 266},
- {- 8, 64, 276},
- {- 8, 78, 280},
- {- 8, 92, 284},
- {- 8, 106, 286},
+ { 12, 128, 232},
+ { 12, 128, 232},
+ { 12, 128, 232},
+ { 12, 128, 232},
+ { 12, 128, 232},
+ { 12, 128, 232},
+ { 12, 128, 232},
+ { 12, 128, 232},
+ { 12, 128, 232},
+ { 12, 128, 232},
+ { 12, 128, 232},
+ { 12, 128, 232},
+ { 12, 128, 232},
+ { 12, 128, 232},
+ { 12, 128, 232},
+ { 12, 128, 232},
};
static const CSL_DssWbPipeScalerCoeff gScalerCoefDownScaleM19[
@@ -1457,10 +1457,10 @@ static void CSL_dssWbPipeGetChromaRes(uint32_t dataFormat,
{
if (TRUE == Fvid2_isDataFmtYuv422(dataFormat))
{
- *chromaWidth = width;
- *chromaHeight = height / 2U;
+ *chromaWidth = width / 2U;
+ *chromaHeight = height;
}
- if (TRUE == Fvid2_isDataFmtYuv420(dataFormat))
+ else if (TRUE == Fvid2_isDataFmtYuv420(dataFormat))
{
*chromaWidth = width / 2U;
*chromaHeight = height / 2U;
@@ -1476,6 +1476,7 @@ static void CSL_dssWbPipeGetChromaRes(uint32_t dataFormat,
*chromaWidth = 0U;
*chromaHeight = 0U;
}
+
}
static void CSL_dssWbPipeSetScalerCoeff(
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0000 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0008 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0010 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0018 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0020 = 0x2818fe
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0028 = 0xb8386000
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0030 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0038 = 0x1000
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0040 = 0x96004d
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0048 = 0x7eb0792
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0050 = 0x83
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0058 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0060 = 0x400000
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0068 = 0x200000
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0070 = 0x200
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0078 = 0x1c0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0080 = 0x180
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0088 = 0x140
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0090 = 0xe8
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0098 = 0xe8
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af00a0 = 0xe8
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af00a8 = 0xe8
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af00b0 = 0xe8
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af00b8 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af00c0 = 0x10000
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af00c8 = 0x20000
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af00d0 = 0x30000
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af00d8 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af00e0 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af00e8 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af00f0 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af00f8 = 0xc20000
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0100 = 0xc20000
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0108 = 0xc20000
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0110 = 0xc20000
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0118 = 0xc20000
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0120 = 0xc20000
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0128 = 0xc20000
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0130 = 0xc20000
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0138 = 0x200
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0140 = 0x1c0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0148 = 0x180
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0150 = 0x140
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0158 = 0x200
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0160 = 0x1c0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0168 = 0x180
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0170 = 0x140
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0178 = 0x100
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0180 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0188 = 0x10000
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0190 = 0x20000
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0198 = 0x30000
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af01a0 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af01a8 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af01b0 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af01b8 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af01c0 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af01c8 = 0x10000
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af01d0 = 0x20000
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af01d8 = 0x30000
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af01e0 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af01e8 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af01f0 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af01f8 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0200 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0208 = 0x2cf04ff
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0210 = 0x2cf04ff
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0218 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0220 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0228 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0230 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0238 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0240 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0248 = 0x0
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Mar 21 18:45:58 UTC 2022) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
Value at addr 0x4af0020 = 0x2818fe
There is no improvement about aliasing effect. The autovideo_AVCRGB_00.yuv in the zip is the RGB image and the autovideo_csitx_1280x720_image00.yuv is the UYVY image converted from RGB image. The red line has aliasing effect .
Pls check it .
Regards
Hi,
Any further update on this ticket? Let us know if we can close it otherwise.
Regards,
Brijesh