Part Number: AM623
Other Parts Discussed in Thread: TSC2007
Hi,
SDK:08.03.00.19
Customer has disabled the gpu according to the instructions below figure, but the file system cannot boot up at present. How can the file system be modified to adapt to 6231?

The error as follows:
[ 14.803125] max_p2p_conn = 8, max_sta_conn = 8 Starting Load/Save RF Kill Switch Status...
[ 14.849629] wlan: version = SD8987---16.92.10.p208-MXM5X16210-GPL-(FP92)
[ 14.859212] wlan: Driver loaded successfully
[ OK ] Started Load/Save RF Kill Switch Status.
[ *** ] A start job is running for udev Wai…ice Initialization (30s / 3min 2s)