This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM623: eMMC Boot Configuration - Raw Mode vs Filesystem Mode Setup

Part Number: AM623

Tool/software:

Hi,

I would like to understand the difference between raw mode and filesystem (FS) mode in eMMC boot. How can I set up both raw mode and filesystem mode for booting from eMMC at the U-Boot and Linux levels? Additionally, what are the exact steps to configure raw mode and filesystem mode in the User Data Area (UDA)?

Current eMMC Boot Configuration I'm using:

Primary Boot: eMMC UDA in Filesystem mode
Pins B7-B0: 01000011
Backup Boot: Ethernet RGMII
Pins B15-B8: 00010000

Thanks,
Murali Vikas