This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6412: AM6412 Pinout creation

Part Number: AM6412
Other Parts Discussed in Thread: SYSCONFIG

Hello,

Back in my initial thread relative to the pin-out of the AM6412 CPU, I did ask for guidance if the following steps are the correct way to go...

1) Using the information presented in the latest datasheet. Table 6_1 , containing generic names

AND

2) Using the csv file from the sysconfig tool

I did have a reply (show below)

/////

Alex

A combination of both the datasheet and the SysConfig pinmux csv file would currently be the best way to to provide the necessary custom data for the schematic symbol.   

I think this could be a good enhancement to the tool, add an output file that could be used as a source for symbol generation. For this process, you would need ball name, signal name, ball number, direction.  Do you need any other data?

////

I want to clarify if the usage of Table 6.1 from the datasheet , is the correct way to go  schematic symbol creation.

I did spot some discrepancies between this table 6.1  (where there is no reference of the dual use of ADC In signals [can be GPIs] ) and table 6.2 (ADC0 Signal descriptions : There is reference that some signals can be used as GP inputs only)..

Please explain further as this is a very critical step for us.

Thanks

Alex