Other Parts Discussed in Thread: SYSCONFIG
Hello,
Back in my initial thread relative to the pin-out of the AM6412 CPU, I did ask for guidance if the following steps are the correct way to go...
1) Using the information presented in the latest datasheet. Table 6_1 , containing generic names
AND
2) Using the csv file from the sysconfig tool
I did have a reply (show below)
/////
Alex
A combination of both the datasheet and the SysConfig pinmux csv file would currently be the best way to to provide the necessary custom data for the schematic symbol.
I think this could be a good enhancement to the tool, add an output file that could be used as a source for symbol generation. For this process, you would need ball name, signal name, ball number, direction. Do you need any other data?
////
I want to clarify if the usage of Table 6.1 from the datasheet , is the correct way to go schematic symbol creation.
I did spot some discrepancies between this table 6.1 (where there is no reference of the dual use of ADC In signals [can be GPIs] ) and table 6.2 (ADC0 Signal descriptions : There is reference that some signals can be used as GP inputs only)..
Please explain further as this is a very critical step for us.
Thanks
Alex