This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6412: AM6412 HSR PRP support

Part Number: AM6412

Hi,

For our new project to be used in energy management  we are looking for a processor(replacement for Omap L138) in TI Arm microprocessors portfolio.

The most critical requirements are;

1. Dual core processor. Arm for Linux OS plus a second core for processing voltage/current values read from an 8-channel external ADC.

2. 2 ethernet port and HSR/PRP.(Gigabit ethernet support is not mandatory) 

3. Graphical LCD interface.(Touch screen will not be used)

Based on the  above requirements AM6412 seems a good candidate except lack of a display interface. 

For the LCD part we are planning to implement a graphical LCD driver in  kernel level.  But I need to clarify the following points.

1. Does the current SDK support  HSR/PRP protocol on PRU-ICSS module offloading A53 core.

2. Is it possible to implement a bare metal application on R5 core to process data received from external ADCs via SPI interface.

3. Is it possible develop/debug bare metal application on R5 core without intervention of A53 core.

Best regards.