Hi Ti:
I have 2 J7 EVM and both boot from SD card. However,when I connect same camera to EVM on CSI port one EVM(1#) can get data from camera but the other EVM(2#) can not. Whatever use linux SDK or RTOS SDK. The situation is same using CSI0 or CSI1. So what could be wrong with this?By the way, the register 0x04504048 is switch between 0x00333307 and 0x00222207 in EVM(2#).Thanks.