Part Number: TDA4VM
Hi guys,
I am trying to run an econ camera module using TDA4VM SoC.
This is the camera modules link for ref:
I have followed the manual but I can't make the board recognize the sensor.
I have double-checked that name_overlay is defined correctly in eEnv.txt
psdk_setup_file=.psdk_setup
check_psdk_setup=load mmc 1:1 ${loadaddr} ${psdk_setup_file}
# Reset to the default environment
do_psdk_setup=env default -f -a; saveenv
# If not previously configured, then configure the environment and indicate this by writing a file
uenvcmd=if run check_psdk_setup; then echo "Already setup."; else run do_psdk_setup; mw.b ${loadaddr} 0 1; fatwrite mmc 1:1 ${loadaddr} .psdk_setup 1; reset; fi
dorprocboot=1
name_overlays=k3-j721e-edgeai-apps.dtbo k3-j721e-sk-NeduCAM25-2cam.dtbo
when I run init_script.sh it returns no value (A USB cam is recognizable).
v4l2 list devices for ref.
root@tda4vm-sk:/run/media/mmcblk0p1# v4l2-ctl --list-devices
TI-CSI2RX (platform:4500000.ticsi2rx):
/dev/media0
TI-CSI2RX (platform:4510000.ticsi2rx):
/dev/media1
vxd-dec (platform:vxd-dec):
/dev/video1
vxe-enc (platform:vxe-enc):
/dev/video0
root@tda4vm-sk:/run/media/mmcblk0p1# [ 656.504821] Checking for MMU outstanding requests failed!
[ 656.610713] Checking for MMU outstanding requests failed!
dmesg for ref:
dmesg
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x411fd080]
[ 0.000000] Linux version 5.10.120-00009-gbe27a7188056 (dharani@dharani-LP) (aarch64-none-linux-gnu-gcc (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 9.2.1 20191025, GNU ld (GNU Toolc2
[ 0.000000] Machine model: Texas Instruments J721E SK
[ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
[ 0.000000] printk: bootconsole [ns16550a0] enabled
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a0000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a0100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a1000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a1100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a2000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 31 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a2100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a4000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, size 31 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a4100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a6000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a6000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a6100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a6100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a7000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a7000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a7100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a7100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a8000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c66-dma-memory@a8000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a8100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c66-memory@a8100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a9000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c66-dma-memory@a9000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a9100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c66-memory@a9100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000aa000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c71-dma-memory@aa000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000aa100000, size 79 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c71-memory@aa100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000b2000000, size 96 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-dma-memory@b2000000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: initialized node vision_apps_shared-memories, compatible id dma-heap-carveout
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000d8000000, size 192 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-core-heap-memory-lo@d8000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000e4000000, size 8 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-virtual-eth-queues@e4000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000e4800000, size 24 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-virtual-eth-buffers@e4800000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000880000000, size 624 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-core-heap-memory-hi@880000000, compatible id shared-dma-pool
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal [mem 0x0000000100000000-0x00000008ffffffff]
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x000000009e7fffff]
[ 0.000000] node 0: [mem 0x000000009e800000-0x00000000aeffffff]
[ 0.000000] node 0: [mem 0x00000000af000000-0x00000000afffffff]
[ 0.000000] node 0: [mem 0x00000000b0000000-0x00000000b7ffffff]
[ 0.000000] node 0: [mem 0x00000000b8000000-0x00000000d7ffffff]
[ 0.000000] node 0: [mem 0x00000000d8000000-0x00000000e5ffffff]
[ 0.000000] node 0: [mem 0x00000000e6000000-0x00000000ffffffff]
[ 0.000000] node 0: [mem 0x0000000880000000-0x00000008a6ffffff]
[ 0.000000] node 0: [mem 0x00000008a7000000-0x00000008ffffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000008ffffffff]
[ 0.000000] On node 0 totalpages: 1048576
[ 0.000000] DMA zone: 8192 pages used for memmap
[ 0.000000] DMA zone: 0 pages reserved
[ 0.000000] DMA zone: 524288 pages, LIFO batch:63
[ 0.000000] Normal zone: 8192 pages used for memmap
[ 0.000000] Normal zone: 524288 pages, LIFO batch:63
[ 0.000000] cma: Reserved 400 MiB at 0x00000000e7000000
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.2
[ 0.000000] percpu: Embedded 22 pages/cpu s50008 r8192 d31912 u90112
[ 0.000000] pcpu-alloc: s50008 r8192 d31912 u90112 alloc=22*4096
[ 0.000000] pcpu-alloc: [0] 0 [0] 1
[ 0.000000] Detected PIPT I-cache on CPU0
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] CPU features: detected: EL2 vector hardening
[ 0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
[ 0.000000] CPU features: detected: Spectre-BHB
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1032192
[ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),256k(ospi.env),1m(ospi.sysfw),256k(ospi.et
[ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] software IO TLB: mapped [mem 0x000000009a800000-0x000000009e800000] (64MB)
[ 0.000000] Memory: 1828020K/4194304K available (10880K kernel code, 1126K rwdata, 4188K rodata, 1792K init, 431K bss, 1956684K reserved, 409600K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 960 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] GICv3: Distributor has no Range Selector support
[ 0.000000] GICv3: 16 PPIs implemented
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001900000
[ 0.000000] ITS [mem 0x01820000-0x0182ffff]
[ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[ 0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[ 0.000000] ITS@0x0000000001820000: allocated 524288 Devices @8a7800000 (flat, esz 8, psz 64K, shr 0)
[ 0.000000] ITS: using cache flushing for cmd queue
[ 0.000000] GICv3: using LPI property table @0x00000008a7030000
[ 0.000000] GIC: using cache flushing for LPI property table
[ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x00000008a7040000
[ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[ 0.000002] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[ 0.008406] Console: colour dummy device 80x25
[ 0.012971] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[ 0.023641] pid_max: default: 32768 minimum: 301
[ 0.028396] LSM: Security Framework initializing
[ 0.033153] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.040731] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.049521] rcu: Hierarchical SRCU implementation.
[ 0.054574] Platform MSI: msi-controller@1820000 domain created
[ 0.060822] PCI/MSI: /bus@100000/interrupt-controller@1800000/msi-controller@1820000 domain created
[ 0.070133] EFI services will not be available.
[ 0.074865] smp: Bringing up secondary CPUs ...
[ 0.088142] Detected PIPT I-cache on CPU1
[ 0.088166] GICv3: CPU1: found redistributor 1 region 0:0x0000000001920000
[ 0.088177] GICv3: CPU1: using allocated LPI pending table @0x00000008a7050000
[ 0.088212] CPU1: Booted secondary processor 0x0000000001 [0x411fd080]
[ 0.088263] smp: Brought up 1 node, 2 CPUs
[ 0.117606] SMP: Total of 2 processors activated.
[ 0.122410] CPU features: detected: 32-bit EL0 Support
[ 0.127665] CPU features: detected: CRC32 instructions
[ 0.141604] CPU: All CPU(s) started at EL2
[ 0.145802] alternatives: patching kernel code
[ 0.150827] devtmpfs: initialized
[ 0.159645] KASLR disabled due to lack of seed
[ 0.164288] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.174251] futex hash table entries: 512 (order: 3, 32768 bytes, linear)
[ 0.186292] pinctrl core: initialized pinctrl subsystem
[ 0.191950] DMI not present or invalid.
[ 0.196197] NET: Registered protocol family 16
[ 0.201424] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations
[ 0.208739] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.216799] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.225102] thermal_sys: Registered thermal governor 'step_wise'
[ 0.225104] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.231685] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.245317] ASID allocator initialised with 65536 entries
[ 0.267384] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.274240] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.281090] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.287937] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.295400] cryptd: max_cpu_qlen set to 1000
[ 0.301456] k3-chipinfo 43000014.chipid: Family:J721E rev:SR2.0 JTAGID[0x1bb6402f] Detected
[ 0.310267] vsys_3v3: supplied by vusb-main5v0
[ 0.315254] iommu: Default domain type: Translated
[ 0.320392] SCSI subsystem initialized
[ 0.324517] mc: Linux media interface: v0.10
[ 0.328890] videodev: Linux video capture interface: v2.00
[ 0.334528] pps_core: LinuxPPS API ver. 1 registered
[ 0.339601] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.348939] PTP clock support registered
[ 0.352957] EDAC MC: Ver: 3.0.0
[ 0.356748] FPGA manager framework
[ 0.360259] Advanced Linux Sound Architecture Driver Initialized.
[ 0.366851] clocksource: Switched to clocksource arch_sys_counter
[ 0.373173] VFS: Disk quotas dquot_6.6.0
[ 0.377205] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.386822] Carveout Heap: Exported 512 MiB at 0x00000000b8000000
[ 0.393114] NET: Registered protocol family 2
[ 0.397856] IP idents hash table entries: 65536 (order: 7, 524288 bytes, linear)
[ 0.406428] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear)
[ 0.415179] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.423381] TCP bind hash table entries: 32768 (order: 7, 524288 bytes, linear)
[ 0.431200] TCP: Hash tables configured (established 32768 bind 32768)
[ 0.437993] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear)
[ 0.444884] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear)
[ 0.452280] NET: Registered protocol family 1
[ 0.457010] RPC: Registered named UNIX socket transport module.
[ 0.463066] RPC: Registered udp transport module.
[ 0.467883] RPC: Registered tcp transport module.
[ 0.472688] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.479272] PCI: CLS 0 bytes, default 64
[ 0.483649] hw perfevents: enabled with armv8_cortex_a72 PMU driver, 7 counters available
[ 0.494025] Initialise system trusted keyrings
[ 0.498669] workingset: timestamp_bits=46 max_order=20 bucket_order=0
[ 0.506891] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.513096] NFS: Registering the id_resolver key type
[ 0.518290] Key type id_resolver registered
[ 0.522565] Key type id_legacy registered
[ 0.526689] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.533537] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.541178] 9p: Installing v9fs 9p2000 file system support
[ 0.566429] Key type asymmetric registered
[ 0.570615] Asymmetric key parser 'x509' registered
[ 0.575613] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[ 0.583172] io scheduler mq-deadline registered
[ 0.587797] io scheduler kyber registered
[ 0.593363] pinctrl-single 4301c000.pinctrl: 94 pins, size 376
[ 0.599541] pinctrl-single 11c000.pinctrl: 173 pins, size 692
[ 0.608191] k3-ringacc 2b800000.ringacc: Failed to get MSI domain
[ 0.614465] k3-ringacc 3c000000.ringacc: Failed to get MSI domain
[ 0.622319] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 0.630502] arm-smmu-v3 36600000.iommu: ias 48-bit, oas 48-bit (features 0x00001faf)
[ 0.638768] arm-smmu-v3 36600000.iommu: allocated 65536 entries for cmdq
[ 0.645850] arm-smmu-v3 36600000.iommu: allocated 32768 entries for evtq
[ 0.654430] arm-smmu-v3 36600000.iommu: msi_domain absent - falling back to wired irqs
[ 0.667505] brd: module loaded
[ 0.673946] loop: module loaded
[ 0.677561] sysfs: cannot create duplicate filename '/devices/platform/dma_buf_phys'
[ 0.685487] CPU: 1 PID: 1 Comm: swapper/0 Not tainted 5.10.120-00009-gbe27a7188056 #1
[ 0.693486] Hardware name: Texas Instruments J721E SK (DT)
[ 0.699087] Call trace:
[ 0.701591] dump_backtrace+0x0/0x1a0
[ 0.705327] show_stack+0x18/0x68
[ 0.708711] dump_stack+0xd0/0x12c
[ 0.712182] sysfs_warn_dup+0x60/0x80
[ 0.715917] sysfs_create_dir_ns+0xe0/0xf8
[ 0.720098] kobject_add_internal+0x98/0x288
[ 0.724455] kobject_add+0x94/0x100
[ 0.728013] device_add+0xe0/0x740
[ 0.731484] platform_device_add+0x100/0x238
[ 0.735841] platform_device_register_full+0xcc/0x150
[ 0.741002] dma_buf_phys_init+0x6c/0x9c
[ 0.745003] do_one_initcall+0x54/0x1b8
[ 0.748919] kernel_init_freeable+0x220/0x2a0
[ 0.753367] kernel_init+0x14/0x114
[ 0.756924] ret_from_fork+0x10/0x34
[ 0.760581] kobject_add_internal failed for dma_buf_phys with -EEXIST, don't try to register things with the same name in the same directory.
[ 0.773796] megasas: 07.714.04.00-rc1
[ 0.779290] tun: Universal TUN/TAP device driver, 1.6
[ 0.784707] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[ 0.791113] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 0.797186] sky2: driver version 1.30
[ 0.801482] VFIO - User Level meta-driver version: 0.3
[ 0.807234] i2c /dev entries driver
[ 0.811502] sdhci: Secure Digital Host Controller Interface driver
[ 0.817819] sdhci: Copyright(c) Pierre Ossman
[ 0.822447] sdhci-pltfm: SDHCI platform and OF driver helper
[ 0.828767] ledtrig-cpu: registered to indicate activity on CPUs
[ 0.835072] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 0.842281] optee: probing for conduit method.
[ 0.846843] optee: revision 3.17 (15a746d2)
[ 0.846978] optee: dynamic shared memory is enabled
[ 0.861777] optee: initialized driver
[ 0.866796] NET: Registered protocol family 17
[ 0.871416] 9pnet: Installing 9P2000 support
[ 0.875811] Key type dns_resolver registered
[ 0.880264] Loading compiled-in X.509 certificates
[ 0.890404] k3-ringacc 2b800000.ringacc: Failed to get MSI domain
[ 0.896745] k3-ringacc 3c000000.ringacc: Failed to get MSI domain
[ 0.905242] ti-sci 44083000.dmsc: ABI: 3.1 (firmware rev 0x0008 '8.4.1--v08.04.01 (Jolly Jellyfi')
[ 0.963186] omap_i2c 40b00000.i2c: bus 0 rev0.12 at 100 kHz
[ 0.969323] omap_i2c 40b10000.i2c: bus 1 rev0.12 at 100 kHz
[ 0.975408] omap_i2c 42120000.i2c: bus 2 rev0.12 at 100 kHz
[ 1.003016] i2c i2c-3: Added multiplexed i2c bus 4
[ 1.007993] i2c i2c-3: Added multiplexed i2c bus 5
[ 1.012891] pca954x 3-0071: registered 2 multiplexed busses for I2C switch pca9543
[ 1.020648] omap_i2c 2000000.i2c: bus 3 rev0.12 at 400 kHz
[ 1.026747] omap_i2c 2010000.i2c: bus 6 rev0.12 at 100 kHz
[ 1.055632] i2c i2c-7: Added multiplexed i2c bus 8
[ 1.060629] i2c i2c-7: Added multiplexed i2c bus 9
[ 1.065528] pca954x 7-0070: registered 2 multiplexed busses for I2C switch pca9543
[ 1.073316] omap_i2c 2030000.i2c: bus 7 rev0.12 at 400 kHz
[ 1.079816] ti-sci-intr bus@100000:bus@28380000:interrupt-controller2: Interrupt Router 137 domain created
[ 1.089834] ti-sci-intr bus@100000:interrupt-controller0: Interrupt Router 131 domain created
[ 1.098654] ti-sci-intr bus@100000:main-navss:interrupt-controller1: Interrupt Router 213 domain created
[ 1.108548] ti-sci-inta 33d00000.interrupt-controller: Interrupt Aggregator domain 209 created
[ 1.131850] j721e-pcie 2900000.pcie: host bridge /bus@100000/pcie@2900000 ranges:
[ 1.139526] j721e-pcie 2900000.pcie: IO 0x0010001000..0x0010010fff -> 0x0010001000
[ 1.147802] j721e-pcie 2900000.pcie: MEM 0x0010011000..0x0017ffffff -> 0x0010011000
[ 1.156078] j721e-pcie 2900000.pcie: IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
[ 1.165002] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
[ 1.172687] j721e-pcie 2910000.pcie: IO 0x0018001000..0x0018010fff -> 0x0018001000
[ 1.180967] j721e-pcie 2910000.pcie: MEM 0x0018011000..0x001fffffff -> 0x0018011000
[ 1.189244] j721e-pcie 2910000.pcie: IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
[ 1.198512] k3-ringacc 2b800000.ringacc: Ring Accelerator probed rings:286, gp-rings[96,20] sci-dev-id:235
[ 1.208391] k3-ringacc 2b800000.ringacc: dma-ring-reset-quirk: disabled
[ 1.215149] k3-ringacc 2b800000.ringacc: RA Proxy rev. 66346100, num_proxies:64
[ 1.224213] k3-ringacc 3c000000.ringacc: Ring Accelerator probed rings:1024, gp-rings[440,150] sci-dev-id:211
[ 1.234359] k3-ringacc 3c000000.ringacc: dma-ring-reset-quirk: disabled
[ 1.241122] k3-ringacc 3c000000.ringacc: RA Proxy rev. 66346100, num_proxies:64
[ 1.249110] 40a00000.serial: ttyS1 at MMIO 0x40a00000 (irq = 15, base_baud = 6000000) is a 8250
[ 1.258548] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 27, base_baud = 3000000) is a 8250
[ 1.267292] printk: console [ttyS2] enabled
[ 1.275731] printk: bootconsole [ns16550a0] disabled
[ 1.286225] 2810000.serial: ttyS3 at MMIO 0x2810000 (irq = 28, base_baud = 3000000) is a 8250
[ 1.295191] 2840000.serial: ttyS6 at MMIO 0x2840000 (irq = 29, base_baud = 3000000) is a 8250
[ 1.307415] davinci_mdio 46000f00.mdio: Configuring MDIO in manual mode
[ 1.350860] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 1.359580] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867
[ 1.367875] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00101, cpsw version 0x6BA80100 Ports: 2 quirks:00000000
[ 1.381615] davinci_mdio c000f00.mdio: Configuring MDIO in manual mode
[ 1.426856] davinci_mdio c000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 1.434409] davinci_mdio c000f00.mdio: no live phy, scanning all
[ 1.458219] davinci_mdio c000f00.mdio: phy[0]: device c000f00.mdio:00, driver unknown
[ 1.466057] davinci_mdio c000f00.mdio: phy[1]: device c000f00.mdio:01, driver unknown
[ 1.473868] davinci_mdio c000f00.mdio: phy[2]: device c000f00.mdio:02, driver unknown
[ 1.481678] davinci_mdio c000f00.mdio: phy[3]: device c000f00.mdio:03, driver unknown
[ 1.489491] davinci_mdio c000f00.mdio: phy[4]: device c000f00.mdio:04, driver unknown
[ 1.497301] davinci_mdio c000f00.mdio: phy[5]: device c000f00.mdio:05, driver unknown
[ 1.505112] davinci_mdio c000f00.mdio: phy[6]: device c000f00.mdio:06, driver unknown
[ 1.512923] davinci_mdio c000f00.mdio: phy[7]: device c000f00.mdio:07, driver unknown
[ 1.520733] davinci_mdio c000f00.mdio: phy[8]: device c000f00.mdio:08, driver unknown
[ 1.528542] davinci_mdio c000f00.mdio: phy[9]: device c000f00.mdio:09, driver unknown
[ 1.536352] davinci_mdio c000f00.mdio: phy[10]: device c000f00.mdio:0a, driver unknown
[ 1.544248] davinci_mdio c000f00.mdio: phy[11]: device c000f00.mdio:0b, driver unknown
[ 1.552148] davinci_mdio c000f00.mdio: phy[12]: device c000f00.mdio:0c, driver unknown
[ 1.560048] davinci_mdio c000f00.mdio: phy[13]: device c000f00.mdio:0d, driver unknown
[ 1.567952] davinci_mdio c000f00.mdio: phy[14]: device c000f00.mdio:0e, driver unknown
[ 1.575883] davinci_mdio c000f00.mdio: phy[15]: device c000f00.mdio:0f, driver unknown
[ 1.583781] davinci_mdio c000f00.mdio: phy[16]: device c000f00.mdio:10, driver unknown
[ 1.591678] davinci_mdio c000f00.mdio: phy[17]: device c000f00.mdio:11, driver unknown
[ 1.599575] davinci_mdio c000f00.mdio: phy[18]: device c000f00.mdio:12, driver unknown
[ 1.607472] davinci_mdio c000f00.mdio: phy[19]: device c000f00.mdio:13, driver unknown
[ 1.615371] davinci_mdio c000f00.mdio: phy[20]: device c000f00.mdio:14, driver unknown
[ 1.623269] davinci_mdio c000f00.mdio: phy[21]: device c000f00.mdio:15, driver unknown
[ 1.631166] davinci_mdio c000f00.mdio: phy[22]: device c000f00.mdio:16, driver unknown
[ 1.639062] davinci_mdio c000f00.mdio: phy[23]: device c000f00.mdio:17, driver unknown
[ 1.646958] davinci_mdio c000f00.mdio: phy[24]: device c000f00.mdio:18, driver unknown
[ 1.654855] davinci_mdio c000f00.mdio: phy[25]: device c000f00.mdio:19, driver unknown
[ 1.662752] davinci_mdio c000f00.mdio: phy[26]: device c000f00.mdio:1a, driver unknown
[ 1.670651] davinci_mdio c000f00.mdio: phy[27]: device c000f00.mdio:1b, driver unknown
[ 1.678550] davinci_mdio c000f00.mdio: phy[28]: device c000f00.mdio:1c, driver unknown
[ 1.686450] davinci_mdio c000f00.mdio: phy[29]: device c000f00.mdio:1d, driver unknown
[ 1.694383] davinci_mdio c000f00.mdio: phy[30]: device c000f00.mdio:1e, driver unknown
[ 1.702281] davinci_mdio c000f00.mdio: phy[31]: device c000f00.mdio:1f, driver unknown
[ 1.710247] am65-cpsw-nuss c000000.ethernet: initializing am65 cpsw nuss version 0x6BA01901, cpsw version 0x6BA80101 Ports: 9 quirks:00000000
[ 1.724798] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010a, freq:200000000, add_val:4 pps:0
[ 1.840187] vdd_mmc1: supplied by vsys_3v3
[ 1.845084] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fc7100
[ 1.851966] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fc7100
[ 1.858805] omap-mailbox 31f82000.mailbox: omap mailbox rev 0x66fc7100
[ 1.865636] omap-mailbox 31f83000.mailbox: omap mailbox rev 0x66fc7100
[ 1.872446] omap-mailbox 31f84000.mailbox: omap mailbox rev 0x66fc7100
[ 1.882674] j721e-pcie 2900000.pcie: host bridge /bus@100000/pcie@2900000 ranges:
[ 1.890178] j721e-pcie 2900000.pcie: IO 0x0010001000..0x0010010fff -> 0x0010001000
[ 1.898258] j721e-pcie 2900000.pcie: MEM 0x0010011000..0x0017ffffff -> 0x0010011000
[ 1.906337] j721e-pcie 2900000.pcie: IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
[ 2.917084] j721e-pcie 2900000.pcie: PCI host bridge to bus 0000:00
[ 2.923346] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 2.928820] pci_bus 0000:00: root bus resource [io 0x0000-0xffff] (bus address [0x10001000-0x10010fff])
[ 2.938280] pci_bus 0000:00: root bus resource [mem 0x10011000-0x17ffffff]
[ 2.945162] pci 0000:00:00.0: [104c:b00d] type 01 class 0x060400
[ 2.951154] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x4 may corrupt adjacent RW1C bits
[ 2.960850] pci 0000:00:00.0: supports D1
[ 2.964848] pci 0000:00:00.0: PME# supported from D0 D1 D3hot
[ 2.972732] pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[ 2.982482] pci_bus 0000:01: busn_res: [bus 01-ff] end is updated to 01
[ 2.989095] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 2.994284] pcieport 0000:00:00.0: PME: Signaling with IRQ 492
[ 3.000634] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
[ 3.008119] j721e-pcie 2910000.pcie: IO 0x0018001000..0x0018010fff -> 0x0018001000
[ 3.016199] j721e-pcie 2910000.pcie: MEM 0x0018011000..0x001fffffff -> 0x0018011000
[ 3.024278] j721e-pcie 2910000.pcie: IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
[ 4.034996] j721e-pcie 2910000.pcie: PCI host bridge to bus 0001:00
[ 4.041256] pci_bus 0001:00: root bus resource [bus 00-ff]
[ 4.046729] pci_bus 0001:00: root bus resource [io 0x10000-0x1ffff] (bus address [0x18001000-0x18010fff])
[ 4.056361] pci_bus 0001:00: root bus resource [mem 0x18011000-0x1fffffff]
[ 4.063239] pci 0001:00:00.0: [104c:b00d] type 01 class 0x060400
[ 4.069232] pci_bus 0001:00: 2-byte config write to 0001:00:00.0 offset 0x4 may corrupt adjacent RW1C bits
[ 4.078924] pci 0001:00:00.0: supports D1
[ 4.082922] pci 0001:00:00.0: PME# supported from D0 D1 D3hot
[ 4.090640] pci 0001:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[ 4.100584] pci_bus 0001:01: busn_res: [bus 01-ff] end is updated to 01
[ 4.107192] pci 0001:00:00.0: PCI bridge to [bus 01]
[ 4.112357] pcieport 0001:00:00.0: PME: Signaling with IRQ 494
[ 4.119123] ti-udma 285c0000.dma-controller: Channels: 26 (tchan: 13, rchan: 13, gp-rflow: 8)
[ 4.129823] ti-udma 31150000.dma-controller: Channels: 122 (tchan: 61, rchan: 61, gp-rflow: 16)
[ 4.145515] spi-nor spi0.0: s28hs512t (65536 Kbytes)
[ 4.150492] 8 cmdlinepart partitions found on MTD device 47040000.spi.0
[ 4.157090] Creating 8 MTD partitions on "47040000.spi.0":
[ 4.162562] 0x000000000000-0x000000080000 : "ospi.tiboot3"
[ 4.168546] 0x000000080000-0x000000280000 : "ospi.tispl"
[ 4.174252] 0x000000280000-0x000000680000 : "ospi.u-boot"
[ 4.180035] 0x000000680000-0x0000006c0000 : "ospi.env"
[ 4.185556] 0x0000006c0000-0x0000007c0000 : "ospi.sysfw"
[ 4.191250] 0x0000007c0000-0x000000800000 : "ospi.env.backup"
[ 4.197380] 0x000000800000-0x000003fc0000 : "ospi.rootfs"
[ 4.203176] 0x000003fc0000-0x000004000000 : "ospi.phypattern"
[ 4.213654] davinci_mdio 46000f00.mdio: Configuring MDIO in manual mode
[ 4.258861] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 4.267527] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867
[ 4.275818] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00101, cpsw version 0x6BA80100 Ports: 2 quirks:00000000
[ 4.289865] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48
[ 4.296845] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
[ 4.304057] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
[ 4.310410] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010a, freq:500000000, add_val:1 pps:0
[ 4.320852] davinci_mdio c000f00.mdio: Configuring MDIO in manual mode
[ 4.366860] davinci_mdio c000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 4.374413] davinci_mdio c000f00.mdio: no live phy, scanning all
[ 4.398324] davinci_mdio c000f00.mdio: phy[0]: device c000f00.mdio:00, driver unknown
[ 4.406184] davinci_mdio c000f00.mdio: phy[1]: device c000f00.mdio:01, driver unknown
[ 4.413995] davinci_mdio c000f00.mdio: phy[2]: device c000f00.mdio:02, driver unknown
[ 4.421806] davinci_mdio c000f00.mdio: phy[3]: device c000f00.mdio:03, driver unknown
[ 4.429616] davinci_mdio c000f00.mdio: phy[4]: device c000f00.mdio:04, driver unknown
[ 4.437427] davinci_mdio c000f00.mdio: phy[5]: device c000f00.mdio:05, driver unknown
[ 4.445238] davinci_mdio c000f00.mdio: phy[6]: device c000f00.mdio:06, driver unknown
[ 4.453048] davinci_mdio c000f00.mdio: phy[7]: device c000f00.mdio:07, driver unknown
[ 4.460861] davinci_mdio c000f00.mdio: phy[8]: device c000f00.mdio:08, driver unknown
[ 4.468671] davinci_mdio c000f00.mdio: phy[9]: device c000f00.mdio:09, driver unknown
[ 4.476485] davinci_mdio c000f00.mdio: phy[10]: device c000f00.mdio:0a, driver unknown
[ 4.484383] davinci_mdio c000f00.mdio: phy[11]: device c000f00.mdio:0b, driver unknown
[ 4.492280] davinci_mdio c000f00.mdio: phy[12]: device c000f00.mdio:0c, driver unknown
[ 4.500178] davinci_mdio c000f00.mdio: phy[13]: device c000f00.mdio:0d, driver unknown
[ 4.508080] davinci_mdio c000f00.mdio: phy[14]: device c000f00.mdio:0e, driver unknown
[ 4.515992] davinci_mdio c000f00.mdio: phy[15]: device c000f00.mdio:0f, driver unknown
[ 4.523891] davinci_mdio c000f00.mdio: phy[16]: device c000f00.mdio:10, driver unknown
[ 4.531789] davinci_mdio c000f00.mdio: phy[17]: device c000f00.mdio:11, driver unknown
[ 4.539685] davinci_mdio c000f00.mdio: phy[18]: device c000f00.mdio:12, driver unknown
[ 4.547581] davinci_mdio c000f00.mdio: phy[19]: device c000f00.mdio:13, driver unknown
[ 4.555478] davinci_mdio c000f00.mdio: phy[20]: device c000f00.mdio:14, driver unknown
[ 4.563375] davinci_mdio c000f00.mdio: phy[21]: device c000f00.mdio:15, driver unknown
[ 4.571272] davinci_mdio c000f00.mdio: phy[22]: device c000f00.mdio:16, driver unknown
[ 4.579171] davinci_mdio c000f00.mdio: phy[23]: device c000f00.mdio:17, driver unknown
[ 4.587070] davinci_mdio c000f00.mdio: phy[24]: device c000f00.mdio:18, driver unknown
[ 4.594966] davinci_mdio c000f00.mdio: phy[25]: device c000f00.mdio:19, driver unknown
[ 4.602863] davinci_mdio c000f00.mdio: phy[26]: device c000f00.mdio:1a, driver unknown
[ 4.610760] davinci_mdio c000f00.mdio: phy[27]: device c000f00.mdio:1b, driver unknown
[ 4.618658] davinci_mdio c000f00.mdio: phy[28]: device c000f00.mdio:1c, driver unknown
[ 4.626558] davinci_mdio c000f00.mdio: phy[29]: device c000f00.mdio:1d, driver unknown
[ 4.634475] davinci_mdio c000f00.mdio: phy[30]: device c000f00.mdio:1e, driver unknown
[ 4.642372] davinci_mdio c000f00.mdio: phy[31]: device c000f00.mdio:1f, driver unknown
[ 4.650336] am65-cpsw-nuss c000000.ethernet: initializing am65 cpsw nuss version 0x6BA01901, cpsw version 0x6BA80101 Ports: 9 quirks:00000000
[ 4.664046] am65-cpsw-nuss c000000.ethernet: set new flow-id-base 140
[ 4.671012] am65-cpsw-nuss c000000.ethernet: /bus@100000/ethernet@c000000/ethernet-ports/port@1 error retrieving port phy: -19
[ 4.685415] mmc0: CQHCI version 5.10
[ 4.687588] debugfs: Directory 'pd:27' with parent 'pm_genpd' already present!
[ 4.696285] debugfs: Directory 'pd:26' with parent 'pm_genpd' already present!
[ 4.704542] debugfs: Directory 'pd:242' with parent 'pm_genpd' already present!
[ 4.711893] debugfs: Directory 'pd:241' with parent 'pm_genpd' already present!
[ 4.719208] debugfs: Directory 'pd:240' with parent 'pm_genpd' already present!
[ 4.726533] debugfs: Directory 'pd:239' with parent 'pm_genpd' already present!
[ 4.746694] ALSA device list:
[ 4.749659] No soundcards found.
[ 5.755614] mmc0: SDHCI controller on 4fb0000.mmc [4fb0000.mmc] using ADMA 64-bit
[ 5.764250] Waiting for root device PARTUUID=14cb2911-02...
[ 5.816213] mmc0: new ultra high speed DDR50 SDXC card at address aaaa
[ 5.823095] mmcblk0: mmc0:aaaa SN128 119 GiB
[ 5.828721] mmcblk0: p1 p2
[ 6.181303] EXT4-fs (mmcblk0p2): recovery complete
[ 6.186916] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 6.195049] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 6.201614] devtmpfs: mounted
[ 6.205445] Freeing unused kernel memory: 1792K
[ 6.210073] Run /sbin/init as init process
[ 6.214159] with arguments:
[ 6.214161] /sbin/init
[ 6.214163] with environment:
[ 6.214165] HOME=/
[ 6.214167] TERM=linux
[ 6.381014] systemd[1]: System time before build time, advancing clock.
[ 6.431298] NET: Registered protocol family 10
[ 6.436247] Segment Routing with IPv6
[ 6.459397] systemd[1]: systemd 244.5+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -)
[ 6.481113] systemd[1]: Detected architecture arm64.
[ 6.519698] systemd[1]: Set hostname to <tda4vm-sk>.
[ 6.746282] systemd[1]: /lib/systemd/system/docker.socket:6: ListenStream= references a path below legacy directory /var/run/, updating /var/run/docker.sock \xe2\x86\x92 /run/docker.sock; please update the u.
[ 6.820700] random: systemd: uninitialized urandom read (16 bytes read)
[ 6.827432] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.
[ 6.839756] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)
[ 6.849770] systemd[1]: Created slice system-getty.slice.
[ 6.870938] random: systemd: uninitialized urandom read (16 bytes read)
[ 6.878279] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ 6.898942] random: systemd: uninitialized urandom read (16 bytes read)
[ 6.906149] systemd[1]: Created slice User and Session Slice.
[ 6.927062] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ 6.950982] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ 6.974967] systemd[1]: Reached target Paths.
[ 6.990919] systemd[1]: Reached target Remote File Systems.
[ 7.010908] systemd[1]: Reached target Slices.
[ 7.026915] systemd[1]: Reached target Swap.
[ 7.047576] systemd[1]: Listening on RPCbind Server Activation Socket.
[ 7.070949] systemd[1]: Reached target RPC Port Mapper.
[ 7.093199] systemd[1]: Listening on Process Core Dump Socket.
[ 7.115060] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ 7.146717] systemd[1]: Condition check resulted in Journal Audit Socket being skipped.
[ 7.155093] systemd[1]: Listening on Journal Socket (/dev/log).
[ 7.175165] systemd[1]: Listening on Journal Socket.
[ 7.191221] systemd[1]: Listening on Network Service Netlink Socket.
[ 7.215133] systemd[1]: Listening on udev Control Socket.
[ 7.235053] systemd[1]: Listening on udev Kernel Socket.
[ 7.257177] systemd[1]: Mounting Huge Pages File System...
[ 7.277103] systemd[1]: Mounting POSIX Message Queue File System...
[ 7.301119] systemd[1]: Mounting Kernel Debug File System...
[ 7.321481] systemd[1]: Mounting Temporary Directory (/tmp)...
[ 7.341302] systemd[1]: Starting Create list of static device nodes for the current kernel...
[ 7.369053] systemd[1]: Starting Start psplash boot splash screen...
[ 7.393867] systemd[1]: Starting RPC Bind...
[ 7.407074] systemd[1]: Condition check resulted in File System Check on Root Device being skipped.
[ 7.419030] systemd[1]: Starting Journal Service...
[ 7.442339] systemd[1]: Starting Load Kernel Modules...
[ 7.457304] systemd[1]: Starting Remount Root and Kernel File Systems...
[ 7.480110] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[ 7.481346] systemd[1]: Starting udev Coldplug all Devices...
[ 7.509693] systemd[1]: Started RPC Bind.
[ 7.523282] systemd[1]: Started Journal Service.
[ 7.751666] systemd-journald[221]: Received client request to flush runtime journal.
[ 7.867790] urandom_read_iter: 47 callbacks suppressed
[ 7.867793] random: systemd: uninitialized urandom read (16 bytes read)
[ 7.894959] random: systemd: uninitialized urandom read (16 bytes read)
[ 7.905174] random: systemd-journal: uninitialized urandom read (16 bytes read)
[ 8.342419] CAN device driver interface
[ 8.600312] img_enc 4200000.video-encoder: vxe_enc_probe: using heap 1 for internal alloc
[ 8.638277] Current ser address ports is 0x26
[ 8.659065] k3-dsp-rproc 4d80800000.dsp: assigned reserved memory node vision-apps-c66-dma-memory@a9000000
[ 8.683671] k3-dsp-rproc 4d80800000.dsp: configured DSP for IPC-only mode
[ 8.757156] Current ser address ports is 0x44
[ 8.783986] remoteproc remoteproc0: 4d80800000.dsp is available
[ 8.799843] Current expander address ports is 0x11
[ 8.826338] img_enc 4200000.video-encoder: encoder registered as /dev/video0
[ 8.870256] [drm] Initialized tidss 1.0.0 20180215 for 4a00000.dss on minor 0
[ 8.880172] remoteproc remoteproc0: attaching to 4d80800000.dsp
[ 8.896866] img_dec 4300000.video-decoder: decoder registered as /dev/video1
[ 8.918742] Current SIO ports is 0
[ 8.961844] Console: switching to colour frame buffer device 240x67
[ 8.979472] Current CSI ports is 0x0
[ 8.988223] tidss 4a00000.dss: [drm] fb0: tidssdrmfb frame buffer device
[ 9.010878] camera-mipi-clk = 800MHz
[ 9.019165] ar0234 8-0044: MIPI Clock = 800, MIPI Lanes = 4
[ 9.040334] k3-dsp-rproc 4d80800000.dsp: DSP initialized in IPC-only mode
[ 9.058141] ar0234 8-0044: supply avdd not found, using dummy regulator
[ 9.067140] remoteproc0#vdev0buffer: assigned reserved memory node vision-apps-c66-dma-memory@a9000000
[ 9.195443] ar0234 8-0044: supply dovdd not found, using dummy regulator
[ 9.243257] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 9.248795] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xd
[ 9.264006] urandom_read_iter: 25 callbacks suppressed
[ 9.264010] random: systemd: uninitialized urandom read (16 bytes read)
[ 9.279348] random: systemd: uninitialized urandom read (16 bytes read)
[ 9.288190] ar0234 8-0044: supply dvdd not found, using dummy regulator
[ 9.305106] remoteproc0#vdev0buffer: registered virtio0 (type 7)
[ 9.324229] platform 41000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1)
[ 9.386968] ar0234 8-0044: Issuing CHIP reset for Deserializer ...
[ 9.431650] remoteproc remoteproc0: remote processor 4d80800000.dsp is now attached
[ 9.467051] platform 41000000.r5f: configured R5F for IPC-only mode
[ 9.499975] k3-dsp-rproc 4d81800000.dsp: assigned reserved memory node vision-apps-c66-dma-memory@a8000000
[ 9.535066] platform 41000000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a0000000
[ 9.586236] k3-dsp-rproc 4d81800000.dsp: configured DSP for IPC-only mode
[ 9.590870] random: crng init done
[ 9.598314] remoteproc remoteproc1: 41000000.r5f is available
[ 9.604412] remoteproc remoteproc1: attaching to 41000000.r5f
[ 9.611888] platform 41000000.r5f: R5F core initialized in IPC-only mode
[ 9.620082] remoteproc1#vdev0buffer: assigned reserved memory node vision-apps-r5f-dma-memory@a0000000
[ 9.639807] virtio_rpmsg_bus virtio1: rpmsg host is online
[ 9.647709] remoteproc1#vdev0buffer: registered virtio1 (type 7)
[ 9.650943] remoteproc remoteproc2: 4d81800000.dsp is available
[ 9.659860] virtio_rpmsg_bus virtio1: creating channel ti.ipc4.ping-pong addr 0xd
[ 9.661803] remoteproc remoteproc1: remote processor 41000000.r5f is now attached
[ 9.667448] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0xe
[ 9.696535] platform 5c00000.r5f: configured R5F for IPC-only mode
[ 9.711149] platform 5c00000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a2000000
[ 9.711501] remoteproc remoteproc2: attaching to 4d81800000.dsp
[ 9.761042] k3-dsp-rproc 4d81800000.dsp: DSP initialized in IPC-only mode
[ 9.761339] remoteproc remoteproc3: 5c00000.r5f is available
[ 9.796015] remoteproc2#vdev0buffer: assigned reserved memory node vision-apps-c66-dma-memory@a8000000
[ 9.855035] remoteproc remoteproc3: attaching to 5c00000.r5f
[ 9.859270] virtio_rpmsg_bus virtio2: rpmsg host is online
[ 9.862873] virtio_rpmsg_bus virtio2: creating channel rpmsg_chrdev addr 0xd
[ 9.899485] remoteproc2#vdev0buffer: registered virtio2 (type 7)
[ 9.907436] platform 5c00000.r5f: R5F core initialized in IPC-only mode
[ 9.925041] remoteproc remoteproc2: remote processor 4d81800000.dsp is now attached
[ 9.939292] k3-dsp-rproc 64800000.dsp: assigned reserved memory node vision-apps-c71-dma-memory@aa000000
[ 9.941098] remoteproc3#vdev0buffer: assigned reserved memory node vision-apps-r5f-dma-memory@a2000000
[ 9.963917] k3-dsp-rproc 64800000.dsp: configured DSP for IPC-only mode
[ 9.979563] remoteproc remoteproc4: 64800000.dsp is available
[ 9.992050] remoteproc remoteproc4: attaching to 64800000.dsp
[ 9.999002] remoteproc remoteproc4: unsupported resource 65538
[ 10.007168] k3-dsp-rproc 64800000.dsp: DSP initialized in IPC-only mode
[ 10.016385] remoteproc4#vdev0buffer: assigned reserved memory node vision-apps-c71-dma-memory@aa000000
[ 10.022051] virtio_rpmsg_bus virtio3: rpmsg host is online
[ 10.035499] virtio_rpmsg_bus virtio4: rpmsg host is online
[ 10.037048] virtio_rpmsg_bus virtio3: creating channel rpmsg_chrdev addr 0xd
[ 10.042908] remoteproc4#vdev0buffer: registered virtio4 (type 7)
[ 10.052880] virtio_rpmsg_bus virtio4: creating channel rpmsg_chrdev addr 0xd
[ 10.057103] remoteproc remoteproc4: remote processor 64800000.dsp is now attached
[ 10.075533] remoteproc3#vdev0buffer: registered virtio3 (type 7)
[ 10.122907] remoteproc remoteproc3: remote processor 5c00000.r5f is now attached
[ 10.164411] platform 5d00000.r5f: configured R5F for IPC-only mode
[ 10.181100] m_can_platform 40528000.can: m_can device registered (irq=20, version=32)
[ 10.195090] m_can_platform 2701000.can: m_can device registered (irq=42, version=32)
[ 10.209880] m_can_platform 2751000.can: m_can device registered (irq=44, version=32)
[ 10.224741] m_can_platform 2791000.can: m_can device registered (irq=46, version=32)
[ 10.247797] platform 5d00000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a4000000
[ 10.311132] remoteproc remoteproc5: 5d00000.r5f is available
[ 10.317171] remoteproc remoteproc5: attaching to 5d00000.r5f
[ 10.328183] platform 5d00000.r5f: R5F core initialized in IPC-only mode
[ 10.334857] remoteproc5#vdev0buffer: assigned reserved memory node vision-apps-r5f-dma-memory@a4000000
[ 10.355348] virtio_rpmsg_bus virtio5: rpmsg host is online
[ 10.367007] remoteproc5#vdev0buffer: registered virtio5 (type 7)
[ 10.373237] virtio_rpmsg_bus virtio3: creating channel rpmsg_chrdev addr 0x15
[ 10.382978] virtio_rpmsg_bus virtio5: creating channel rpmsg_chrdev addr 0xd
[ 10.390153] virtio_rpmsg_bus virtio5: creating channel rpmsg_chrdev addr 0x15
[ 10.401249] virtio_rpmsg_bus virtio5: creating channel ti.ipc4.ping-pong addr 0xe
[ 10.408875] virtio_rpmsg_bus virtio4: creating channel rpmsg_chrdev addr 0x15
[ 10.417151] remoteproc remoteproc5: remote processor 5d00000.r5f is now attached
[ 10.424674] virtio_rpmsg_bus virtio4: creating channel ti.ipc4.ping-pong addr 0xe
[ 10.432355] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0x15
[ 10.439597] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xe
[ 10.450289] virtio_rpmsg_bus virtio2: creating channel rpmsg_chrdev addr 0x15
[ 10.457760] virtio_rpmsg_bus virtio2: creating channel ti.ipc4.ping-pong addr 0xe
[ 10.465418] virtio_rpmsg_bus virtio3: creating channel ti.ipc4.ping-pong addr 0xe
[ 10.479109] platform 5e00000.r5f: configured R5F for remoteproc mode
[ 10.485544] omap_i2c 2030000.i2c: controller timed out
[ 10.490723] ar0234 8-0044: Failed writing register ret = -110!
[ 10.516326] ar0234 8-0044: fpdlink3_write_8b_reg:write reg error: reg = 0x1,val = 0x2
[ 10.527938] platform 5e00000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a6000000
[ 10.533648] ar0234 8-0044: fpdlink3_config_init(587): Failed
[ 10.555983] remoteproc remoteproc6: 5e00000.r5f is available
[ 10.572517] remoteproc remoteproc6: Direct firmware load for j7-main-r5f1_0-fw failed with error -2
[ 10.582095] ar0234 8-0044: fpdlink3_config_init_failed
[ 10.585367] remoteproc remoteproc6: powering up 5e00000.r5f
[ 10.594935] remoteproc remoteproc6: Direct firmware load for j7-main-r5f1_0-fw failed with error -2
[ 10.598958] platform 5f00000.r5f: configured R5F for remoteproc mode
[ 10.607954] remoteproc remoteproc6: request_firmware failed: -2
[ 10.650307] ar0234: probe of 8-0044 failed with error -5
[ 10.675267] Current ser address ports is 0x25
[ 10.679686] Current ser address ports is 0x43
[ 10.685243] platform 5f00000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a7000000
[ 10.706900] Current expander address ports is 0x10
[ 10.714079] remoteproc remoteproc7: 5f00000.r5f is available
[ 10.723469] Current SIO ports is 1
[ 10.743546] remoteproc remoteproc7: Direct firmware load for j7-main-r5f1_1-fw failed with error -2
[ 10.754398] remoteproc remoteproc7: powering up 5f00000.r5f
[ 10.760099] Current CSI ports is 0x1
[ 10.763726] remoteproc remoteproc7: Direct firmware load for j7-main-r5f1_1-fw failed with error -2
[ 10.774891] remoteproc remoteproc7: request_firmware failed: -2
[ 10.789028] camera-mipi-clk = 800MHz
[ 10.860554] ar0234 8-0043: MIPI Clock = 800, MIPI Lanes = 4
[ 10.904529] ar0234 8-0043: supply avdd not found, using dummy regulator
[ 10.935043] ar0234 8-0043: supply dovdd not found, using dummy regulator
[ 10.947538] ar0234 8-0043: supply dvdd not found, using dummy regulator
[ 11.174151] usbcore: registered new interface driver usbfs
[ 11.184271] cdns-csi2rx 4504000.csi-bridge: Probed CSI2RX with 4/4 lanes, 4 streams, external D-PHY
[ 11.198472] remoteproc remoteproc8: b034000.pru is available
[ 11.220534] remoteproc remoteproc9: b004000.rtu is available
[ 11.240474] cdns-csi2rx 4514000.csi-bridge: Probed CSI2RX with 4/4 lanes, 4 streams, external D-PHY
[ 11.242993] usbcore: registered new interface driver hub
[ 11.256166] remoteproc remoteproc10: b00a000.txpru is available
[ 11.268634] remoteproc remoteproc11: b038000.pru is available
[ 11.269674] usbcore: registered new device driver usb
[ 11.274871] remoteproc remoteproc12: b006000.rtu is available
[ 11.288512] remoteproc remoteproc13: b00c000.txpru is available
[ 11.296219] remoteproc remoteproc14: b134000.pru is available
[ 11.316903] remoteproc remoteproc15: b104000.rtu is available
[ 11.324275] remoteproc remoteproc16: b10a000.txpru is available
[ 11.331979] remoteproc remoteproc17: b138000.pru is available
[ 11.345593] remoteproc remoteproc18: b106000.rtu is available
[ 11.352336] remoteproc remoteproc19: b10c000.txpru is available
[ 11.456034] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ 11.495679] omap_rng 4e10000.rng: Random Number Generator ver. 241b34c
[ 11.962863] omap_i2c 2030000.i2c: timeout waiting for bus ready
[ 11.968791] ar0234 8-0043: Failed writing register ret = -16!
[ 11.974538] ar0234 8-0043: fpdlink3_write_8b_reg:write reg error: reg = 0x4c,val = 0x12
[ 11.982534] ar0234 8-0043: fpdlink3_serializer_ports_config(442): Failed
[ 11.989267] ar0234 8-0043: fpdlink3_config_init(612): Failed
[ 11.994924] ar0234 8-0043: fpdlink3_config_init_failed
[ 12.000263] ar0234: probe of 8-0043 failed with error -5
[ 12.203688] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 12.209209] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[ 12.217024] xhci-hcd xhci-hcd.0.auto: hcc params 0x200073c9 hci version 0x100 quirks 0x0000002000010010
[ 12.226445] xhci-hcd xhci-hcd.0.auto: irq 648, io mem 0x06410000
[ 12.232633] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10
[ 12.240894] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 12.248120] usb usb1: Product: xHCI Host Controller
[ 12.252994] usb usb1: Manufacturer: Linux 5.10.120-00009-gbe27a7188056 xhci-hcd
[ 12.260295] usb usb1: SerialNumber: xhci-hcd.0.auto
[ 12.265431] hub 1-0:1.0: USB hub found
[ 12.269209] hub 1-0:1.0: 1 port detected
[ 12.273317] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 12.278810] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
[ 12.286466] xhci-hcd xhci-hcd.0.auto: Host supports USB 3.0 SuperSpeed
[ 12.293014] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 12.301151] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 5.10
[ 12.309404] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 12.316616] usb usb2: Product: xHCI Host Controller
[ 12.321489] usb usb2: Manufacturer: Linux 5.10.120-00009-gbe27a7188056 xhci-hcd
[ 12.328786] usb usb2: SerialNumber: xhci-hcd.0.auto
[ 12.333913] hub 2-0:1.0: USB hub found
[ 12.337684] hub 2-0:1.0: 1 port detected
[ 12.542871] usb 1-1: new high-speed USB device number 2 using xhci-hcd
[ 12.968751] Bluetooth: Core ver 2.22
[ 12.979233] usb 1-1: New USB device found, idVendor=0451, idProduct=8142, bcdDevice= 1.00
[ 12.993363] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=1
[ 13.006153] NET: Registered protocol family 31
[ 13.020177] Bluetooth: HCI device and connection manager initialized
[ 13.037810] Bluetooth: HCI socket layer initialized
[ 13.049782] usb 1-1: SerialNumber: FA080841A4CD
[ 13.063325] hub 1-1:1.0: USB hub found
[ 13.069713] Bluetooth: L2CAP socket layer initialized
[ 13.075825] hub 1-1:1.0: 4 ports detected
[ 13.083794] Bluetooth: SCO socket layer initialized
[ 13.106950] usb 2-1: new SuperSpeed Gen 1 USB device number 2 using xhci-hcd
[ 13.135325] usb 2-1: New USB device found, idVendor=0451, idProduct=8140, bcdDevice= 1.00
[ 13.145607] usb 2-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 13.160450] hub 2-1:1.0: USB hub found
[ 13.167372] hub 2-1:1.0: 4 ports detected
[ 13.379072] am65-cpsw-nuss 46000000.ethernet eth0: PHY [46000f00.mdio:00] driver [TI DP83867] (irq=POLL)
[ 13.424742] am65-cpsw-nuss 46000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[ 17.560189] am65-cpsw-nuss 46000000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
[ 17.568901] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 134.364231] Initializing XFRM netlink socket
[ 135.879237] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
[ 135.893198] Bridge firewalling registered
[ 136.410130] process 'docker/tmp/qemu-check664261453/check' started with executable stack