This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Here is a dump of k3conf help from the target:
k3conf --help
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-64-g48cb8e8 built Fri Dec 16 11:42:13 UTC 2022) |
| SoC | J7200 SR1.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.5.2--v08.05.02 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
NAME
k3conf - TI K3 Configuration Diagnostic Tool
SYNOPSIS
k3conf [--host <id>] [--version] [--help] [--cpuinfo] <command> [<args>]
DESCRIPTION
k3conf is standalone application designed to provide a quick'n easy way to
diagnose/debug/audit TI K3 architecture based processors configuration at
runtime, with no particular kernel dependency.
k3conf is designed to be as much platform-agnostic as possible, being able to
run on any Linux platform and easily ported to other OS.
Even if k3conf today focuses mainly on TISCI related functionality, it is
intended to be extended to any other area.
OPTIONS
--host <id>
Use this host id for communicating with sysfw
--help
Print k3conf help.
--version
Print k3conf version.
--cpuinfo
Print the host processor information.
COMMANDS
k3conf show hosts
Prints all the available TISCI hosts
k3conf show threads
Prints all the available TISCI secure proxy threads
k3conf show device
Prints all the available TISCI devices
k3conf show device <dev_id>
Prints the corresponding device id information
k3conf show clock
Prints all the available TISCI clocks
k3conf show clock <dev_id>
Prints the clocks for corresponding device id
k3conf show processor
Prints all the available TISCI processors
k3conf show rm
Prints resources managed by System firmware
k3conf show rm <dev_id>
Prints resources managed by System firmware for corresponding device
k3conf dump device
Prints device status of all the TISCI devices
k3conf dump device <dev_id>
Prints the corresponding device id status
k3conf dump clock
Prints clock status all the available TISCI clocks
k3conf dump clock <dev_id>
Prints the available clock status for corresponding device id
k3conf dump processor
Prints status of all the available TISCI processors
k3conf dump processor <proc_id>
Prints status of the given TISCI processors
k3conf dump rm [OPTIONS]
Prints resource allocation for all utypes / hosts
k3conf dump rm [OPTIONS] <type>
Prints resource allocation for corresponding type
k3conf dump rm [OPTIONS] <type> <subtype>
Prints resource allocation for corresponding device/type
[OPTIONS]
-h <host_id>
Filter only for corresponding host_id
k3conf enable device <dev_id>
Enables the TISCI device and prints the status
k3conf enable clock <dev_id> <clk_id>
Enables the TISCI clock and prints the status
k3conf disable device <dev_id>
Disables the TISCI device and prints the status
k3conf disable clock <dev_id> <clk_id>
Disables the TISCI clock and prints the status
k3conf set clock <dev_id> <clk_id> <freq>
Sets the clock frequency and prints the status
k3conf read <addr>
Prints the value at the specified io memory
k3conf write <addr> <val>
Writes the value at the specified io memory
Best Regards,
Keerthy