Part Number: 66AK2G12
Other Parts Discussed in Thread: EVMK2GX,
There are several related posts which seem to indicate that the EVMK2GX either 1) does NOT support booting from eMMC:
or 2) that it MAY support booting from the eMMC:
I have had no success getting it working and am looking for a definitive answer to the following:
1) can the EVMK2GX board boot directly from the eMMC (assuming the resistor/switch strapping is correct)? If YES, is there a set of instructions for the EVMK2GX specifically?
2) if the EVMK2GX can NOT boot from the eMMC - what is the underlying issue? Is it an issue with the 66AK2G12 itself, or an issue with the EVMK2GX board?
thanks,
Jeremy