Hello,
I'm evaluating the opportunity to move a project I work on, from Linux PSP 03.20.00.14 to the most recent PSP 03.21.00.03.
One point I'm concerned with is the MMC/SD driver performance, since we use SD for both system boot and data acquisition.
By comparing "Device Driver Features and Performance Guide" for both PSP releases (links [1] and [2] respectively) it appears that throughput performance have dropped on the OMAP-L138 by more than 60%. This may perhaps be due to different testing conditions, that do not show up from the table anyway. Since I noticed from the same benchmark pages that other drivers also seem to suffer of performance drops, I'm asking if anyone had the opportunity to compare the two PSP performances, especially with respect to MMC/SD functionality.
If such a degradation is confirmed, is there any known reason for that? Anyway if this is the case, I'd probably drop the idea to migrate to the most recent kernel.
Thank you in advance,
Regards,
Andrea
Links: