Part Number: TDA4VM
I'm attempting rerun calibration inference on the pre-trained YOLO X human pose estimation model in Model Zoo and then write a custom post processing function that adds on the the keypoints+skeleton drawing for judging the pose itself.
#!/usr/bin/env python
# coding: utf-8
# In[1]:
import os
import re
import sys
import cv2
import tqdm
import onnx
import math
import copy
import shutil
import platform
import itertools
import numpy as np
import onnxruntime as rt
import ipywidgets as widgets
import matplotlib.pyplot as plt
import matplotlib.patches as mpatches
from pathlib import Path
from munkres import Munkres
from numpy.lib.stride_tricks import as_strided
from IPython.display import Markdown as md
from PIL import Image, ImageFont, ImageDraw, ImageEnhance
from scripts.utils import imagenet_class_to_name, download_model, loggerWritter, get_svg_path, get_preproc_props, single_img_visualise
# In[2]:
def preprocess_for_onnx_pose_estimation(image_path, size, mean, scale, layout, reverse_channels, pad_color=114, pad_type="center"):
# Step 1
# read the image using openCVimport json_tricks as json
img = cv2.imread(image_path)
# Step 2
# convert to RGB
img = img[:,:,::-1]
# Step 3
# Most of the onnx models are trained using
# 512x512 images. The general rule of thumb
# is to scale the input image while preserving
# the original aspect ratio so that the
# longer edge is 512 pixels, and then
# pad the scaled image to 512x512
size = (size,size) if not isinstance(size, (list,tuple)) else size
desired_size = size[-1]
old_size = img.shape[:2] # old_size is in (height, width) format
ratio = float(desired_size)/max(old_size)
new_size = tuple([int(x*ratio) for x in old_size])
# new_size should be in (width, height) format
img = cv2.resize(img, (new_size[1], new_size[0]))
delta_w = size[1] - new_size[1]
delta_h = size[0] - new_size[0]
if pad_type=="corner":
top, left = 0, 0
bottom, right = delta_h, delta_w
else:
delta_w = size[1] - new_size[1]
delta_h = size[0] - new_size[0]
top, bottom = delta_h//2, delta_h-(delta_h//2)
left, right = delta_w//2, delta_w-(delta_w//2)
img = cv2.copyMakeBorder(img, top, bottom, left, right, cv2.BORDER_CONSTANT,
value=pad_color)
# Step 4
# Apply scaling and mean subtraction.
# if your model is built with an input
# normalization layer, then you might
# need to skip this
if mean is not None and scale is not None:
img = img.astype('float32')
for mean, scale, ch in zip(mean, scale, range(img.shape[2])):
img[:,:,ch] = ((img.astype('float32')[:,:,ch] - mean) * scale)
# Step 5
if reverse_channels:
img = img[:,:,::-1]
# Step 6
img = np.expand_dims(img,axis=0)
img = np.transpose(img, (0, 3, 1, 2))
return img, top, left, ratio
# In[3]:
calib_images = [
'sample-images/yoga0.jpg',
'sample-images/yoga1.bmp',
'sample-images/yoga2.bmp',
]
output_dir = '../custom-artifacts-temp/onnx/yolox_s_pose_ti_lite_49p5_78p0.onnx'
#onnx_model_path_TDA4VM = '/opt/model_zoo/ONR-KD-7060-human-pose-yolox-s-640x640/model/yolox_s_pose_ti_lite_49p5_78p0.onnx'
#onnx_model_path_EdgeAIcloud = '/home/root/notebooks/model-zoo/models/vision/keypoint/coco/edgeai-yolox/yolox_s_pose_ti_lite_49p5_78p0.onnx'
onnx_model_path_EdgeAIcloud = '/home/root/notebooks/prebuilt-models/8bits/kd-7060_onnxrt_coco_edgeai-yolox_yolox_s_pose_ti_lite_49p5_78p0_onnx/model/yolox_s_pose_ti_lite_49p5_78p0.onnx'
onnx.shape_inference.infer_shapes_path(onnx_model_path_EdgeAIcloud, onnx_model_path_EdgeAIcloud)
#compilation options - knobs to tweak
num_bits =8
accuracy =1
log_dir = Path("logs").mkdir(parents=True, exist_ok=True)
# stdout and stderr saved to a *.log file.
with loggerWritter("logs/custon-model-onnx"):
# model compilation options
compile_options = {
'tidl_tools_path' : os.environ['TIDL_TOOLS_PATH'],
'artifacts_folder' : output_dir,
'tensor_bits' : num_bits,
'accuracy_level' : accuracy,
'advanced_options:calibration_frames' : len(calib_images),
'advanced_options:calibration_iterations' : 3, # used if accuracy_level = 1
'debug_level' : 1,
'deny_list' : "MaxPool" #Comma separated string of operator types as defined by ONNX runtime, ex "MaxPool, Concat"
}
# create the output dir if not present
# clear the directory
os.makedirs(output_dir, exist_ok=True)
for root, dirs, files in os.walk(output_dir, topdown=False):
[os.remove(os.path.join(root, f)) for f in files]
[os.rmdir(os.path.join(root, d)) for d in dirs]
# In[4]:
# create & compile model with compile options specified above
so = rt.SessionOptions()
EP_list = ['TIDLCompilationProvider','CPUExecutionProvider']
sess = rt.InferenceSession(onnx_model_path_EdgeAIcloud ,providers=EP_list, provider_options=[compile_options, {}], sess_options=so)
input_details = sess.get_inputs()
print('input_details: ', input_details)
output_details = sess.get_outputs()
print('output_details: ', output_details)
label = 'ONR-KD-7060-human-pose-yolox-s-640x640'
pad_color = 128 if 'ae' in label and 'yolo' not in label else 114
pad_type = "corner" if 'yolox' in label else "center"
size = 640
mean = [0.0, 0.0, 0.0]
scale = [1.0, 1.0, 1.0]
layout = 0
reverse_channels = True
# run inference for each calibration image
for num in tqdm.trange(len(calib_images)):
#output = list(sess.run(None, {input_details[0].name : preprocess_for_onnx_pose_estimation(calib_images[num], size, mean, scale, layout, reverse_channels, pad_color, pad_type)}))[0]
image_name = calib_images[num]
print('label = ', label)
print('pad_color = ', pad_color)
print('pad_type = ', pad_type)
print('image_name = ', image_name)
processed_image, top, left, ratio = preprocess_for_onnx_pose_estimation(image_name, size, mean, scale, layout, reverse_channels, pad_color, pad_type)
print('processed_image', processed_image)
print('top', top)
print('left', left)
print('ratio', ratio)
if not input_details[0].type == 'tensor(float)':
processed_image = np.uint8(processed_image)
image_size = processed_image.shape[3]
print('image_size = ', image_size)
out_file=None
output=None
output = list(sess.run(None, {input_details[0].name : processed_image})) #[0]
print('output = ', output)
#%matplotlib inline
#output_image = single_img_visualise(output, image_size, calib_images[num], out_file, top, left, ratio, udp=True, thickness=2, radius=5, label=label)
# plot the outut using matplotlib
#plt.rcParams["figure.figsize"]=20,20
#plt.rcParams['figure.dpi'] = 200 # 200 e.g. is really fine, but slower
#plt.imshow(output_image)
#plt.show()
# In[5]:
# subgraphs visualization for debugging
subgraph_link =get_svg_path(output_dir)
for sg in subgraph_link:
hl_text = os.path.join(*Path(sg).parts[4:])
sg_rel = os.path.join('../', sg)
display(md("[{}]({})".format(hl_text,sg_rel)))
# In[6]:
root_src_dir = output_dir
root_dst_dir = 'custom-artifacts/onnx/yolox_s_pose_ti_lite_49p5_78p0.onnx'
for src_dir, dirs, files in os.walk(root_src_dir):
dst_dir = src_dir.replace(root_src_dir, root_dst_dir, 1)
if not os.path.exists(dst_dir):
os.makedirs(dst_dir)
for file_ in files:
src_file = os.path.join(src_dir, file_)
dst_file = os.path.join(dst_dir, file_)
if os.path.exists(dst_file):
os.remove(dst_file)
shutil.copy(src_file, dst_dir)
# In[7]:
del so
print('closed calibration inference session...')
# In[8]:
# use compiled image for inference
out_file=None
image_name = 'sample-images/yoga0.jpg'
delegate_options = {
'artifacts_folder': './custom-artifacts/onnx/yolox_s_pose_ti_lite_49p5_78p0.onnx'
}
print('delegate_options: ', delegate_options)
# In[9]:
so0 = rt.SessionOptions()
EP_list = ['TIDLCompilationProvider','CPUExecutionProvider']
print('EP_list: ', EP_list)
# In[ ]:
sess0 = rt.InferenceSession(onnx_model_path_EdgeAIcloud ,providers=EP_list, provider_options=[delegate_options, {}], sess_options=so0)
print('session0 started')
# In[ ]:
input_details0 = sess0.get_inputs()
print('input_details0: ', input_details0)
# In[ ]:
processed_image, top, left, ratio = preprocess_for_onnx_pose_estimation(image_name, size, mean, scale, layout, reverse_channels, pad_color, pad_type)
if not input_details[0].type == 'tensor(float)':
processed_image = np.uint8(processed_image)
image_size = processed_image.shape[3]
output0 = list(sess0.run(None, {input_details0[0].name : processed_image}))[0]
# In[ ]:
# post processing
get_ipython().run_line_magic('matplotlib', 'inline')
output_image = single_img_visualise(output0, image_size, image_name, out_file, top, left, ratio, udp=True, thickness=2, radius=5, label=label)
# plot the outut using matplotlib
plt.rcParams["figure.figsize"]=20,20
plt.rcParams['figure.dpi'] = 200 # 200 e.g. is really fine, but slower
plt.imshow(output_image)
plt.show()
double free or corruption (!prev)