This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Forum,
I have a histogram running on the C7x core of the TDA4vm, I would like to add a timestamp to the histogram collected so that we can synchronize this capture with external equipment measurements. I was looking to use something like clock_gettime so that I can get down to the milliseconds range. That call is not available, I was wondering if there is another call that could be used to achieve this or if there was a way to get the timestamp from the RTC.
Thank You,
- George
George,
You can use the C7x's TSC to do so. (__TSC; 1ns resolution for c7x clocked @ 1GHz)
Regards,
Varun