This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Some problems with the official SDK compiling MCU

Genius 13655 points

Part Number: TDA4VM

Hello Champs,

On Jacinto 7 evaluation board + J721S2XSOMG01EVM SOM board, customer tried to compile mcu2 based on ti-processor-sdk-rtos-j721e-evm-08_02_00_05 SDK with "make vx_app_rtos_linux_mcu2_0 -j16". The mcu2_0 image was pushed into the board with ssh /lib/firmware/vision_apps_evm and then rebooted, but it didn't start. 

By the way, customer wanted to know where is the default output of the print function "appLogPrintf" in the MCU core and where can he see it, and why can't he see the print log of the MCU in the out-of-the-box mcu uart?

Thank you very much!

Thanks
Regards
Shine