Part Number: PROCESSOR-SDK-AM62X
Dear TI supporter,
I have run example mcan from mcu_plus_sdk_am62x_08_05_00_14 for CAN0.
This example is running with:
- MCU_MCAN0_CLKSEL_CLK_SEL is utilized MCU_PLL0_HSDIV4_CLKOUT
- The input clock frequency of MCU_MCAN0 that get in MCU_PLL0 is 80MHz
Currently I need to measure "Total bit rate tolerance [%]" and "PLL-tolerance[%]" value
I think this parameters are provided by TI, so can you give me this parameters or if not is there a way to do or calculate this parameters with.
Best regards,
Hieu