Part Number: AM625
The MCU UART RX pin cannot receive any signal, but the RX signal can be tested correctly by the oscilloscope, AM6254 chip cannot receive it. MCU UART TX pin can transmit signals that can be recognized by the computer. When MCU UART RX pin is set to normal GPIO output, it can output up and down signal normally. We also try to add 10k resistor on RX signal and pull it up to 3.3V, there is no change. What may be the reason for this? The board design is referred to PROC142. Thank you.