Tool/software:
Hi all,
We are trying to connect an SD card to the MMC2 Port on our system, we have enabled the sdhci2 on your device tree, but it seems it is not working , i mean when card is connected we are not able to detect in the linux. we are able to see mmc2 driver is loaded in the kernal boot logs, but whenever we connect the SD card, it is not detected.
below are the Device tree added in our system:
by default 3.3v is provided to the SD card. we are able to see 1.8V on the SD_CD when the card is not detected and when connected it goes LOW.
sdhci2: mmc@fa20000 { compatible = "ti,am62-sdhci"; reg = <0x00 0x0fa20000 0x00 0x1000>, <0x00 0x0fa28000 0x00 0x400>; interrupts = <GIC_SPI 82 IRQ_TYPE_LEVEL_HIGH>; power-domains = <&k3_pds 184 TI_SCI_PD_EXCLUSIVE>; clocks = <&k3_clks 184 5>, <&k3_clks 184 6>; clock-names = "clk_ahb", "clk_xin"; bus-width = <4>; ti,clkbuf-sel = <0x7>; ti,otap-del-sel-legacy = <0x8>; ti,otap-del-sel-sd-hs = <0x0>; ti,otap-del-sel-sdr12 = <0x0>; ti,otap-del-sel-sdr25 = <0x0>; ti,otap-del-sel-sdr50 = <0x8>; ti,otap-del-sel-sdr104 = <0x7>; ti,otap-del-sel-ddr50 = <0x8>; ti,itap-del-sel-legacy = <0xa>; ti,itap-del-sel-sd-hs = <0xa>; ti,itap-del-sel-sdr12 = <0xa>; ti,itap-del-sel-sdr25 = <0x1>; status = "disabled"; }; /* On-module Wi-Fi on WB SKUs, module-specific SDIO otherwise */ pinctrl_sdhci2: main-mmc2-pins-default { pinctrl-single,pins = < AM62X_IOPAD(0x120, PIN_INPUT, 0) /* (C24) MMC2_CMD */ /* WiFi_SDIO_CMD */ AM62X_IOPAD(0x118, PIN_INPUT, 0) /* (D25) MMC2_CLK */ /* WiFi_SDIO_CLK */ AM62X_IOPAD(0x114, PIN_INPUT, 0) /* (B24) MMC2_DAT0 */ /* WiFi_SDIO_DATA0 */ AM62X_IOPAD(0x110, PIN_INPUT, 0) /* (C25) MMC2_DAT1 */ /* WiFi_SDIO_DATA1 */ AM62X_IOPAD(0x10c, PIN_INPUT, 0) /* (E23) MMC2_DAT2 */ /* WiFi_SDIO_DATA2 */ AM62X_IOPAD(0x108, PIN_INPUT, 0) /* (D24) MMC2_DAT3 */ /* WiFi_SDIO_DATA3 */ AM62X_IOPAD(0x11c, PIN_INPUT, 0) /* (#N/A) MMC2_CLKB */ AM62X_IOPAD(0x0124, PIN_INPUT_PULLUP, 7) /* (A23) MMC2_SDCD.GPIO0_71 */ >; }; /* MMC2 */ &sdhci2 { pinctrl-names = "default"; pinctrl-0 = <&pinctrl_sdhci2>; cd-gpios = <&main_gpio0 71 GPIO_ACTIVE_LOW>; disable-wp; ti,driver-strength-ohm = <50>; ti,fails-without-test-cd; status = "okay"; };