This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
we are trying to boot from SD card using the MMC2 port.we have done the changes in the device tree as below,
};
/* On-module Wi-Fi on WB SKUs, module-specific SDIO otherwise */ pinctrl_sdhci2: main-mmc2-pins-default { pinctrl-single,pins = < AM62X_IOPAD(0x120, PIN_INPUT, 0) /* (C24) MMC2_CMD */ /* WiFi_SDIO_CMD */ AM62X_IOPAD(0x118, PIN_INPUT, 0) /* (D25) MMC2_CLK */ /* WiFi_SDIO_CLK */ AM62X_IOPAD(0x114, PIN_INPUT, 0) /* (B24) MMC2_DAT0 */ /* WiFi_SDIO_DATA0 */ AM62X_IOPAD(0x110, PIN_INPUT, 0) /* (C25) MMC2_DAT1 */ /* WiFi_SDIO_DATA1 */ AM62X_IOPAD(0x10c, PIN_INPUT, 0) /* (E23) MMC2_DAT2 */ /* WiFi_SDIO_DATA2 */ AM62X_IOPAD(0x108, PIN_INPUT, 0) /* (D24) MMC2_DAT3 */ /* WiFi_SDIO_DATA3 */ AM62X_IOPAD(0x11c, PIN_INPUT, 0) /* (#N/A) MMC2_CLKB */ >; }; /* Verdin SD_2_CD# as GPIO */ pinctrl_sd2_cd_gpio: main-gpio0-71-pins-default { pinctrl-single,pins = < AM62X_IOPAD(0x0124, PIN_INPUT_PULLUP, 7) /* (A23) MMC2_SDCD.GPIO0_71 */ /* SODIMM 157 */ >; }; &sdhci2 { pinctrl-names = "default"; pinctrl-0 = <&pinctrl_sdhci2>, <&pinctrl_sd2_cd_gpio>; cd-gpios = <&main_gpio1 71 GPIO_ACTIVE_LOW>; disable-wp; ti,fails-without-test-cd; ti,driver-strength-ohm = <33>; status = "okay"; };
we bitbake .wic image and write it into external Sd card using Sudo DD commad.
the issue is that when i try to boot from Sd card using mmc2.
in u-boot when i use the commad mmc dev 2, it returns an error stating No MMC 2 device found.
is there anything wrong in the above config or suggest me a way to boot from MMC2!
Thanks in advance.
Hello,
The SD card connector is interfaced to MMC1 port on TI AM62x EVM. Have you connected the connector to MMC2 port on your board?
Can you also clarify if you have made the changes in the U-Boot or Kernel device trees? If you could share the modifications in git diff format that would be helpful.
Thanks!
Hi, we have connected the SD card to MMC2 port , and the above are changes added to the kernel device tree file and one more change is that currenlty we have disabled the sdhci1m usb1 and usb2 in kernel device tree.
there is no change made in u-boot
Hi, could you please help clarify the following queries?
Also, since you haven't changed the U-Boot device trees, the U-Boot expectedly will not identify any MMC2 device.
we have designed a custom board in which the SD card boot is from MMC2, is it possible to boot from MMC2.
if i update the u-boot device tree to add MMC2, will it boot from MMC2
we have designed a custom board in which the SD card boot is from MMC2, is it possible to boot from MMC2.
The ROM cannot boot the `tiboot3.bin` from the SD card interfaced to MMC2 port.
Hi,
Thanks for the reply.
As you said we cannot boot sd card from the mmc2. We have tried multiple options. But I believe we can use that port to connect a sd card which should detect as normal sd card under lsblk.
Will this be possible?
Hello,
Will this be possible?
Yes, but on paper. The TRM does mention the MMC1/2 ports are designed to work with both SD or SDIO devices.
However, we have not tested the SD card interfaced to MMC2. There are also no reported instances of any other customer testing the same.
Regards,
Prashant