Other Parts Discussed in Thread: 4460
Hi all,
I use the http://omappedia.com/wiki/4AI.1.4_OMAP4_Icecream_Sandwich_Panda_Notes for my 4460 panda board. Everything is good. But I want to boot panda board from MMC2. So I use J3 expansion connector that according to the block:
I also configure SYSBOOT pin of OMAP to boot according to order of peripheral : USB-UART-MMC1-MMC2. I user usb4boot (http://pandaboard.org/content/usb-downloader-and-usb-second-stage-bootloader-omap4) to boot uboot into omap4460. When I’m in uboot, I use “mmc_init 1” command to start SD card. But the initialization is fail and I cann’t read or write the SD card use uboot command.
Help me!
Thank you for your help and reply.
Best regards!