Hello,
We have the EVMC6670L assembled with TMDXEVMPCI AMC-PCIe adapter card, set up for PCI-e boot using switch settings, and installed in a HP x8600 workstation server class PC running Fedora 10 Linux. We've followed the procedures as documented in the PCIe Boot Example that came with MCSDK 2.00.00.11 release (mcsdk_2_00_00_11\tools\boot_loader\examples\pcie\docs\README.pdf). Specifically, here are the steps we've followed:
- updated IBL following the Step 1 "Programming IBL on the EEPROM at bus address 0x51" procedures in the boot loader instructions for evmc6670
- set EVM to PCIE boot via switch setting
switch pin1 2 3 4
SW3: off on on off
SW4: on on on on
SW5: on on on off
SW6: off on on on
SW9: on
However, the Linux PC does not enumerate the PCIe device at all. Please help!
Regards,
James