Part Number: AM4376
Hello,
I am trying to run EIP demo code on IDk board but it is not working as expected to communicate with EIP molex tool as suggested.
PFA.
Version:
AM4376: PRU-ICSS-EthernetIP_Adapter_01.00.03.04 patch applicability to sdk version
change wireshark log extension to .pcapng
� M<+ �������� 8 AMD Ryzen 5 PRO 4650U with Radeon Graphics (with SSE4.2) % 64-bit Windows 10 (2009), build 19044 2 Dumpcap (Wireshark) 3.4.5 (v3.4.5-0-g7db1feb42ce9) � � 2 \Device\NPF_{68BEBA26-BAEB-4A39-9EB9-EB8ABE2BF013} Ethernet % 64-bit Windows 10 (2009), build 19044 � d U� �0�vB B �j]Ռ���� E 4S�@ �#[��d��
�d����� ���^� � d d U� �u�vB B �j]Ռ���� E 4S�@ �#Z��d��
�d����� ���^� � d d U� ��vB B �j]Ռ���� E 4S�@ �#Y��d��
�d����� ���^� � d L U� ���v* * �j]Ռ���� �������d�j]���
L L U� �� w* * �j]Ռ���� �������d�j]���
L L U� PBw* * �j]Ռ���� �������d�j]���
L � U� Ww� � 33 �������`u. u�� �A�-]�r� "# u�� 'q������� ��� '