Part Number: TDA4AL-Q1
Other Parts Discussed in Thread: TCAN1043
hi Ti team,
our device is a CAN wakeup device. when there is no activity on the CAN bus, TDA4 need configure the EN and STB of the TJA1043 and it will enter the sleep mode, so, the 3.3V power will be shoutdown by the INH pin of TJA1043, to keep the whole device shutdown mode power consumption to be under 0.25mA. there are some questions need to be confirmed, please help me to check it.
1) is there any risk for the TDA4 system if TDA4 inform TJA1043 shutdown the 3.3V power for TDA4 system?
2)what state does the TDA4 system need to get in to be ready to inform TJA1043 to shutdown the 3.3V power?
3) can we come to the conclusion that there is no risk for the TDA4 system because of the to safe power down sequence of the TDA4 system?