Part Number: TDA2P-ACD
Dear TI colleague,
i have several questions regarding the Display subsystem (DSS) module.
1st question:
I only found DSS can support output up to 1080p @60fps via HDMI in datasheet.
My concern is if TDA2P-ACD can support the video output via parallel link with the following parameter:
Resolution&fps&Type: 2672*1936 @9fps YUV 422 (blanking about 20% additional)
Basically the pixel clock will be around 111MHz
btw. is there a specific limit scope on the DSS parallel output horizontal/vertical pixel like 1920x1080 60fps? or its just related to pixel clock.
2nd question:
I wanna ask if parallel video output can be switched directly from 1920*1080@60fps to 1200*800@30fps when device power supply is ON ?
or this kind of output switch need reinitialization of system?
Look forward to your reply
BR