This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6442: one MDIO link for both CPSW and ICSSG interface

Part Number: AM6442


(reposted because of formatting isssue ...)

Hello,

Same question than Victorien, 

Can an MDIO interface be connected to both CPSW and ICGSSG ?

For instance, to control CPSW RGMII2 and PRU/ICSSG1 MII0     (while having also ICSSG0 RGMII1 & 2  and its own MDIO)

If so is it better to run the code from the PRU side or from an A core  ?

Best regard