Part Number: TDA4AH-Q1
Other Parts Discussed in Thread: TDA4VH
Hi,
I came upon this post and wanted to confirm the solution that was given within. Specifically on the allowable choices of DDR sub systems when not all of them are in use. Based on the response to this post it is a requirement for the TDA4VH to use the DDR sub systems in order so DDRSS0 and then if two are needed it would be DDRSS0 and DDRSS1 and so on. Meaning the use of only DDRSS1 and DDRSS3 would not be possible. Is this stated in the datasheet or TRM and I missed this requirement upon my initial pass? I only came upon this as the DDR Register configuration tool only allows these DDRSS combinations. Any clarification would be appreciated.
Best,
Chris