Part Number: TDA4VM
Hello Ti,
I am using the functions available on the PDK 8.6 example udma:memcpy_test.c for NAVSS MCU UDMA-P to transfer data between the PCIe Controller and a local buffer in MCU OCRAM.
The example with the buffers allocated there works fine.
If I replace the source or destination buffer by my local buffer in MCU OCRAM, the DMA transfer also works.
Buf if I replace the source or destination buffer by the PCIe buffer it fails, throwing a data exception.
Are there extra steps to configure UDMA for PCIe? Is there any example available?
Thank you and Regards,
Marina