Part Number: AM623
SPI data pins are named as D0 and D1. Where can i find information about the usage regarding in/output or which one is MISO / MOSI?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM623
SPI data pins are named as D0 and D1. Where can i find information about the usage regarding in/output or which one is MISO / MOSI?

Hello Martin Stelter
Thank you for the query.
Please refer to the below explanation and the sections in the TRM.
5.4.1.4.1 SPI Bootloader Operation
Please refer to Section 5.4.1 for more information that applies to SPI boot mode
The SPI boot mode supports the 1S-1S-1S mode only. The Read Command is 8-bits (0x03) followed by a 24 bit (3 byte) address. There are no dummy cycles issued after the read command. The frequency of operation supported is 6.250 MHz. OSPI0_D0 will have data transfers FROM the processor TO the flash device, and OSPI0_D1 will have data transfers TO the processor FROM the flash device
12.2.3.2.1 Basic MCSPI Pins for Controller Mode
12.2.3.2.2 Basic MCSPI Pins for Peripheral Mode
Pls let me know if this helps.
Regards,
Sreenivasa