Part Number: TDA4VH-Q1
Other Parts Discussed in Thread: CSD18543Q3A, CSD18563Q5A, LM5143
51 Reference design power MOSFET selection: 1, whether CSD18563Q5A has a vehicle model, the same question CSD18543Q3A 2, if not, the same package (the same application environment), TI has no alternative recommendation
52 Reference circuit LM5143 two power supplies: VOUT1/VOUT2 output current detection, without requiring high accuracy, can the sense resistor R165 be removed, directly sampling at both ends of the power inductor L22, what are the disadvantages?
What does the cross-resistance R150 and R151 on the differential sampling path do, and can they be removed? See screenshot
53 Reference Design: Is SoC Supply Noise Speaking purely for the convenience of testing power supply ripple close to the load pins? Another test method tests the ripple across the capacitance on the back of the load pins. What is the difference between the two methods
See screenshot
54 The JTAG schematic uses 60PIN, can I directly use a connector with only JTAG debug signals?
55 OCULINK interface definitions need to be given a copy
56 Reference Design Multiphase Power Far/Near Feedback: PCB Reference Design Selects Remote Feedback, Sampling Selects One, R208&R203 Combination or R205&R201 - What is the role of series resistance, the role of resistance is only network transformation?
The GOSNS of frequency compensation COMP takes the remote feedback ground, that is, the SOC PWR is close to GND - what is the purpose?

57 Reference Design Power Supply LM5143: Series Resistors on the Differential Sampling Path, What Does It Do?
58 Reference Design Power Supply LM5143: What is the purpose of introducing current sensing separately in parallel branches, and reintroducing current sensing after merging?