This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6442: Signal configuration on Single Chip Servo Motor Control

Part Number: AM6442


Hi

Is it possible to send "PRG0_ECAP0_IN_APWM_OUT" signal from the same PRU slice at the same time while the PRU slice is processing EnDat2.2? 

 

According to

      https://www.ti.com/lit/an/sprad03/sprad03.pdf

      https://www.ti.com/lit/zip/sprad03

 

It seems that the signal "PRG0_ECAP0_IN_APWM_OUT" (Ball U5, Signal name PRG0_PRU1_GPIO15, MuxMode10)

 

is output from PRU_ICSSG0 slice1.

  

And, this signal is connected to SN74AXC4T245PWT on TIDEP-01015 3-axis adapter board.

 

 

At the same time, PRU_ICSSG0 slice0 could be using to handle EnDat2.2.

   

I believe that "PRG0_ECAP0_IN_APWM_OUT" signal can only be output at GPIO mode.

 

And, EnDat2.2 could be running on MII mode.

Is it possible to send "PRG0_ECAP0_IN_APWM_OUT" signals from the same PRU slice at the same time while the PRU slice is processing EnDat2.2? 

How does the "www.ti.com/.../sprad03.pdf" work