Part Number: AM5729
Hi,
We are developing a custom board with AM5729 processor. Boot Mode is set to SD card - MMC.
We have taken the IDK Eval kit as a reference . We are using only EMIF1(1GB - 32bit data) in our design.
Whereas in eval card there are both EMIF1(1GB - 32bit) and EMIF2(1GB - 32bit) available in that .Also it works in interleaved mode.
In our design, We have to implemented test code to test in non-interleaved mode(Modified the GEL file in CCS). It is working.
Please suggest the suitable DDR configurations that are needed to be modifed in Uboot for linux.