Part Number: AM62A7
Firstly,I use tiboot3.bin to boot my SOC.
The tiboot3.bin is build from SBL_EMMC_Stage1 example of SDK.
The MCU firmware is the helloworld example of SDK.
The MCU firmware is load ok.And it entry address is right.Also I use CCS debug the MCU firmware,the mcu firmware can run,but it stuck in sciclient get messages sentences.
sysFW is in tiboot3.bin and SOC M4 ROM will load run it,as I know.Is it wrong?In boot flow M4 have 180sec Watchdog.When is it closed by whose?
All the log and operations of mine is shown as follows: