Part Number: AM68A
Other Parts Discussed in Thread: CDCE6214, DS90UB953-Q1
I’ve got a question to AM68A in conjunction with a DS90UB953.
We have a display with a DS90UB914A deserializer. Both datasheets mentioned that they are compatible with each other. We require DVP mode in DS90UB953.
My Question is: How do we synchronize the clock between CSI from AM68A and DS90UB953? In SNLA270A (Backwards capability Modes) at page 6, note 2 it is mentioned that the input clock in DVP mode shall be synchronized with CSI clock. Since the processor does not have an input pin for synchronization we have a problem. We could not use the “same” clock frequency in AM68A CSI and external oscillator cause they are not synchronized.
One approach is the usage of a e.g CDCE6214 and route the CSI clock from processor over this IC to the DS90UB953 serializer and derive a synchronized input clock.
Or does this paragraph “only” mean, the input clock at serializer side and the PCLK at deserializer side are the same frequency and "unrelated" to CSI clock. (Functional block diagram, 7.2 in 953 Datasheet).
Have we misunderstood this paragraph or is there a much smarter solution?