Other Parts Discussed in Thread: SYSCONFIG
Hello,
From TRM rev G page 8526, about DS signal
"(2) Used for HS400 mode (MMCSD0 Only);" ==> DataStrobe OK but in the previous page 8525
"12.3.5.1.2 MMCSD Not Supported Features
MMCSD0 Host Controller:
•
Multi-Media Card:
– 3.3 V, 3.0 V and 1.2 V
– Secure Digital Card and SDIO
– Muxing of other LVCMOS interfaces onto the MMCSD interface at the SoC level
– HS400 DDR: • 1.8 V, 0-200 MHz, 8-bit bus width, 400 MBps"
I conclude that you tried to implement HS400 mode w/o success, and for now HS400 is not available.
So MMC0_DS (G19) signal is useless, but it is still present is the sysconfig tool rev1.17,
should I unselect G19 and avoid to route (ball-out) this signal to save some space in my layout ?
or will you try again to implement it in a SR3 version ?
BR
Thanks.