This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] AM3352: Number of assigned MAC addresses

Part Number: AM3352


Hi,

I read on the forums (https://e2e.ti.com/support/processors-group/processors/f/processors-forum/166910/am335x-efuse-mac-ids-always-valid/609758#609758) that any AM335x device has either 2 or 3 MAC addresses programmed to them. According to the linked thread it is only ZCZ packages with PRU-ICSS that have 3, all other have 2 MAC addresses.

In a very limited test run on my end I have checked the configuration on a ZCE packaged AM3352 (i.e. no PRU-ICSS) and can see that 3 address are flashed. I know this as the macid0 is signifying the lower range and that macid1 is the higher range of assigned MAC addresses.

macid 0: b8:80:4f:ec:81:72
macid 1: b8:80:4f:ec:81:74

Can you confirm that actually all AM335x devices (or at least ZCE packaged AM3352) have 3 MAC addresses assigned and that it will continue to be that way?

Best regards

Måns