Part Number: TDA4VM

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VM

Hi,
Please let me know which application are you running? Is this a out-of-the-box SDK demo or your custom demo?
I see that the CSI logs are from MCU2_1 whereas in the SDK, it would come from MCU2_0.
Hence, could you brief me what are the changes done in the SDK?
Also, could you share me all the logs ( app logs + logs of "source ./vision_apps_init.sh") in .txt file?
Regards,
Nikhil
hi
In our PSDKRA, DMPAC is allocated to mcu2_1. This is done to balance to load between mcu2_0 and mcu2_1. mcu2_1 runs capture, isp, msc, ldc, display and AEWB algorithm. mcu2_0 runs dmpac and ethernet firmware.
Now the following error appears:

log:
Inside the script--------- [MCU2_0] 4.170848 s: CIO: Init ... Done !!! [MCU2_0] 4.170920 s: ### CPU Frequency = 1000000000 Hz [MCU2_0] 4.170962 s: APP: Init ... !!! [MCU2_0] 4.170987 s: SCICLIENT: Init ... !!! [MCU2_0] 4.172095 s: SCICLIENT: DMSC FW version [21.9.1--v2021.09a (Terrific Lla] [MCU2_0] 4.172146 s: SCICLIENT: DMSC FW revision 0x15 [MCU2_0] 4.172179 s: SCICLIENT: DMSC FW ABI revision 3.1 [MCU2_0] 4.172220 s: SCICLIENT: Init ... Done !!! [MCU2_0] 4.172247 s: UDMA: Init ... !!! [MCU2_0] 4.181850 s: UDMA: Init ... Done !!! [MCU2_0] 4.181913 s: MEM: Init ... !!! [MCU2_0] 4.181956 s: MEM: Created heap (DDR_SHARED_MEM, id=0, flags=0x00000004) @ d9000000 of size 16777216 bytes !!! [MCU2_0] 4.182031 s: MEM: Created heap (L3_MEM, id=1, flags=0x00000000) @ 3600000 of size 262144 bytes !!! [MCU2_0] 4.182090 s: MEM: Init ... Done !!! [MCU2_0] 4.183209 s: FVID2: Init ... !!! [MCU2_0] 4.183304 s: FVID2: Init ... Done !!! [MCU2_0] 4.183357 s: CSI2RX: Init ... !!! [MCU2_0] 4.189068 s: CSI2RX: Init ... Done !!! [MCU2_0] 4.189131 s: CSI2TX: Init ... !!! [MCU2_0] 4.193729 s: CSI2TX: Init ... Done !!! [MCU2_0] 4.193790 s: IPC: Init ... !!! [MCU2_0] 4.193854 s: IPC: 8 CPUs participating in IPC !!! [MCU2_0] 4.193912 s: IPC: Waiting for HLOS to be ready ... !!! [MCU2_0] 14.127412 s: IPC: HLOS is ready !!! [MCU2_0] 14.162663 s: IPC: Init ... Done !!! [MCU2_0] 14.598498 s: REMOTE_SERVICE: Init ... !!! [MCU2_0] 14.601215 s: REMOTE_SERVICE: Init ... Done !!! [MCU2_0] 14.601294 s: DSS: Init ... !!! [MCU2_0] 14.601327 s: DSS: Display type is eDP !!! [MCU2_0] 14.601357 s: DSS: M2M Path is enabled !!! [MCU2_0] 14.601386 s: DSS: SoC init ... !!! [MCU2_0] 14.647900 s: DSS: SoC init ... Done !!! [MCU2_0] 14.647950 s: DSS: Board init ... !!! [MCU2_0] 14.647981 s: DSS: Board init ... Done !!! [MCU2_0] 14.667097 s: DSS: Init ... Done !!! [MCU2_0] 14.667173 s: VHWA: DMPAC: Init ... !!! [MCU2_0] 14.668526 s: VHWA: DOF Init ... !!! [MCU2_0] 14.720094 s: VHWA: DOF Init ... Done !!! [MCU2_0] 14.720174 s: VHWA: DMPAC: Init ... Done !!! [MCU2_0] 14.720228 s: VX_ZONE_INIT:Enabled [MCU2_0] 14.720261 s: VX_ZONE_ERROR:Enabled [MCU2_0] 14.720288 s: VX_ZONE_WARNING:Enabled [MCU2_0] 14.722237 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target DMPAC_SDE [MCU2_0] 14.722477 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target DMPAC_DOF [MCU2_0] 14.722705 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target IPU1-1 [MCU2_0] 14.722761 s: VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!! [MCU2_0] 14.722799 s: APP: OpenVX Target kernel init ... !!! [MCU2_0] 14.723646 s: APP: OpenVX Target kernel init ... Done !!! [MCU2_0] 14.723699 s: UDMA Copy: Init ... !!! [MCU2_0] 14.736071 s: UDMA Copy: Init ... Done !!! [MCU2_0] 14.736149 s: ETHFW: Init ... !!! [MCU2_0] 14.773296 s: ETHFW: Shared multicasts (software fanout): [MCU2_0] 14.773376 s: 01:00:5e:7f:03:01 [MCU2_0] 14.773434 s: 01:00:5e:0a:00:03 [MCU2_0] 14.773480 s: 01:00:5e:0a:00:01 [MCU2_0] 14.773525 s: 01:00:5e:40:ff:fb [MCU2_0] 14.773568 s: ff:ff:ff:ff:ff:ff [MCU2_0] 14.773613 s: ETHFW: Reserved multicasts: [MCU2_0] 14.773639 s: 01:80:c2:00:00:0e [MCU2_0] 14.773683 s: 01:1b:19:00:00:00 [MCU2_0] 14.773917 s: EnetMcm: CPSW_9G on MAIN NAVSS [MCU2_0] 14.794407 s: PHY 1 is alive [MCU2_0] 14.794831 s: Mdio_ioctl: PHY 1 is not configured for C22 access [MCU2_0] 14.794910 s: EnetPhyMdioDflt_readC22: PHY 1: Failed to read C22 reg: -12 [MCU2_0] 14.795209 s: EnetPhy_bindDriver: PHY 1: OUI:2b8094 Model:03 Ver:02 <-> 'bcm89881' : OK [MCU2_0] 14.796973 s: [MCU2_0] ETHFW Version : 0.02.00 [MCU2_0] 14.797046 s: ETHFW Build Date: Sep 11, 2023 [MCU2_0] 14.797084 s: ETHFW Build Time: 16:52:46 [MCU2_0] 14.797118 s: ETHFW Commit SHA: 103e7367 [MCU2_0] 14.797193 s: ETHFW: Init ... DONE !!! [MCU2_0] 14.797224 s: ETHFW: Remove server Init ... !!! [MCU2_0] 14.797287 s: cfg->numVirtPorts is 2 [MCU2_0] 14.797336 s: virtPorts 9 is mac port, and phy port is 9 [MCU2_0] 14.797549 s: CpswProxyServer: Virtual port configuration: [MCU2_0] 14.797606 s: mpu_1_0 <-> Switch port 0: mpu_1_0_ethswitch-device-0 [MCU2_0] 14.797657 s: mpu_1_0 <-> MAC port 6: mpu_1_0_ethmac-device-6 [MCU2_0] 14.798662 s: CpswProxyServer: initialization completed (core: mcu2_0) [MCU2_0] 14.798728 s: ETHFW: Remove server Init ... DONE !!! [MCU2_0] 14.799996 s: Starting lwIP, local interface IP is dhcp-enabled [MCU2_0] 14.826704 s: Host MAC address: 70:ff:76:1d:92:63 [MCU2_0] 14.837670 s: [LWIPIF_LWIP] Enet LLD netif initialized successfully [MCU2_0] 14.864781 s: Function:CpswProxyServer_attachExtHandlerCb,HostId:0,CpswType:6,VirPort:0 [MCU2_0] 14.868890 s: [LWIPIF_LWIP_IC] Interface started successfully [MCU2_0] 14.869078 s: [LWIPIF_LWIP_IC] NETIF INIT SUCCESS [MCU2_0] 14.878986 s: APP: Init ... Done !!! [MCU2_0] 14.879044 s: APP: Run ... !!! [MCU2_0] 14.879069 s: APP: Run ... Done !!! [MCU2_0] 14.900435 s: [LWIPIF_LWIP_IC] Interface started successfully [MCU2_0] 14.900510 s: [LWIPIF_LWIP_IC] NETIF INIT SUCCESS [MCU2_0] 14.900624 s: Added interface 'br4', IP is 0.0.0.0 [MCU2_0] 14.958291 s: Function:CpswProxyServer_attachExtHandlerCb,HostId:0,CpswType:6,VirPort:9 [MCU2_1] 4.328260 s: CIO: Init ... Done !!! [MCU2_1] 4.328333 s: ### CPU Frequency = 1000000000 Hz [MCU2_1] 4.328393 s: APP: Init ... !!! [MCU2_1] 4.328423 s: SCICLIENT: Init ... !!! [MCU2_1] 4.329585 s: SCICLIENT: DMSC FW version [21.9.1--v2021.09a (Terrific Lla] [MCU2_1] 4.329637 s: SCICLIENT: DMSC FW revision 0x15 [MCU2_1] 4.329673 s: SCICLIENT: DMSC FW ABI revision 3.1 [MCU2_1] 4.329712 s: SCICLIENT: Init ... Done !!! [MCU2_1] 4.329739 s: UDMA: Init ... !!! [MCU2_1] 4.341688 s: UDMA: Init ... Done !!! [MCU2_1] 4.341753 s: MEM: Init ... !!! [MCU2_1] 4.341802 s: MEM: Created heap (DDR_SHARED_MEM, id=0, flags=0x00000004) @ da000000 of size 16777216 bytes !!! [MCU2_1] 4.341880 s: MEM: Created heap (L3_MEM, id=1, flags=0x00000001) @ 3640000 of size 262144 bytes !!! [MCU2_1] 4.341941 s: MEM: Init ... Done !!! [MCU2_1] 4.341968 s: FVID2: Init ... !!! [MCU2_1] 4.342039 s: FVID2: Init ... Done !!! [MCU2_1] 4.342089 s: ISS: Init ... !!! [MCU2_1] 4.342324 s: ISX031 in used [MCU2_1] 4.342443 s: ar0233 not in used [MCU2_1] 6.046999 s: IssSensor_Init ... Done !!! [MCU2_1] 6.047087 s: IPC: Init ... !!! [MCU2_1] 6.047187 s: IPC: 8 CPUs participating in IPC !!! [MCU2_1] 6.047257 s: IPC: Waiting for HLOS to be ready ... !!! [MCU2_1] 14.180077 s: IPC: HLOS is ready !!! [MCU2_1] 14.211023 s: IPC: Init ... Done !!! [MCU2_1] 14.598497 s: REMOTE_SERVICE: Init ... !!! [MCU2_1] 14.601310 s: REMOTE_SERVICE: Init ... Done !!! [MCU2_1] 14.601431 s: vissRemoteServer_Init ... Done !!! [MCU2_1] 14.601502 s: IttRemoteServer_Init ... Done !!! [MCU2_1] 14.601537 s: VHWA: VPAC Init ... !!! [MCU2_1] 14.603384 s: VHWA: LDC Init ... !!! [MCU2_1] 14.663893 s: VHWA: LDC Init ... Done !!! [MCU2_1] 14.663978 s: VHWA: MSC Init ... !!! [MCU2_1] 14.737078 s: VHWA: MSC Init ... Done !!! [MCU2_1] 14.737146 s: VHWA: NF Init ... !!! [MCU2_1] 14.746353 s: VHWA: NF Init ... Done !!! [MCU2_1] 14.746425 s: VHWA: VISS Init ... !!! [MCU2_1] 14.788485 s: VHWA: VISS Init ... Done !!! [MCU2_1] 14.788554 s: VHWA: VPAC Init ... Done !!! [MCU2_1] 14.788604 s: VX_ZONE_INIT:Enabled [MCU2_1] 14.788636 s: VX_ZONE_ERROR:Enabled [MCU2_1] 14.788664 s: VX_ZONE_WARNING:Enabled [MCU2_1] 14.790592 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target IPU1-0 [MCU2_1] 14.790841 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target VPAC_NF [MCU2_1] 14.791085 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target VPAC_LDC1 [MCU2_1] 14.791307 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target VPAC_MSC1 [MCU2_1] 14.791576 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target VPAC_MSC2 [MCU2_1] 14.791889 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target VPAC_VISS1 [MCU2_1] 14.792181 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target CAPTURE1 [MCU2_1] 14.792467 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target CAPTURE2 [MCU2_1] 14.792752 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target DISPLAY1 [MCU2_1] 14.793034 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target DISPLAY2 [MCU2_1] 14.793274 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target CSITX [MCU2_1] 14.793573 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target CAPTURE3 [MCU2_1] 14.793855 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target CAPTURE4 [MCU2_1] 14.794150 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target CAPTURE5 [MCU2_1] 14.794433 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target CAPTURE6 [MCU2_1] 14.794708 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target CAPTURE7 [MCU2_1] 14.794998 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target CAPTURE8 [MCU2_1] 14.795247 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target DSS_M2M1 [MCU2_1] 14.795498 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target DSS_M2M2 [MCU2_1] 14.795729 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target DSS_M2M3 [MCU2_1] 14.795971 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:54] Added target DSS_M2M4 [MCU2_1] 14.796029 s: VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!! [MCU2_1] 14.796067 s: APP: OpenVX Target kernel init ... !!! [MCU2_1] 14.811834 s: APP: OpenVX Target kernel init ... Done !!! [MCU2_1] 14.811901 s: UDMA Copy: Init ... !!! [MCU2_1] 14.823183 s: UDMA Copy: Init ... Done !!! [MCU2_1] 14.823252 s: APP: Init ... Done !!! [MCU2_1] 14.823323 s: APP: Run ... !!! [MCU2_1] 14.823349 s: APP: Run ... Done !!! [MCU2_1] 15.816652 s: VX_ZONE_ERROR:[tivxTargetKernelInstanceAlloc:115] kernel com.ti.capture has not been registered on this CPU [MCU2_1] 15.816729 s: VX_ZONE_ERROR:[tivxTargetKernelInstanceAlloc:116] Please register this kernel on the appropriate target core [MCU2_1] 15.816796 s: VX_ZONE_ERROR:[tivxTargetNodeDescNodeCreate:761] target_kernel_instance is NULL [MCU2_1] 15.918102 s: ImageSensor_RemoteServiceHandler: IM_SENSOR_CMD_STREAM_ON [MCU2_1] 15.918195 s: sensor: ISX031-MAX96717F stream on start ... [MCU2_0] 17.098837 s: Function:CpswProxyServer_setPromiscModeHandlerCb,HostId:0,Handle:a32cd97c,CoreKey:38acb7e6,mode:disable [MCU2_0] 17.099403 s: Function:CpswProxyServer_setPromiscModeHandlerCb,HostId:0,Handle:a32cd97c,CoreKey:38acb7e6,mode:disable [MCU2_1] 17.322118 s: VX_ZONE_ERROR:[tivxTargetKernelInstanceAlloc:115] kernel com.ti.capture has not been registered on this CPU [MCU2_1] 17.322201 s: VX_ZONE_ERROR:[tivxTargetKernelInstanceAlloc:116] Please register this kernel on the appropriate target core [MCU2_1] 17.322268 s: VX_ZONE_ERROR:[tivxTargetNodeDescNodeCreate:761] target_kernel_instance is NULL [MCU2_1] 17.423411 s: ImageSensor_RemoteServiceHandler: IM_SENSOR_CMD_PWROFF
Please tell me how to fix this error, thank you
In our PSDKRA, DMPAC is allocated to mcu2_1. This is done to balance to load between mcu2_0 and mcu2_1. mcu2_1 runs capture, isp, msc, ldc, display and AEWB algorithm. mcu2_0 runs dmpac and ethernet firmware.
This is not exactly correct. mcu2_0 runs capture, isp, msc ldc and mcu2_1 runs dmpac. So we cannot enable capture on mcu2_1 in the released sdk.
Regards,
Brijesh
Our current approach is to run capture, isp, msc ldc on mcu2_1, but now the following error appears
[MCU2_1] 15.816652 s: VX_ZONE_ERROR:[tivxTargetKernelInstanceAlloc:115] kernel com.ti.capture has not been registered on this CPU
[MCU2_1] 15.816729 s: VX_ZONE_ERROR:[tivxTargetKernelInstanceAlloc:116] Please register this kernel on the appropriate target core
[MCU2_1] 15.816796 s: VX_ZONE_ERROR:[tivxTargetNodeDescNodeCreate:761] target_kernel_instance is NULL
[MCU2_1] 15.918102 s: ImageSensor_RemoteServiceHandler: IM_SENSOR_CMD_STREAM_ON
Please tell me how to fix it, thanks
But have you made any changes in the code to move capture and other components to mcu2_1? By default it isnot supported.
Regards,
Brijesh
Hello, I just changed some common configurations of the code, as follows
app_cfg_mcu2_0.h
app_cfg_mcu2_1.h
tivx_platform_psdk_j7.h
rm_cfg.c
Which component codes still need to be modified? I want to discuss, exchange and learn with the master, thank you very much
Hi,
Could you may be provide a patch over the SDK which contains your changes for moving capture to MCU2_1?
Also additionally the below error would come if you have not done the target side registration of capture node on MCU2_1
[MCU2_1] 15.816652 s: VX_ZONE_ERROR:[tivxTargetKernelInstanceAlloc:115] kernel com.ti.capture has not been registered on this CPU
[MCU2_1] 15.816729 s: VX_ZONE_ERROR:[tivxTargetKernelInstanceAlloc:116] Please register this kernel on the appropriate target core
i.e. I think you should enable ENABLE_CSI2RX on app_cfg_mcu2_1.h and disable in app_cfg_mcu2_0.h.
Regards,
Nikhil
HI TI
Thanks for the support. Next, I will spend time studying the TDA4 visual technology solution. After I have a better understanding, I will ask your company for advice. Thank you for your previous support.
Sure, Thank you. Closing this thread until then. Please respond here within 30 days to reopen this thread. Else you could open a new thread referencing to this one.
Regards,
Nikhil