Part Number: AM6412
Hi Experts
i have booted our custom board with am6412 soc using base rootfs image,but when i am trying with default image ,rootfs got stucked,can you suggest some points to debug
i am attaching logs
U-Boot SPL 2021.01-g2ee8efd654 (Sep 02 2023 - 07:39:46 +0000) EEPROM not available at 80, trying to read at 81 Reading on-board EEPROM at 0x51 failed 1 SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar') SPL initial stack usage: 13424 bytes Trying to boot from MMC1 Authentication passed Authentication passed Authentication passed Authentication passed init_env from device 9 not supported! Starting ATF on ARM64 core... NOTICE: BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty NOTICE: BL31: Built : 07:22:02, Aug 31 2023 I/TC: I/TC: OP-TEE version: 3.20.0 (gcc version 9.2.1 20191025 (GNU Toolchain for the A-profile Architecture 9.2-2019. 12 (arm-9.10))) #1 Thu Aug 31 07:22:07 UTC 2023 aarch64 I/TC: WARNING: This OP-TEE configuration might be insecure! I/TC: WARNING: Please check optee.readthedocs.io/.../porting_guidelines.html I/TC: Primary CPU initializing I/TC: SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar') I/TC: HUK Initialized I/TC: Activated SA2UL device I/TC: Enabled firewalls for SA2UL TRNG device I/TC: SA2UL TRNG initialized I/TC: SA2UL Drivers initialized I/TC: Primary CPU switching to normal world boot U-Boot SPL 2021.01-g2ee8efd654 (Sep 02 2023 - 07:39:41 +0000) EEPROM not available at 80, trying to read at 81 Reading on-board EEPROM at 0x51 failed 1 SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar') Trying to boot from MMC1 Authentication passed Authentication passed U-Boot 2021.01-g2ee8efd654 (Sep 02 2023 - 07:39:41 +0000) SoC: AM64X SR2.0 HS-FS Model: Texas Instruments AM642 EVM EEPROM not available at 80, trying to read at 81 Reading on-board EEPROM at 0x51 failed 1 DRAM: 2 GiB NAND: 0 MiB MMC: mmc@fa10000: 0, mmc@fa00000: 1 Loading Environment from FAT... Unable to use mmc 0:1... In: serial@2800000 Out: serial@2800000 Err: serial@2800000 EEPROM not available at 80, trying to read at 81 Reading on-board EEPROM at 0x51 failed 1 Net: No ethernet found. Hit any key to stop autoboot: 0 => setenv bootpart 0:2 => boot switch to partitions #0, OK mmc0(part 0) is current device SD/MMC found on device 0 Failed to load 'boot.scr' ** Unrecognized filesystem type ** 19147264 bytes read in 107 ms (170.7 MiB/s) 55185 bytes read in 2 ms (26.3 MiB/s) ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 000000008feef000, end 000000008fffffff ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] [ 0.000000] Linux version 5.10.168-g2c23e6c538 (oe-user@oe-host) (aarch64-none-linux-gnu-gcc (GNU Toolchain f or the A-profile Architecture 9.2-2019.12 (arm-9.10)) 9.2.1 20191025, GNU ld (GNU Toolchain for the A-profile Ar chitecture 9.2-2019.12 (arm-9.10)) 2.33.1.20191209) #1 SMP PREEMPT Mon Sep 11 13:37:39 UTC 2023 [ 0.000000] Machine model: TI VVDN 5WRU Board [ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '') [ 0.000000] printk: bootconsole [ns16550a0] enabled [ 0.000000] efi: UEFI not found. [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a1100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a2000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a2100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a3000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a3000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a3100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a3100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node m4f-dma-memory@a4000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node m4f-memory@a4100000, compatible id shared-dma-pool [ 0.000000] Zone ranges: [ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff] [ 0.000000] DMA32 empty [ 0.000000] Normal empty [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000080000000-0x000000009e7fffff] [ 0.000000] node 0: [mem 0x000000009e800000-0x00000000a57fffff] [ 0.000000] node 0: [mem 0x00000000a5800000-0x00000000ffffffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffffff] [ 0.000000] cma: Reserved 512 MiB at 0x00000000dd000000 [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: Trusted OS migration not required [ 0.000000] psci: SMC Calling Convention v1.2 [ 0.000000] percpu: Embedded 22 pages/cpu s51288 r8192 d30632 u90112 [ 0.000000] Detected VIPT I-cache on CPU0 [ 0.000000] CPU features: detected: ARM erratum 845719 [ 0.000000] CPU features: detected: GIC system register CPU interface [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 516096 [ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=fc40000. spi.0:1m(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),256k(ospi.env),256k(ospi.env.backup),57088k@8m(ospi.rootfs ),256k(ospi.phypattern);omap2-nand.0:2m(NAND.tiboot3),2m(NAND.tispl),2m(NAND.tiboot3.backup),4m(NAND.u-boot),256 k(NAND.u-boot-env),256k(NAND.u-boot-env.backup),-(NAND.file-system) root=PARTUUID=a072ccc7-391a-034b-b370-9187b4 6822ff rw rootfstype=ext4 rootwait [ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear) [ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] Memory: 1398792K/2097152K available (11200K kernel code, 1162K rwdata, 4308K rodata, 1920K init, 431K bss, 174072K reserved, 524288K cma-reserved) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] rcu: RCU event tracing is enabled. [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2. [ 0.00
0000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] Tracing variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 256 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] GICv3: Distributor has no Range Selector support
[ 0.000000] GICv3: 16 PPIs implemented
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001840000
[ 0.000000] ITS [mem 0x01820000-0x0182ffff]
[ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[ 0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[ 0.000000] ITS@0x0000000001820000: allocated 524288 Devices @80800000 (flat, esz 8, psz 64K, shr 0)
[ 0.000000] ITS: using cache flushing for cmd queue
[ 0.000000] GICv3: using LPI property table @0x0000000080030000
[ 0.000000] GIC: using cache flushing for LPI property table
[ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000080040000
[ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 4407
95210634 ns
[ 0.000006] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[ 0.008598] Console: colour dummy device 80x25
[ 0.013197] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=8
00000)
[ 0.023874] pid_max: default: 32768 minimum: 301
[ 0.028706] LSM: Security Framework initializing
[ 0.033501] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.041078] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.051178] rcu: Hierarchical SRCU implementation.
[ 0.056476] Platform MSI: msi-controller@1820000 domain created
[ 0.062907] PCI/MSI: /bus@f4000/interrupt-controller@1800000/msi-controller@1820000 domain created
[ 0.072212] EFI services will not be available.
[ 0.077157] smp: Bringing up secondary CPUs ...
I/TC: Secondary CPU 1 initializing
I/TC: Secondary CPU 1 switching to normal world boot
[ 0.090797] Detected VIPT I-cache on CPU1
[ 0.090843] GICv3: CPU1: found redistributor 1 region 0:0x0000000001860000
[ 0.090858] GICv3: CPU1: using allocated LPI pending table @0x0000000080050000
[ 0.090931] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.091073] smp: Brought up 1 node, 2 CPUs
[ 0.120460] SMP: Total of 2 processors activated.
[ 0.125274] CPU features: detected: 32-bit EL0 Support
[ 0.130548] CPU features: detected: CRC32 instructions
[ 0.144306] CPU: All CPU(s) started at EL2
[ 0.148512] alternatives: patching kernel code
[ 0.154389] devtmpfs: initialized
[ 0.166488] KASLR disabled due to lack of seed
[ 0.171316] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.181292] futex hash table entries: 512 (order: 3, 32768 bytes, linear)
[ 0.206918] pinctrl core: initialized pinctrl subsystem
[ 0.213038] DMI not present or invalid.
[ 0.217814] NET: Registered protocol family 16
[ 0.224325] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
[ 0.231733] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.239836] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.248658] thermal_sys: Registered thermal governor 'step_wise'
[ 0.248666] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.255318] cpuidle: using governor menu
[ 0.266310] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.273330] ASID allocator initialised with 65536 entries
[ 0.309693] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.316591] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.323444] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.330292] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.338605] cryptd: max_cpu_qlen set to 1000
[ 0.346773] k3-chipinfo 43000014.chipid: Family:AM64X rev:SR2.0 JTAGID[0x1bb3802f] Detected
[ 0.356078] vsys_5v0: supplied by evm_12v0
[ 0.360964] vsys_3v3: supplied by evm_12v0
[ 0.365822] vdd_mmc1: supplied by vsys_3v3
[ 0.370620] vddb_3v3_display: supplied by vsys_3v3
[ 0.376911] iommu: Default domain type: Translated
[ 0.382399] SCSI subsystem initialized
[ 0.386985] mc: Linux media interface: v0.10
[ 0.391395] videodev: Linux video capture interface: v2.00
[ 0.397110] pps_core: LinuxPPS API ver. 1 registered
[ 0.402185] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.411528] PTP clock support registered
[ 0.415573] EDAC MC: Ver: 3.0.0
[ 0.419758] omap-mailbox 29020000.mailbox: omap mailbox rev 0x66fc9100
[ 0.426715] omap-mailbox 29040000.mailbox: omap mailbox rev 0x66fc9100
[ 0.433535] omap-mailbox 29060000.mailbox: omap mailbox rev 0x66fc9100
[ 0.441170] FPGA manager framework
[ 0.444784] Advanced Linux Sound Architecture Driver Initialized.
[ 0.452295] clocksource: Switched to clocksource arch_sys_counter
[ 0.458834] VFS: Disk quotas dquot_6.6.0
[ 0.462921] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.476614] NET: Registered protocol family 2
[ 0.481398] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.490515] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
[ 0.499332] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 0.507567] TCP bind hash table entries: 16384 (order: 6, 262144 bytes, linear)
[ 0.515369] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.522344] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.529250] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.536781] NET: Registered protocol family 1
[ 0.541926] RPC: Registered named UNIX socket transport module.
[ 0.548012] RPC: Registered udp transport module.
[ 0.552822] RPC: Registered tcp transport module.
[ 0.557634] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.564226] NET: Registered protocol family 44
[ 0.568784] PCI: CLS 0 bytes, default 64
[ 0.573671] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
[ 0.586911] Initialise system trusted keyrings
[ 0.591811] workingset: timestamp_bits=46 max_order=19 bucket_order=0
[ 0.602975] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.609798] NFS: Registering the id_resolver key type
[ 0.615112] Key type id_resolver registered
[ 0.619419] Key type id_legacy registered
[ 0.623607] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.630461] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.638282] 9p: Installing v9fs 9p2000 file system support
[ 0.687601] Key type asymmetric registered
[ 0.691816] Asymmetric key parser 'x509' registered
[ 0.696868] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[ 0.704441] io scheduler mq-deadline registered
[ 0.709071] io scheduler kyber registered
[ 0.715840] pinctrl-single 4084000.pinctrl: 33 pins, size 132
[ 0.722376] pinctrl-single f4000.pinctrl: 180 pins, size 720
[ 0.729380] pinctrl-single a40000.timesync-router: 512 pins, size 2048
[ 0.746953] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 0.771183] brd: module loaded
[ 0.783309] loop: module loaded
[ 0.787732] megasas: 07.714.04.00-rc1
[ 0.796825] tun: Universal TUN/TAP device driver, 1.6
[ 0.802874] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[ 0.809329] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 0.815463] sky2: driver version 1.30
[ 0.820540] VFIO - User Level meta-driver version: 0.3
[ 0.827243] i2c /dev entries driver
[ 0.832640] sdhci: Secure Digital Host Controller Interface driver
[ 0.838986] sdhci: Copyright(c) Pierre Ossman
[ 0.844332] sdhci-pltfm: SDHCI platform and OF driver helper
[ 0.851478] ledtrig-cpu: registered to indicate activity on CPUs
[ 0.858176] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 0.866748] optee: probing for conduit method.
I/TC: Reserved shared memory is enabled
I/TC: Dynamic shared memory is enabled
I/TC: Normal World virtualization support is disabled
I/TC: Asynchronous notifications are disabled
[ 0.871405] optee: revision 3.20 (8e74d476)
[ 0.888126] optee: dynamic shared memory is enabled
[ 0.897894] optee: initialized driver
[ 0.902302] gpio-mux: probe of mux-controller failed with error -2
[ 0.911147] NET: Registered protocol family 17
[ 0.915967] 9pnet: Installing 9P2000 support
[ 0.920457] Key type dns_resolver registered
[ 0.925366] Loading compiled-in X.509 certificates
[ 0.949760] ti-sci 44043000.dmsc: lpm region is required for suspend but not provided.
[ 0.957993] ti-sci 44043000.dmsc: ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar')
[ 1.019790] omap-gpmc 3b000000.memory-controller: GPMC revision 6.0
[ 1.026283] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[ 1.036227] omap_i2c 4900000.i2c: bus 0 rev0.12 at 400 kHz
[ 1.043439] omap_i2c 20000000.i2c: bus 1 rev0.12 at 100 kHz
[ 1.051199] omap_i2c 20010000.i2c: bus 2 rev0.12 at 400 kHz
[ 1.058420] omap_i2c 20020000.i2c: bus 3 rev0.12 at 100 kHz
[ 1.065530] omap_i2c 20030000.i2c: bus 4 rev0.12 at 100 kHz
[ 1.071798] ti-sci-intr bus@f4000:bus@4000000:interrupt-controller1: Interrupt Router 5 domain created
[ 1.081572] ti-sci-intr bus@f4000:interrupt-controller0: Interrupt Router 3 domain created
[ 1.090410] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created
[ 1.114301] j721e-pcie f102000.pcie: host bridge /bus@f4000/pcie@f102000 ranges:
[ 1.121945] j721e-pcie f102000.pcie: IO 0x0068001000..0x0068010fff -> 0x0068001000
[ 1.130243] j721e-pcie f102000.pcie: MEM 0x0068011000..0x006fffffff -> 0x0068011000
[ 1.138534] j721e-pcie f102000.pcie: IB MEM 0x0000000000..0x0fffffffff -> 0x0000000000
[ 2.150672] j721e-pcie f102000.pcie: PCI host bridge to bus 0000:00
[ 2.157146] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 2.162761] pci_bus 0000:00: root bus resource [io 0x0000-0xffff] (bus address [0x68001000-0x68010fff])
[ 2.172453] pci_bus 0000:00: root bus resource [mem 0x68011000-0x6fffffff]
[ 2.179526] pci 0000:00:00.0: [104c:b010] type 01 class 0x060400
[ 2.185684] pci 0000:00:00.0: reg 0x10: [mem 0x00000000-0xfffffffff 64bit pref]
[ 2.193236] pci 0000:00:00.0: supports D1
[ 2.197336] pci 0000:00:00.0: PME# supported from D0 D1 D3hot
[ 2.206039] pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[ 2.216715] pci_bus 0000:01: busn_res: [bus 01-ff] end is updated to 01
[ 2.223525] pci 0000:00:00.0: BAR 0: no space for [mem size 0x1000000000 64bit pref]
[ 2.231443] pci 0000:00:00.0: BAR 0: failed to assign [mem size 0x1000000000 64bit pref]
[ 2.239720] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 2.245414] pcieport 0000:00:00.0: PME: Signaling with IRQ 45
[ 2.252184] ti-udma 485c0100.dma-controller: Number of rings: 68
[ 2.259756] ti-udma 485c0100.dma-controller: Channels: 24 (bchan: 12, tchan: 6, rchan: 6)
[ 2.270151] ti-udma 485c0000.dma-controller: Number of rings: 288
[ 2.285117] ti-udma 485c0000.dma-controller: Channels: 44 (tchan: 29, rchan: 15)
[ 2.296416] printk: console [ttyS2] disabled
[ 2.300883] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 17, base_baud = 3000000) is a 8250
[ 2.309651] printk: console [ttyS2] enabled
[ 2.309651] printk: console [ttyS2] enabled
[ 2.318095] printk: bootconsole [ns16550a0] disabled
[ 2.318095] printk: bootconsole [ns16550a0] disabled
[ 2.332708] spi-nor spi0.0: unrecognized JEDEC id bytes: 00 00 00 00 00 00
[ 2.339635] spi-nor: probe of spi0.0 failed with error -2
[ 2.358684] davinci_mdio 8000f00.mdio: Configuring MDIO in manual mode
[ 2.404297] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 2.411874] davinci_mdio 8000f00.mdio: no live phy, scanning all
[ 2.446069] davinci_mdio 8000f00.mdio: phy[0]: device 8000f00.mdio:00, driver unknown
[ 2.453997] davinci_mdio 8000f00.mdio: phy[1]: device 8000f00.mdio:01, driver unknown
[ 2.461825] davinci_mdio 8000f00.mdio: phy[2]: device 8000f00.mdio:02, driver unknown
[ 2.469652] davinci_mdio 8000f00.mdio: phy[3]: device 8000f00.mdio:03, driver unknown
[ 2.477475] davinci_mdio 8000f00.mdio: phy[4]: device 8000f00.mdio:04, driver unknown
[ 2.485296] davinci_mdio 8000f00.mdio: phy[5]: device 8000f00.mdio:05, driver unknown
[ 2.493117] davinci_mdio 8000f00.mdio: phy[6]: device 8000f00.mdio:06, driver unknown
[ 2.500938] davinci_mdio 8000f00.mdio: phy[7]: device 8000f00.mdio:07, driver unknown
[ 2.508759] davinci_mdio 8000f00.mdio: phy[8]: device 8000f00.mdio:08, driver unknown
[ 2.516580] davinci_mdio 8000f00.mdio: phy[9]: device 8000f00.mdio:09, driver unknown
[ 2.524402] davinci_mdio 8000f00.mdio: phy[10]: device 8000f00.mdio:0a, driver unknown
[ 2.532315] davinci_mdio 8000f00.mdio: phy[11]: device 8000f00.mdio:0b, driver unknown
[ 2.540224] davinci_mdio 8000f00.mdio: phy[12]: device 8000f00.mdio:0c, driver unknown
[ 2.548139] davinci_mdio 8000f00.mdio: phy[13]: device 8000f00.mdio:0d, driver unknown
[ 2.556048] davinci_mdio 8000f00.mdio: phy[14]: device 8000f00.mdio:0e, driver unknown
[ 2.563958] davinci_mdio 8000f00.mdio: phy[15]: device 8000f00.mdio:0f, driver unknown
[ 2.571878] davinci_mdio 8000f00.mdio: phy[16]: device 8000f00.mdio:10, driver unknown
[ 2.579887] davinci_mdio 8000f00.mdio: phy[17]: device 8000f00.mdio:11, driver unknown
[ 2.587797] davinci_mdio 8000f00.mdio: phy[18]: device 8000f00.mdio:12, driver unknown
[ 2.595709] davinci_mdio 8000f00.mdio: phy[19]: device 8000f00.mdio:13, driver unknown
[ 2.603619] davinci_mdio 8000f00.mdio: phy[20]: device 8000f00.mdio:14, driver unknown
[ 2.611527] davinci_mdio 8000f00.mdio: phy[21]: device 8000f00.mdio:15, driver unknown
[ 2.619435] davinci_mdio 8000f00.mdio: phy[22]: device 8000f00.mdio:16, driver unknown
[ 2.627344] davinci_mdio 8000f00.mdio: phy[23]: device 8000f00.mdio:17, driver unknown
[ 2.635251] davinci_mdio 8000f00.mdio: phy[24]: device 8000f00.mdio:18, driver unknown
[ 2.643159] davinci_mdio 8000f00.mdio: phy[25]: device 8000f00.mdio:19, driver unknown
[ 2.651067] davinci_mdio 8000f00.mdio: phy[26]: device 8000f00.mdio:1a, driver unknown
[ 2.658979] davinci_mdio 8000f00.mdio: phy[27]: device 8000f00.mdio:1b, driver unknown
[ 2.666887] davinci_mdio 8000f00.mdio: phy[28]: device 8000f00.mdio:1c, driver unknown
[ 2.674794] davinci_mdio 8000f00.mdio: phy[29]: device 8000f00.mdio:1d, driver unknown
[ 2.682703] davinci_mdio 8000f00.mdio: phy[30]: device 8000f00.mdio:1e, driver unknown
[ 2.690619] davinci_mdio 8000f00.mdio: phy[31]: device 8000f00.mdio:1f, driver unknown
[ 2.698740] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA00903, cpsw version 0x6
BA80903 Ports: 3 quirks:00000006
[ 2.711662] am65-cpsw-nuss 8000000.ethernet: /bus@f4000/ethernet@8000000/ethernet-ports/port@1 read phy-mode
err -22
[ 2.724795] am65-cpsw-nuss: probe of 8000000.ethernet failed with error -22
[ 2.734025] am65-cpts 39000000.cpts: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:0
[ 2.743265] k3-j72xx-soc-thermal b00000.temperature-sensor: invalid resource
[ 2.750396] k3-j72xx-soc-thermal: probe of b00000.temperature-sensor failed with error -22
[ 2.761892] mmc0: CQHCI version 5.10
[ 2.765151] mmc1: CQHCI version 5.10
[ 2.781898] debugfs: Directory 'pd:114' with parent 'pm_genpd' already present!
[ 2.801909] ALSA device list:
[ 2.804931] No soundcards found.
[ 2.807139] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit
[ 2.882406] mmc0: Command Queue Engine enabled
[ 2.886915] mmc0: new high speed MMC card at address 0001
[ 2.893137] mmcblk0: mmc0:0001 8GTF4R 7.28 GiB
[ 2.897879] mmcblk0boot0: mmc0:0001 8GTF4R partition 1 4.00 MiB
[ 2.903948] mmcblk0boot1: mmc0:0001 8GTF4R partition 2 4.00 MiB
[ 2.910147] mmcblk0rpmb: mmc0:0001 8GTF4R partition 3 512 KiB, chardev (237:0)
[ 2.920438] mmcblk0: p1 p2 p4
[ 4.291255] sdhci-am654 fa00000.mmc: Power on failed
[ 4.326879] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit
[ 4.956781] EXT4-fs (mmcblk0p2): recovery complete
[ 4.962181] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 4.970369] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 4.976548] devtmpfs: mounted
[ 4.981097] Freeing unused kernel memory: 1920K
[ 4.985761] Run /sbin/init as init process
[ 5.153688] systemd[1]: System time before build time, advancing clock.
[ 5.217067] NET: Registered protocol family 10
[ 5.222836] Segment Routing with IPv6
[ 5.261273] systemd[1]: systemd 244.5+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +S
YSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 def
ault-hierarchy=hybrid)
[ 5.283610] systemd[1]: Detected architecture arm64.
Welcome to Arago 2021.09!
[ 5.321304] systemd[1]: Set hostname to <am64xx-evm>.
[ 5.330293] random: systemd: uninitialized urandom read (16 bytes read)
[ 5.337049] systemd[1]: Initializing machine ID from random generator.
[ 5.653371] systemd[1]: Configuration file /etc/systemd/system/vvdn_init.service is marked executable. Please
remove executable permission bits. Proceeding anyway.
[ 5.702087] systemd[1]: /lib/systemd/system/startwlansta.service:7: Unknown key name 'After' in section 'Serv
ice', ignoring.
[ 5.714997] systemd[1]: /lib/systemd/system/startwlanap.service:7: Unknown key name 'After' in section 'Servi
ce', ignoring.
[ 5.751228] systemd[1]: /lib/systemd/system/irqbalanced.service:6: Unknown key name 'ConditionCPUs' in sectio
n 'Unit', ignoring.
[ 5.793024] systemd[1]: /lib/systemd/system/docker.socket:6: ListenStream= references a path below legacy dir
ectory /var/run/, updating /var/run/docker.sock �→ /run/docker.sock; please update the unit file accordingly.
[ 5.943026] random: systemd: uninitialized urandom read (16 bytes read)
[ 5.954878] systemd[1]: Created slice system-getty.slice.
[ OK ] Created slice system-getty.slice.
[ 5.976599] random: systemd: uninitialized urandom read (16 bytes read)
[ 5.985736] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ 6.010885] systemd[1]: Created slice system-syslog\x2dng.slice.
[ OK ] Created slice system-syslog\x2dng.slice.
[ 6.034876] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 6.057037] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password �…ts to Console Directory Watch.
[ 6.080926] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password R�…uests to Wall Directory Watch.
[ 6.104867] systemd[1]: Reached target Paths.
[ OK ] Reached target Paths.
[ 6.124644] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 6.144629] systemd[1]: Reached target Slices.
[ OK ] Reached target Slices.
[ 6.164655] systemd[1]: Reached target Swap.
[ OK ] Reached target Swap.
[ 6.208527] systemd[1]: Listening on RPCbind Server Activation Socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ 6.232791] systemd[1]: Reached target RPC Port Mapper.
[ OK ] Reached target RPC Port Mapper.
[ 6.258756] systemd[1]: Listening on Process Core Dump Socket.
[ OK ] Listening on Process Core Dump Socket.
[ 6.281103] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ 6.309411] systemd[1]: Condition check resulted in Journal Audit Socket being skipped.
[ 6.318521] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 6.340681] random: systemd: uninitialized urandom read (16 bytes read)
[ 6.348135] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 6.369139] random: systemd: uninitialized urandom read (16 bytes read)
[ 6.376461] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 6.400683] random: systemd: uninitialized urandom read (16 bytes read)
[ 6.408193] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 6.429202] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 6.459113] systemd[1]: Mounting Huge Pages File System...
Mounting Huge Pages File System...
[ 6.486866] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 6.514897] systemd[1]: Mounting Kernel Debug File System...
Mounting Kernel Debug File System...
[ 6.543275] systemd[1]: Mounting Temporary Directory (/tmp)...
Mounting Temporary Directory (/tmp)...
[ 6.571843] systemd[1]: Starting Create list of static device nodes for the current kernel...
Starting Create list of st�…odes for the current kernel...
[ 6.602947] systemd[1]: Starting RPC Bind...
Starting RPC Bind...
[ 6.616954] systemd[1]: Condition check resulted in File System Check on Root Device being skipped.
[ 6.635004] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 6.662081] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 6.683147] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems 6.696175] cryptodev: loading out-of-tree module taints
kernel.
[0m...
[ 6.723298] systemd[1]: Starting udev Coldplug all Devices...
Starting udev Coldplug all Devices...
[ 6.757050] cryptodev: driver 1.10 loaded.
[ 6.762688] systemd[1]: Started RPC Bind.
[ OK ] Started RPC Bind.
[ 6.777749] systemd[1]: Mounted Huge Pages File System.
[ 6.779807] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[ OK ] Mounted Huge Pages File System.
[ 6.809319] systemd[1]: Mounted POSIX Message Queue File System.
[ OK ] Mounted POSIX Message Queue File System.
[ 6.840932] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Mounted Temporary Directory (/tmp).
[ OK ] Started Create list of sta�… nodes for the current kernel.
[ OK ] Started Load Kernel Modules.
[ OK ] Started Remount Root and Kernel File Systems.
Mounting Kernel Configuration File System...
Starting Flush Journal to Persistent Storage...
Starting Apply Kernel Variables...
[ 7.021468] systemd-journald[194]: Received client request to flush runtime journal.
Starting Create System Users...
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Create System Users.
Starting Create Static Device Nodes in /dev...
[ OK ] Started Create Static Device Nodes in /dev.
[ OK ] Reached target Local File Systems (Pre).
Mounting /media/ram...
Mounting /var/volatile...
Starting udev Kernel Device Manager...
[ OK ] Mounted /media/ram.
[ OK ] Started udev Coldplug all Devices.
[ OK ] Mounted /var/volatile.
[ 7.374377] random: systemd: uninitialized urandom read (16 bytes read)
Starting udev Wait for Complete Device Initial[ 7.391619] random: systemd-journal: uninitialized ura
ndom read (16 bytes read)
ization...
[ 7.413320] random: systemd: uninitialized urandom read (16 bytes read)
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Rebuild Dynamic Linker Cache...
Starting Create Volatile Files and Directories...
[ OK ] Started udev Kernel Device Manager.
[ OK ] Started Create Volatile Files and Directories.
Starting Run pending postinsts...
Starting Rebuild Journal Catalog...
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ OK ] Started Rebuild Journal Catalog.
[ OK ] Started Network Time Synchronization.
[ 8.481807] random: systemd: uninitialized urandom read (16 bytes read)
[ OK ] Reached target System Time Set.
[ OK ] Reached target System Time Synchronized.
[ OK ] Started Rebuild Dynamic Linker Cache.
Starting Update is Completed...
[ OK ] Started Update is Completed.
[ 9.136404] random: crng init done
[ 9.139845] random: 71 urandom warning(s) missed due to ratelimiting
[ OK ] Started Load/Save Random Seed.
[ 9.401870] CAN device driver interface
[ 9.477938] at24 2-0050: supply vcc not found, using dummy regulator
[ 9.529124] m_can_platform 20701000.can: m_can device registered (irq=37, version=32)
[ 9.603562] at24 2-0050: 8192 byte 24c64 EEPROM, writable, 32 bytes/write
[ 9.621100] m_can_platform 20711000.can: m_can device registered (irq=39, version=32)
[ 9.924711] k3-m4-rproc 5000000.m4fss: assigned reserved memory node m4f-dma-memory@a4000000
[ 9.967684] k3-m4-rproc 5000000.m4fss: configured M4 for remoteproc mode
[ 10.042235] k3-m4-rproc 5000000.m4fss: local reset is deasserted for device
[ 10.054687] platform 78000000.r5f: configured R5F for remoteproc mode
[ 10.073317] davinci_mdio 300b2400.mdio: Configuring MDIO in manual mode
[ 10.090608] k3_r5_rproc bus@f4000:r5fss@78000000: split-mode not permitted, force configuring for single-cpu
mode
[ 10.114514] remoteproc remoteproc0: 5000000.m4fss is available
[ 10.150987] platform 78000000.r5f: assigned reserved memory node r5f-dma-memory@a0000000
[ 10.151204] remoteproc remoteproc0: powering up 5000000.m4fss
[ 10.169784] remoteproc remoteproc0: Booting fw image am64-mcu-m4f0_0-fw, size 86084
[ 10.181144] davinci_mdio 300b2400.mdio: davinci mdio revision 1.7, bus freq 1000000
[ 10.190393] remoteproc0#vdev0buffer: assigned reserved memory node m4f-dma-memory@a4000000
[ 10.193015] remoteproc remoteproc1: 78000000.r5f is available
[ 10.199388] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 10.204744] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xd
[ 10.215711] remoteproc0#vdev0buffer: registered virtio0 (type 7)
[ 10.217854] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe
[ 10.223831] remoteproc remoteproc0: remote processor 5000000.m4fss is now up
[ 10.266778] remoteproc remoteproc1: powering up 78000000.r5f
[ 10.272590] remoteproc remoteproc1: Booting fw image am64-main-r5f0_0-fw, size 86352
[ 10.284822] davinci_mdio 300b2400.mdio: phy[0]: device 300b2400.mdio:00, driver TI DP83867
[ 10.290770] remoteproc1#vdev0buffer: assigned reserved memory node r5f-dma-memory@a0000000
[ 10.309002] virtio_rpmsg_bus virtio1: rpmsg host is online
[ 10.314788] remoteproc1#vdev0buffer: registered virtio1 (type 7)
[ 10.328454] remoteproc remoteproc1: remote processor 78000000.r5f is now up
[ 10.335616] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0xe
[ 10.339427] platform 78400000.r5f: configured R5F for remoteproc mode
[ 10.433678] k3_r5_rproc bus@f4000:r5fss@78400000: split-mode not permitted, force configuring for single-cpu
mode
[ 10.563141] remoteproc remoteproc3: 30034000.pru is available
[ 10.585457] platform 78400000.r5f: assigned reserved memory node r5f-dma-memory@a2000000
[ 10.662378] remoteproc remoteproc4: 30004000.rtu is available
[ 10.680949] remoteproc remoteproc2: 78400000.r5f is available
[ 10.709812] remoteproc remoteproc5: 3000a000.txpru is available
[ 10.731683] remoteproc remoteproc2: powering up 78400000.r5f
[ 10.737504] remoteproc remoteproc2: Booting fw image am64-main-r5f1_0-fw, size 93260