This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Failure of PC and Target inference of a standalone DL model while migrated from 08.05.00.11 to 08.06.01.03

Part Number: TDA4VM

Hello TI,

I have an ONNX model that is imported and followed by PC and target inference successfully in SDK 08.05.00.11. I have installed SDK 08.06.01.03 and imported the same model successfully. Next when I checked PC(host) inference, ended up getting errors. I have checked for the target inference also. It is also giving errors. We are using standard TDA4VM board.

The error log is shown below.

raju@raju:~/TDA4x_8.06/ti-processor-sdk-rtos-j721e-evm-08_06_01_03/tidl_j721e_08_06_00_10/ti_dl/test$ ./PC_dsp_test_dl_algo.out s:/home/raju/TDA4x_8.06/ti-processor-sdk-rtos-j721e-evm-08_06_01_03/tidl_j721e_08_06_00_10/ti_dl/test/testvecs/config/infer/public/onnx/infer_config_target_08.06.txt

Processing config file #0 : /home/raju/TDA4x_8.06/ti-processor-sdk-rtos-j721e-evm-08_06_01_03/tidl_j721e_08_06_00_10/ti_dl/test/testvecs/config/infer/public/onnx/infer_config_target_08.06.txt 
Error at line:  1127 : in file /opt/Jenkins_OUT/workspace/J7_TIDL_Parent/c7x-mma-tidl/ti_dl/release/tidl_j721e_08_06_00_10/ti_dl/test/src/pc_linux/../tidl_rt.c, of function : TIDLRT_create 
Error Type: TIDL_E_QUANT_STATS_NOT_AVAILABLE            
Error at line:   506 : in file /opt/Jenkins_OUT/workspace/J7_TIDL_Parent/c7x-mma-tidl/ti_dl/release/tidl_j721e_08_06_00_10/ti_dl/test/src/pc_linux/../tidl_tb.c, of function : tidlMultiInstanceTest 
Error Type: TIDL_E_QUANT_STATS_NOT_AVAILABLE 

Can you please guide us based on the above error log?

Thanks,

S Seetharama Raju.