Part Number: TMDS64GPEVM
Other Parts Discussed in Thread: SYSCONFIG
Hi TI Experts
I'm working on a bootloader project on the TMDS64GPEVM development board.
The versions of CCS, SysConfig and mcu_plus_sdk I use are as follows:
CCS: 12.1.0
SDK: mcu_plus_sdk_am64x_08_05_00_24
SysConfig: 1.14.0
I first started by integrating the crypto_aes_ecb_256 project into the sbl_ospi_linux project. As a result, I can use both bootloader and crypto modules and thus I can easily do what I want to do.
Afterwards, I integrated the enet_cpsw_rawhttpserver ethernet project into this project, which ran smoothly. Even though I perform the encryption and ethernet operations in different situations (i.e. when the enet driver is opened, the sa2ul and crypto driver is not opened or vice versa) I get an error like the one below.
Enabling Clocks! EnetUdma_openRxCh: 2086 EnetHostPortDma_open: 121 Cpsw_openInternal: 893 Cpsw_closeInternal: 984 Assertion @ Line: 984 in /home/gtbldadm/nightlybuilds/mcupsdk_internal/jenkins/mcu_plus_sdk_am64x_08_05_00_24/source/networking/enet/core/src/per/V1/cpsw.c: hCpsw->hRxRsvdFlow != NULL
When I run the enet_cpsw_raw http server example in mcu_plus_sdk alone, it works properly. I attribute this to udma. Because both crypto and enet modules use pktdma. When I activate pktdma in both modules in SysConfig, there is no problem. However, while it is running, the problem I mentioned above occurs.
Is this problem related to udma? If not, what could be the reason?
How can I use enet and crypto modules together?
Thanks...