Part Number: AM62A7
Hi,
We are using custom board based on AM62A7 SOC with imx219 camera sensor and using Linux BSP
We referred k3-am62a7-sk-csi-imx219.dts and able to run imx219 camera module with data-lanes 1 and 2.
If we try to change the data-lanes property in dts from 1 2 to 2 3 or 3 4 or 1 4 camera streaming is not working and below error is shown.
Sorry for the delay in sharing schematics.
Attached the schematics of camera section of the board used.