This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM437X: Error in Linux build of AM437x

Guru 10880 points
Part Number: PROCESSOR-SDK-AM437X

Hi,

The customer has installed the SDK for AM437X on a PC with Linux installed. When they run make linux according to the Linux build procedure, they receive an error and it does not seem to complete successfully.

Q1. Is there any reference material on the Linux build procedure for AM437X?

Q2. The error display looks like the following image. I would like to confirm the error content and would like your advice. The SDK installed is "ti-processor-sdk-linux-am437x-evm-08.02.00.24-Linux-x86-Install.bin".

Thanks,

Conor