This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM64B: AM64B-SKEVM SDK9.0 cannot enter the kernel

Part Number: SK-AM64B

Champs.

plz see the attached picture.

AM64 SDK9.0 cannot launched.

How to fix this?

BR Rio

  • Hello Rio,

    Thanks for this query. I need few clarifications before I move ahead.

    So, I am assuming since the customer is trying to bring up kernel, they are booting via SPL?

    Moreover, this is MCU PLUS SDK 9.0, am I correct? (Asking because you might be talking about PROCESSOR SDK AM64x).

    Regards,

    Vaibhav

    ARM Based Processors | FAQ AM62x & AM62A | FAQ AM64x

  • No, this is Linux.

    Only Linux OS can show this kind of screen "GRUB".

    I'm doubting the RootFS has no Debian / other OS inside.

    So, you can tell from the picture, the GRUB asked us to exit due to no OS actually..

    BR Rio

  • Hell Rio,

    Thanks for your response.

    I have assigned this E2E to the correct expert.

    Please expect responses in few business days.

    Regards,

    Vaibhav

    ARM Based Processors | FAQ AM62x & AM62A | FAQ AM64x

  • Hello Rio,
    Will you upload the full boot log?
    Best,
    -Hong

  • Hi Hong:

    As the attached.

    BR Rio

    U-Boot SPL 2023.04-g24098ea90d (Jul 06 2023 - 12:59:40 +0000)
    EEPROM not available at 0x50, trying to read at 0x51
    Resetting on cold boot to workaround ErrataID:i2331
    Please resend tiboot3.bin in case of UART/DFU boot
    resetting ...
    
    U-Boot SPL 2023.04-g24098ea90d (Jul 06 2023 - 12:59:40 +0000)
    EEPROM not available at 0x50, trying to read at 0x51
    SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
    SPL initial stack usage: 13376 bytes
    Trying to boot from MMC2
    mmc fail to send stop cmd
    Error reading cluster
    Authentication passed
    Authentication passed
    Authentication passed
    Authentication passed
    Loading Environment from MMC... MMC Device 0 not found
    *** Warning - No MMC card found, using default environment
    
    Starting ATF on ARM64 core...
    
    NOTICE:  BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty
    NOTICE:  BL31: Built : 00:42:57, Jan 13 2023
    I/TC:
    I/TC: OP-TEE version: 3.20.0 (gcc version 11.3.0 (GCC)) #1 Fri Jan 20 15:42:54 UTC 2023 aarch64
    I/TC: WARNING: This OP-TEE configuration might be insecure!
    I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
    I/TC: Primary CPU initializing
    I/TC: SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
    I/TC: HUK Initialized
    I/TC: Activated SA2UL device
    I/TC: Enabled firewalls for SA2UL TRNG device
    I/TC: SA2UL TRNG initialized
    I/TC: SA2UL Drivers initialized
    I/TC: Primary CPU switching to normal world boot
    
    U-Boot SPL 2023.04-g24098ea90d (Jul 06 2023 - 12:59:40 +0000)
    SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
    Trying to boot from MMC2
    Authentication passed
    Authentication passed
    
    
    U-Boot 2023.04-g24098ea90d (Jul 06 2023 - 12:59:40 +0000)
    
    SoC:   AM64X SR2.0 HS-FS
    Model: Texas Instruments AM642 SK
    Board: AM64B-SKEVM rev A
    DRAM:  2 GiB
    Core:  63 devices, 31 uclasses, devicetree: separate
    MMC:   mmc@fa00000: 1
    Loading Environment from MMC... MMC Device 0 not found
    *** Warning - No MMC card found, using default environment
    
    In:    serial@2800000
    Out:   serial@2800000
    Err:   serial@2800000
    Net:   eth0: ethernet@8000000port@1
    Warning: ethernet@8000000port@2 MAC addresses don't match:
    Address in ROM is               34:08:e1:80:ae:13
    Address in environment is       70:ff:76:1e:bc:49
    , eth1: ethernet@8000000port@2
    Hit any key to stop autoboot:  0
    switch to partitions #0, OK
    mmc1 is current device
    SD/MMC found on device 1
    Failed to load 'boot.scr'
    574 bytes read in 29 ms (18.6 KiB/s)
    Loaded env from uEnv.txt
    Importing environment from mmc1 ...
    mmc fail to send stop cmd
     ** fs_devread read error - block
    Failed to load '/boot/Image'
    ** No partition table - mmc 1 **
    Couldn't find partition mmc 1:2
    Can't set block device
    libfdt fdt_check_header(): FDT_ERR_BADMAGIC
    No FDT memory address configured. Please configure
    the FDT address via "fdt addr <address>" command.
    Aborting!
    ERROR: Did not find a cmdline Flattened Device Tree
    Could not find a valid device tree
    MMC Device 0 not found
    no mmc device at slot 0
    switch to partitions #0, OK
    mmc1 is current device
    Scanning mmc 1:1...
    No EFI system partition
    No EFI system partition
    Failed to persist EFI variables
    BootOrder not defined
    EFI boot manager: Cannot load any image
    Found EFI removable media binary efi/boot/bootaa64.efi
    733184 bytes read in 60 ms (11.7 MiB/s)
    Booting /efi\boot\bootaa64.efi
    Welcome to GRUB!
    
    error: no such device: ((hd0,msdos1)/efi/boot)/EFI/BOOT/grub.cfg.
    error: serial port `com0' isn't found.
    
    
                                                                                       GNU GRUB  version 2.06
    
     lqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqk
     x*boot                                                                                                                                                                                    x
     x                                                                                                                                                                                         x
     x                                                                                                                                                                                         x
     x                                                                                                                                                                                         x
     x                                                                                                                                                                                         x
     x                                                                                                                                                                                         x
     x                                                                                                                                                                                         x
     x                                                                                                                                                                                         x
     x                                                                                                                                                                                         x
     x                                                                                                                                                                                         x
     x                                                                                                                                                                                         x
     x                                                                                                                                                                                         x
     x                                                                                                                                                                                         x
     x                                                                                                                                                                                         x
     x                                                                                                                                                                                         x
     mqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqj
    
          Use the ? and ? keys to select which entry is highlighted.
          Press enter to boot the selected OS, `e' to edit the commands before booting or `c' for a command-line.
       The highlighted entry will be executed automatically in 0s.
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
      Booting `boot'
    
    mmc fail to send stop cmd
    error: failure reading sector 0x1100 from `hd0'.
    
    Press any key to continue...
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    

  • From the log, the MMC0 is not detected .

    it seems the boot mode pin setting is not correct.

    But we do follow the Userguide / TRM to set:

    SW2: 0000 0010

    SW3: 0100 0011

    Is this right?

    BR Rio

  • Hello Rio,
    On SK-AM64B,
    - mmc1 @0xfa00000 is connected for SD card
    - mmc0 @0xfa10000 is not connected
    Best,
    -Hong

  • Hi Hong:

    May you reply us what's the right dip switch for SD boot on AM64 SKEVM?

    BR Ro

  • Hello Rio,
    I'm attaching a working boot log with SDK9.0 on SK-AM64
    BOOTMODE[15:0] setting from the log
    43000030: 00000243
    Best,
    -Hong

    U-Boot SPL 2023.04-g24098ea90d (Jul 06 2023 - 12:59:40 +0000)
    EEPROM not available at 0x50, trying to read at 0x51
    Resetting on cold boot to workaround ErrataID:i2331
    Please resend tiboot3.bin in case of UART/DFU boot
    resetting ...
    
    U-Boot SPL 2023.04-g24098ea90d (Jul 06 2023 - 12:59:40 +0000)
    EEPROM not available at 0x50, trying to read at 0x51
    SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
    SPL initial stack usage: 13376 bytes
    Trying to boot from MMC2
    Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
    Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
    Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
    Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
    Loading Environment from MMC... MMC Device 0 not found
    *** Warning - No MMC card found, using default environment
    
    Starting ATF on ARM64 core...
    
    NOTICE:  BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty
    NOTICE:  BL31: Built : 00:42:57, Jan 13 2023
    I/TC: 
    I/TC: OP-TEE version: 3.20.0 (gcc version 11.3.0 (GCC)) #1 Fri Jan 20 15:42:54 UTC 2023 aarch64
    I/TC: WARNING: This OP-TEE configuration might be insecure!
    I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
    I/TC: Primary CPU initializing
    I/TC: SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
    I/TC: HUK Initialized
    I/TC: Activated SA2UL device
    I/TC: Fixing SA2UL firewall owner for GP device
    I/TC: Enabled firewalls for SA2UL TRNG device
    I/TC: SA2UL TRNG initialized
    I/TC: SA2UL Drivers initialized
    I/TC: Primary CPU switching to normal world boot
    
    U-Boot SPL 2023.04-g24098ea90d (Jul 06 2023 - 12:59:40 +0000)
    SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
    Trying to boot from MMC2
    Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
    Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
    
    
    U-Boot 2023.04-g24098ea90d (Jul 06 2023 - 12:59:40 +0000)
    
    SoC:   AM64X SR1.0 GP
    Model: Texas Instruments AM642 SK
    Board: AM64-SKEVM rev E3
    DRAM:  2 GiB
    Core:  63 devices, 31 uclasses, devicetree: separate
    MMC:   mmc@fa00000: 1
    Loading Environment from MMC... MMC Device 0 not found
    *** Warning - No MMC card found, using default environment
    
    In:    serial@2800000
    Out:   serial@2800000
    Err:   serial@2800000
    Net:   eth0: ethernet@8000000port@1
    Warning: ethernet@8000000port@2 MAC addresses don't match:
    Address in ROM is		ac:1f:0f:8b:26:1a
    Address in environment is	70:ff:76:1d:f3:80
    , eth1: ethernet@8000000port@2
    Hit any key to stop autoboot:  2  0 
    => mmc list
    mmc@fa00000: 1
    => md.l 0x43000030 1
    43000030: 00000243                             C...
    => boot
    switch to partitions #0, OK
    mmc1 is current device
    SD/MMC found on device 1
    Failed to load 'boot.scr'
    574 bytes read in 32 ms (16.6 KiB/s)
    Loaded env from uEnv.txt
    Importing environment from mmc1 ...
    20593152 bytes read in 890 ms (22.1 MiB/s)
    55213 bytes read in 36 ms (1.5 MiB/s)
    Working FDT set to 88000000
    ## Flattened Device Tree blob at 88000000
       Booting using the fdt blob at 0x88000000
    Working FDT set to 88000000
       Loading Device Tree to 000000008feef000, end 000000008fffffff ... OK
    Working FDT set to 8feef000
    
    Starting kernel ...
    
    [    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
    [    0.000000] Linux version 6.1.33-g40c32565ca (oe-user@oe-host) (aarch64-oe-linux-gcc (GCC) 11.3.0, GNU ld (GNU Binutils) 2.38.20220708) #1 SMP PREEMPT Thu Jul  6 14:17:24 UTC 2023
    [    0.000000] Machine model: Texas Instruments AM642 SK
    [    0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
    [    0.000000] printk: bootconsole [ns16550a0] enabled
    [    0.000000] efi: UEFI not found.
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB
    [    0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB
    [    0.000000] OF: reserved mem: initialized node r5f-memory@a1100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a2000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 15 MiB
    [    0.000000] OF: reserved mem: initialized node r5f-memory@a2100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a3000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a3000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a3100000, size 15 MiB
    [    0.000000] OF: reserved mem: initialized node r5f-memory@a3100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node m4f-dma-memory@a4000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, size 15 MiB
    [    0.000000] OF: reserved mem: initialized node m4f-memory@a4100000, compatible id shared-dma-pool
    [    0.000000] Zone ranges:
    [    0.000000]   DMA      [mem 0x0000000080000000-0x00000000ffffffff]
    [    0.000000]   DMA32    empty
    [    0.000000]   Normal   empty
    [    0.000000] Movable zone start for each node
    [    0.000000] Early memory node ranges
    [    0.000000]   node   0: [mem 0x0000000080000000-0x000000009e7fffff]
    [    0.000000]   node   0: [mem 0x000000009e800000-0x00000000a57fffff]
    [    0.000000]   node   0: [mem 0x00000000a5800000-0x00000000ffffffff]
    [    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffffff]
    [    0.000000] cma: Reserved 32 MiB at 0x00000000fba00000
    [    0.000000] psci: probing for conduit method from DT.
    [    0.000000] psci: PSCIv1.1 detected in firmware.
    [    0.000000] psci: Using standard PSCI v0.2 function IDs
    [    0.000000] psci: Trusted OS migration not required
    [    0.000000] psci: SMC Calling Convention v1.2
    [    0.000000] percpu: Embedded 19 pages/cpu s38376 r8192 d31256 u77824
    [    0.000000] Detected VIPT I-cache on CPU0
    [    0.000000] CPU features: detected: GIC system register CPU interface
    [    0.000000] CPU features: detected: ARM erratum 845719
    [    0.000000] alternatives: applying boot alternatives
    [    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 516096
    [    0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 root=PARTUUID=f8739cc1-02 rw rootfstype=ext4 rootwait
    [    0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
    [    0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
    [    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
    [    0.000000] Memory: 1888840K/2097152K available (12480K kernel code, 1294K rwdata, 4040K rodata, 2176K init, 498K bss, 175544K reserved, 32768K cma-reserved)
    [    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
    [    0.000000] rcu: Preemptible hierarchical RCU implementation.
    [    0.000000] rcu: 	RCU event tracing is enabled.
    [    0.000000] rcu: 	RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
    [    0.000000] 	Trampoline variant of Tasks RCU enabled.
    [    0.000000] 	Tracing variant of Tasks RCU enabled.
    [    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
    [    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
    [    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
    [    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
    [    0.000000] GICv3: 256 SPIs implemented
    [    0.000000] GICv3: 0 Extended SPIs implemented
    [    0.000000] Root IRQ handler: gic_handle_irq
    [    0.000000] GICv3: GICv3 features: 16 PPIs
    [    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001840000
    [    0.000000] ITS [mem 0x01820000-0x0182ffff]
    [    0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
    [    0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
    [    0.000000] ITS@0x0000000001820000: allocated 524288 Devices @80800000 (flat, esz 8, psz 64K, shr 0)
    [    0.000000] ITS: using cache flushing for cmd queue
    [    0.000000] GICv3: using LPI property table @0x0000000080030000
    [    0.000000] GIC: using cache flushing for LPI property table
    [    0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000080040000
    [    0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
    [    0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
    [    0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
    [    0.000001] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
    [    0.008610] Console: colour dummy device 80x25
    [    0.013211] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
    [    0.023892] pid_max: default: 32768 minimum: 301
    [    0.028676] LSM: Security Framework initializing
    [    0.033554] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
    [    0.041137] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
    [    0.051233] cblist_init_generic: Setting adjustable number of callback queues.
    [    0.058712] cblist_init_generic: Setting shift to 1 and lim to 1.
    [    0.065034] cblist_init_generic: Setting shift to 1 and lim to 1.
    [    0.071475] rcu: Hierarchical SRCU implementation.
    [    0.076384] rcu: 	Max phase no-delay instances is 1000.
    [    0.082069] Platform MSI: msi-controller@1820000 domain created
    [    0.088470] PCI/MSI: /bus@f4000/interrupt-controller@1800000/msi-controller@1820000 domain created
    [    0.098493] EFI services will not be available.
    [    0.103488] smp: Bringing up secondary CPUs ...
    I/TC: Secondary CPU 1 initializing
    I/TC: Secondary CPU 1 switching to normal world boot
    [    0.117174] Detected VIPT I-cache on CPU1
    [    0.117320] GICv3: CPU1: found redistributor 1 region 0:0x0000000001860000
    [    0.117342] GICv3: CPU1: using allocated LPI pending table @0x0000000080050000
    [    0.117405] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
    [    0.117538] smp: Brought up 1 node, 2 CPUs
    [    0.146924] SMP: Total of 2 processors activated.
    [    0.151737] CPU features: detected: 32-bit EL0 Support
    [    0.157009] CPU features: detected: CRC32 instructions
    [    0.162338] CPU: All CPU(s) started at EL2
    [    0.166524] alternatives: applying system-wide alternatives
    [    0.174329] devtmpfs: initialized
    [    0.187171] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
    [    0.197193] futex hash table entries: 512 (order: 3, 32768 bytes, linear)
    [    0.205694] pinctrl core: initialized pinctrl subsystem
    [    0.211772] DMI not present or invalid.
    [    0.216528] NET: Registered PF_NETLINK/PF_ROUTE protocol family
    [    0.223992] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
    [    0.231462] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
    [    0.239579] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
    [    0.247792] audit: initializing netlink subsys (disabled)
    [    0.253744] audit: type=2000 audit(0.160:1): state=initialized audit_enabled=0 res=1
    [    0.254397] thermal_sys: Registered thermal governor 'step_wise'
    [    0.261704] thermal_sys: Registered thermal governor 'power_allocator'
    [    0.268143] cpuidle: using governor menu
    [    0.279085] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
    [    0.286107] ASID allocator initialised with 65536 entries
    [    0.305091] KASLR disabled due to lack of seed
    [    0.318503] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
    [    0.325477] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
    [    0.331887] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
    [    0.338824] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
    [    0.345229] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
    [    0.352164] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
    [    0.358567] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
    [    0.365502] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
    [    0.374276] k3-chipinfo 43000014.chipid: Family:AM64X rev:SR1.0 JTAGID[0x0bb3802f] Detected
    [    0.384267] iommu: Default domain type: Translated 
    [    0.389282] iommu: DMA domain TLB invalidation policy: strict mode 
    [    0.396057] SCSI subsystem initialized
    [    0.400465] usbcore: registered new interface driver usbfs
    [    0.406133] usbcore: registered new interface driver hub
    [    0.411604] usbcore: registered new device driver usb
    [    0.417319] pps_core: LinuxPPS API ver. 1 registered
    [    0.422401] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    [    0.431751] PTP clock support registered
    [    0.435894] EDAC MC: Ver: 3.0.0
    [    0.440363] omap-mailbox 29020000.mailbox: omap mailbox rev 0x66fc9100
    [    0.447342] omap-mailbox 29040000.mailbox: omap mailbox rev 0x66fc9100
    [    0.454201] omap-mailbox 29060000.mailbox: omap mailbox rev 0x66fc9100
    [    0.461627] FPGA manager framework
    [    0.465242] Advanced Linux Sound Architecture Driver Initialized.
    [    0.472760] clocksource: Switched to clocksource arch_sys_counter
    [    0.479354] VFS: Disk quotas dquot_6.6.0
    [    0.483435] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
    [    0.497856] NET: Registered PF_INET protocol family
    [    0.503203] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
    [    0.512965] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
    [    0.521814] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
    [    0.529767] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
    [    0.537994] TCP bind hash table entries: 16384 (order: 7, 524288 bytes, linear)
    [    0.546098] TCP: Hash tables configured (established 16384 bind 16384)
    [    0.553079] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
    [    0.560032] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
    [    0.567624] NET: Registered PF_UNIX/PF_LOCAL protocol family
    [    0.574063] RPC: Registered named UNIX socket transport module.
    [    0.580177] RPC: Registered udp transport module.
    [    0.584989] RPC: Registered tcp transport module.
    [    0.589797] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    0.596391] NET: Registered PF_XDP protocol family
    [    0.601335] PCI: CLS 0 bytes, default 64
    [    0.606250] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
    [    0.616420] Initialise system trusted keyrings
    [    0.621331] workingset: timestamp_bits=46 max_order=19 bucket_order=0
    [    0.635212] squashfs: version 4.0 (2009/01/31) Phillip Lougher
    [    0.642171] NFS: Registering the id_resolver key type
    [    0.647461] Key type id_resolver registered
    [    0.651740] Key type id_legacy registered
    [    0.655924] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
    [    0.662783] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
    [    0.670624] 9p: Installing v9fs 9p2000 file system support
    [    0.719449] Key type asymmetric registered
    [    0.723644] Asymmetric key parser 'x509' registered
    [    0.728702] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
    [    0.736555] io scheduler mq-deadline registered
    [    0.741203] io scheduler kyber registered
    [    0.748730] pinctrl-single 4084000.pinctrl: 33 pins, size 132
    [    0.755390] pinctrl-single f4000.pinctrl: 180 pins, size 720
    [    0.762465] pinctrl-single a40000.pinctrl: 512 pins, size 2048
    [    0.777028] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
    [    0.793509] loop: module loaded
    [    0.798166] megasas: 07.719.03.00-rc1
    [    0.806542] tun: Universal TUN/TAP device driver, 1.6
    [    0.812604] thunder_xcv, ver 1.0
    [    0.815991] thunder_bgx, ver 1.0
    [    0.819325] nicpf, ver 1.0
    [    0.822511] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
    [    0.829902] hns3: Copyright (c) 2017 Huawei Corporation.
    [    0.835425] hclge is initializing
    [    0.838840] e1000: Intel(R) PRO/1000 Network Driver
    [    0.843825] e1000: Copyright (c) 1999-2006 Intel Corporation.
    [    0.849752] e1000e: Intel(R) PRO/1000 Network Driver
    [    0.854826] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
    [    0.860918] igb: Intel(R) Gigabit Ethernet Network Driver
    [    0.866436] igb: Copyright (c) 2007-2014 Intel Corporation.
    [    0.872182] igbvf: Intel(R) Gigabit Virtual Function Network Driver
    [    0.878591] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
    [    0.884857] sky2: driver version 1.30
    [    0.889520] VFIO - User Level meta-driver version: 0.3
    [    0.895791] usbcore: registered new interface driver usb-storage
    [    0.902896] i2c_dev: i2c /dev entries driver
    [    0.909038] sdhci: Secure Digital Host Controller Interface driver
    [    0.915399] sdhci: Copyright(c) Pierre Ossman
    [    0.920301] Synopsys Designware Multimedia Card Interface Driver
    [    0.926846] sdhci-pltfm: SDHCI platform and OF driver helper
    [    0.933633] ledtrig-cpu: registered to indicate activity on CPUs
    [    0.940054] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
    [    0.947031] usbcore: registered new interface driver usbhid
    [    0.952773] usbhid: USB HID core driver
    [    0.958204] optee: probing for conduit method.
    I/TC: Reserved shared memory is enabled
    I/TC: Dynamic shared memory is enabled
    I/TC: Normal World virtualization support is disabled
    I/TC: Asynchronous notifications are disabled
    [    0.962827] optee: revision 3.20 (8e74d476)
    [    0.979530] optee: dynamic shared memory is enabled
    [    0.989318] optee: initialized driver
    [    0.995534] Initializing XFRM netlink socket
    [    1.000028] NET: Registered PF_PACKET protocol family
    [    1.005405] 9pnet: Installing 9P2000 support
    [    1.009877] Key type dns_resolver registered
    [    1.014830] registered taskstats version 1
    [    1.019093] Loading compiled-in X.509 certificates
    [    1.036608] ti-sci 44043000.system-controller: ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
    [    1.079266] pca953x 0-0070: supply vcc not found, using dummy regulator
    [    1.086266] pca953x 0-0070: using no AI
    [    1.113686] omap_i2c 20010000.i2c: bus 0 rev0.12 at 400 kHz
    [    1.119818] ti-sci-intr 4210000.interrupt-controller: Interrupt Router 5 domain created
    [    1.128258] ti-sci-intr bus@f4000:interrupt-controller@a00000: Interrupt Router 3 domain created
    [    1.137637] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created
    [    1.149815] ti-udma 485c0100.dma-controller: Number of rings: 68
    [    1.157471] ti-udma 485c0100.dma-controller: Channels: 24 (bchan: 12, tchan: 6, rchan: 6)
    [    1.167735] ti-udma 485c0000.dma-controller: Number of rings: 288
    [    1.183252] ti-udma 485c0000.dma-controller: Channels: 44 (tchan: 29, rchan: 15)
    [    1.194524] printk: console [ttyS2] disabled
    [    1.199006] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 304, base_baud = 3000000) is a 8250
    [    1.207912] printk: console [ttyS2] enabled
    [    1.207912] printk: console [ttyS2] enabled
    [    1.216373] printk: bootconsole [ns16550a0] disabled
    [    1.216373] printk: bootconsole [ns16550a0] disabled
    [    1.230534] spi-nor spi0.0: s28hs512t (65536 Kbytes)
    [    1.235684] 7 fixed-partitions partitions found on MTD device fc40000.spi.0
    [    1.242655] Creating 7 MTD partitions on "fc40000.spi.0":
    [    1.248052] 0x000000000000-0x000000100000 : "ospi.tiboot3"
    [    1.255023] 0x000000100000-0x000000300000 : "ospi.tispl"
    [    1.261815] 0x000000300000-0x000000700000 : "ospi.u-boot"
    [    1.268686] 0x000000700000-0x000000740000 : "ospi.env"
    [    1.275266] 0x000000740000-0x000000780000 : "ospi.env.backup"
    [    1.282464] 0x000000800000-0x000003fc0000 : "ospi.rootfs"
    [    1.289437] 0x000003fc0000-0x000004000000 : "ospi.phypattern"
    [    1.298617] davinci_mdio 8000f00.mdio: Configuring MDIO in manual mode
    [    1.344801] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
    [    1.355155] davinci_mdio 8000f00.mdio: phy[0]: device 8000f00.mdio:00, driver TI DP83867
    [    1.363289] davinci_mdio 8000f00.mdio: phy[1]: device 8000f00.mdio:01, driver TI DP83867
    [    1.371431] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA00903, cpsw version 0x6BA80903 Ports: 3 quirks:00000006
    [    1.384347] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.4
    [    1.391484] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512
    [    1.398251] pps pps0: new PPS source ptp0
    [    1.402761] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:1
    [    1.413835] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 16
    [    1.424882] am65-cpts 39000000.cpts: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:0
    [    1.449761] debugfs: Directory 'pd:114' with parent 'pm_genpd' already present!
    [    1.450432] mmc0: CQHCI version 5.10
    [    1.459569] mmc1: CQHCI version 5.10
    [    1.471329] ALSA device list:
    [    1.474364]   No soundcards found.
    [    1.504960] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit
    [    1.504960] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit
    [    1.521738] Waiting for root device PARTUUID=f8739cc1-02...
    [    1.525724] sdhci-am654 fa10000.mmc: card claims to support voltages below defined range
    [    1.546846] mmc0: new SDIO card at address 0001
    [    1.585342] mmc1: new ultra high speed SDR104 SDHC card at address aaaa
    [    1.593028] mmcblk1: mmc1:aaaa SC16G 14.8 GiB 
    [    1.603231]  mmcblk1: p1 p2
    [    1.656792] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Quota mode: none.
    [    1.682786] VFS: Mounted root (ext4 filesystem) on device 179:2.
    [    1.692256] devtmpfs: mounted
    [    1.696815] Freeing unused kernel memory: 2176K
    [    1.701462] Run /sbin/init as init process
    [    1.911089] systemd[1]: System time before build time, advancing clock.
    [    1.963241] NET: Registered PF_INET6 protocol family
    [    1.969960] Segment Routing with IPv6
    [    1.973746] In-situ OAM (IOAM) with IPv6
    [    2.018888] systemd[1]: systemd 250.5+ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK +XKBCOMMON +UTMP +SYSVINIT default-hierarchy=hybrid)
    [    2.050741] systemd[1]: Detected architecture arm64.
    
    Welcome to Arago 2023.04!
    
    [    2.124188] systemd[1]: Hostname set to <am64xx-evm>.
    [    2.134901] systemd[1]: Initializing machine ID from random generator.
    [    2.365415] systemd-sysv-generator[135]: SysV service '/etc/init.d/netopeer2-server' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
    [    2.393553] systemd-sysv-generator[135]: SysV service '/etc/init.d/sysrepo' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
    [    2.417669] systemd-sysv-generator[135]: SysV service '/etc/init.d/thermal-zone-init' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
    [    2.446122] systemd-sysv-generator[135]: SysV service '/etc/init.d/telnetd' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
    [    2.472464] systemd-sysv-generator[135]: SysV service '/etc/init.d/inetd.busybox' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
    [    2.499408] systemd-sysv-generator[135]: SysV service '/etc/init.d/resize_rootfs.sh' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
    [    2.526514] systemd-sysv-generator[135]: SysV service '/etc/init.d/dropbear' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
    [    2.550948] systemd-sysv-generator[135]: SysV service '/etc/init.d/docker.init' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
    [    2.576398] systemd-sysv-generator[135]: SysV service '/etc/init.d/netperf' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
    [    2.887327] systemd[1]: /lib/systemd/system/startwlansta.service:7: Unknown key name 'After' in section 'Service', ignoring.
    [    2.902444] systemd[1]: /lib/systemd/system/startwlanap.service:7: Unknown key name 'After' in section 'Service', ignoring.
    [    2.967592] systemd[1]: /lib/systemd/system/bt-enable.service:9: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
    [    3.063136] systemd[1]: /etc/systemd/system/sync-clocks.service:11: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
    [    3.167968] systemd[1]: Queued start job for default target Graphical Interface.
    [    3.245154] systemd[1]: Created slice Slice /system/getty.
    [  OK  ] Created slice Slice /system/getty.
    [    3.272870] systemd[1]: Created slice Slice /system/modprobe.
    [  OK  ] Created slice Slice /system/modprobe.
    [    3.296962] systemd[1]: Created slice Slice /system/serial-getty.
    [  OK  ] Created slice Slice /system/serial-getty.
    [    3.323977] systemd[1]: Created slice User and Session Slice.
    [  OK  ] Created slice User and Session Slice.
    [    3.345480] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
    [  OK  ] Started Dispatch Password �ts to Console Directory Watch.
    [    3.369419] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
    [  OK  ] Started Forward Password R�uests to Wall Directory Watch.
    [    3.393570] systemd[1]: Reached target Path Units.
    [  OK  ] Reached target Path Units.
    [    3.413096] systemd[1]: Reached target Remote File Systems.
    [  OK  ] Reached target Remote File Systems.
    [    3.433077] systemd[1]: Reached target Slice Units.
    [  OK  ] Reached target Slice Units.
    [    3.453096] systemd[1]: Reached target Swaps.
    [  OK  ] Reached target Swaps.
    [    3.524064] systemd[1]: Listening on RPCbind Server Activation Socket.
    [  OK  ] Listening on RPCbind Server Activation Socket.
    [    3.545175] systemd[1]: Reached target RPC Port Mapper.
    [  OK  ] Reached target RPC Port Mapper.
    [    3.575407] systemd[1]: Listening on Process Core Dump Socket.
    [  OK  ] Listening on Process Core Dump Socket.
    [    3.597607] systemd[1]: Listening on initctl Compatibility Named Pipe.
    [  OK  ] Listening on initctl Compatibility Named Pipe.
    [    3.622210] systemd[1]: Listening on Journal Audit Socket.
    [  OK  ] Listening on Journal Audit Socket.
    [    3.645882] systemd[1]: Listening on Journal Socket (/dev/log).
    [  OK  ] Listening on Journal Socket (/dev/log).
    [    3.670004] systemd[1]: Listening on Journal Socket.
    [  OK  ] Listening on Journal Socket.
    [    3.690256] systemd[1]: Listening on Network Service Netlink Socket.
    [  OK  ] Listening on Network Service Netlink Socket.
    [    3.714212] systemd[1]: Listening on udev Control Socket.
    [  OK  ] Listening on udev Control Socket.
    [    3.737823] systemd[1]: Listening on udev Kernel Socket.
    [  OK  ] Listening on udev Kernel Socket.
    [    3.761875] systemd[1]: Listening on User Database Manager Socket.
    [  OK  ] Listening on User Database Manager Socket.
    [    3.809546] systemd[1]: Mounting Huge Pages File System...
             Mounting Huge Pages File System...
    [    3.835876] systemd[1]: Mounting POSIX Message Queue File System...
             Mounting POSIX Message Queue File System...
    [    3.863950] systemd[1]: Mounting Kernel Debug File System...
             Mounting Kernel Debug File System...
    [    3.881633] systemd[1]: Kernel Trace File System was skipped because of a failed condition check (ConditionPathExists=/sys/kernel/tracing).
    [    3.921605] systemd[1]: Mounting Temporary Directory /tmp...
             Mounting Temporary Directory /tmp...
    [    3.945665] systemd[1]: Starting Create List of Static Device Nodes...
             Starting Create List of Static Device Nodes...
    [    3.975827] systemd[1]: Starting Load Kernel Module configfs...
             Starting Load Kernel Module configfs...
    [    4.026017] systemd[1]: Starting Load Kernel Module drm...
             Starting Load Kernel Module drm...
    [    4.049172] systemd[1]: Starting Load Kernel Module fuse...
             Starting Load Kernel Module fuse...
    [    4.074367] fuse: init (API version 7.37)
    [    4.081881] systemd[1]: Starting RPC Bind...
             Starting RPC Bind...
    [    4.101637] systemd[1]: File System Check on Root Device was skipped because of a failed condition check (ConditionPathIsReadWrite=!/).
    [    4.142031] systemd[1]: Starting Journal Service...
             Starting Journal Service...
    [    4.171975] systemd[1]: Starting Load Kernel Modules...
             Starting Load Kernel Modules...
    [    4.201997] systemd[1]: Starting Generate network units from Kernel command line...
             Starting Generate network �ts from Kernel command line...
    [    4.229544] cryptodev: loading out-of-tree module taints kernel.
    [    4.242048] cryptodev: driver 1.12 loaded.
    [    4.254382] systemd[1]: Starting Remount Root and Kernel File Systems...
             Starting Remount Root and Kernel File Systems...
    [    4.290231] systemd[1]: Starting Coldplug All udev Devices...
    [    4.303125] EXT4-fs (mmcblk1p2): re-mounted. Quota mode: none.
             Starting Coldplug All udev Devices...
    [    4.344283] systemd[1]: Started RPC Bind.
    [  OK  ] Started RPC Bind.
    [    4.367377] systemd[1]: Mounted Huge Pages File System.
    [  OK  ] Mounted Huge Pages File System.
    [    4.389997] systemd[1]: Mounted POSIX Message Queue File System.
    [  OK  ] Mounted POSIX Message Queue File System.
    [    4.418008] systemd[1]: Started Journal Service.
    [  OK  ] Started Journal Service.
    [  OK  ] Mounted Kernel Debug File System.
    [  OK  ] Mounted Temporary Directory /tmp.
    [  OK  ] Finished Create List of Static Device Nodes.
    [  OK  ] Finished Load Kernel Module configfs.
    [  OK  ] Finished Load Kernel Module drm.
    [  OK  ] Finished Load Kernel Module fuse.
    [  OK  ] Finished Load Kernel Modules.
    [  OK  ] Finished Generate network units from Kernel command line.
    [  OK  ] Finished Remount Root and Kernel File Systems.
             Mounting FUSE Control File System...
             Mounting Kernel Configuration File System...
             Starting Flush Journal to Persistent Storage...
             Starting Apply Kernel Variables...
             Starting Create System Users...
    [    4.803664] systemd-journald[149]: Received client request to flush runtime journal.
    [  OK  ] Mounted FUSE Control File System.
    [  OK  ] Mounted Kernel Configuration File System.
    [  OK  ] Finished Flush Journal to Persistent Storage.
    [  OK  ] Finished Apply Kernel Variables.
    [  OK  ] Finished Create System Users.
             Starting Create Static Device Nodes in /dev...
    [  OK  ] Finished Create Static Device Nodes in /dev.
    [  OK  ] Reached target Preparation for Local File Systems.
             Mounting /media/ram...
             Mounting /var/volatile...
    [    5.107444] audit: type=1334 audit(1651167748.192:2): prog-id=5 op=LOAD
    [    5.115159] audit: type=1334 audit(1651167748.204:3): prog-id=6 op=LOAD
             Starting Rule-based Manage�for Device Events and Files...
    [  OK  ] Finished Coldplug All udev Devices.
    [  OK  ] Mounted /media/ram.
    [  OK  ] Mounted /var/volatile.
             Starting Load/Save Random Seed...
    [  OK  ] Reached target Local File Systems.
             Starting Rebuild Dynamic Linker Cache...
             Starting Create Volatile Files and Directories...
    [  OK  ] Finished Create Volatile Files and Directories.
             Starting Rebuild Journal Catalog...
             Starting Network Time Synchronization...
             Starting Record System Boot/Shutdown in UTMP...
    [  OK  ] Started Rule-based Manager for Device Events and Files.
    [  OK  ] Finished Record System Boot/Shutdown in UTMP.
    [  OK  ] Finished Rebuild Journal Catalog.
    [    6.228847] random: crng init done
    [  OK  ] Finished Load/Save Random Seed.
    [  OK  ] Started Network Time Synchronization.
    [  OK  ] Reached target System Time Set.
    [  OK  ] Found device /dev/ttyS2.
    [    7.409157] k3-m4-rproc 5000000.m4fss: assigned reserved memory node m4f-dma-memory@a4000000
    [  OK  ] Finished Rebuild Dynamic Linker Cache.
             Starting Run pending postinsts...
             Starting Update is Completed...
    [    7.499545] k3-m4-rproc 5000000.m4fss: configured M4 for remoteproc mode
    [  OK  ] Finished Update is Completed.
    [    7.611932] k3-m4-rproc 5000000.m4fss: local reset is deasserted for device
    [    7.628811] platform 78000000.r5f: configured R5F for remoteproc mode
    [    7.679464] platform 78000000.r5f: assigned reserved memory node r5f-dma-memory@a0000000
    [    7.723225] remoteproc remoteproc0: 5000000.m4fss is available
    [    7.740568] remoteproc remoteproc1: 78000000.r5f is available
    [    7.760590] remoteproc remoteproc1: powering up 78000000.r5f
    [    7.766452] remoteproc remoteproc1: Booting fw image am64-main-r5f0_0-fw, size 86352
    [    7.801027] remoteproc remoteproc0: powering up 5000000.m4fss
    [    7.808872] remoteproc remoteproc0: Booting fw image am64-mcu-m4f0_0-fw, size 86084
    [    7.827231] rproc-virtio rproc-virtio.0.auto: assigned reserved memory node r5f-dma-memory@a0000000
    [    7.840922] platform 78200000.r5f: configured R5F for remoteproc mode
    [    7.841166] rproc-virtio rproc-virtio.1.auto: assigned reserved memory node m4f-dma-memory@a4000000
    [    7.860982] virtio_rpmsg_bus virtio0: rpmsg host is online
    [    7.867720] rproc-virtio rproc-virtio.0.auto: registered virtio0 (type 7)
    [    7.876454] virtio_rpmsg_bus virtio1: rpmsg host is online
    [    7.883048] remoteproc remoteproc1: remote processor 78000000.r5f is now up
    [    7.890273] rproc-virtio rproc-virtio.1.auto: registered virtio1 (type 7)
    [    7.897244] remoteproc remoteproc0: remote processor 5000000.m4fss is now up
    [    7.904660] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe
    [    7.913601] virtio_rpmsg_bus virtio1: creating channel ti.ipc4.ping-pong addr 0xd
    [    7.921596] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0xe
    [    7.958461] platform 78200000.r5f: assigned reserved memory node r5f-dma-memory@a1000000
    [    7.967705] remoteproc remoteproc2: 78200000.r5f is available
    [    7.987703] remoteproc remoteproc2: powering up 78200000.r5f
    [    7.993500] remoteproc remoteproc2: Booting fw image am64-main-r5f0_1-fw, size 141772
    [    8.007952] platform 78400000.r5f: configured R5F for remoteproc mode
    [    8.010065] rproc-virtio rproc-virtio.2.auto: assigned reserved memory node r5f-dma-memory@a1000000
    [    8.041303] virtio_rpmsg_bus virtio2: rpmsg host is online
    [    8.053862] rproc-virtio rproc-virtio.2.auto: registered virtio2 (type 7)
    [    8.060836] remoteproc remoteproc2: remote processor 78200000.r5f is now up
    [    8.068113] virtio_rpmsg_bus virtio2: creating channel rpmsg_chrdev addr 0xe
    [    8.097108] platform 78400000.r5f: assigned reserved memory node r5f-dma-memory@a2000000
    [    8.107819] remoteproc remoteproc3: 78400000.r5f is available
    [    8.142172] platform 78600000.r5f: configured R5F for remoteproc mode
    [    8.149150] remoteproc remoteproc3: powering up 78400000.r5f
    [    8.155144] remoteproc remoteproc3: Booting fw image am64-main-r5f1_0-fw, size 93260
    [    8.167801] rproc-virtio rproc-virtio.4.auto: assigned reserved memory node r5f-dma-memory@a2000000
    [    8.179599] virtio_rpmsg_bus virtio3: rpmsg host is online
    [    8.186194] rproc-virtio rproc-virtio.4.auto: registered virtio3 (type 7)
    [    8.194324] remoteproc remoteproc3: remote processor 78400000.r5f is now up
    [    8.201638] virtio_rpmsg_bus virtio3: creating channel rpmsg_chrdev addr 0xe
    [    8.228959] platform 78600000.r5f: assigned reserved memory node r5f-dma-memory@a3000000
    [    8.389430] remoteproc remoteproc4: 78600000.r5f is available
    [    8.522093] remoteproc remoteproc4: powering up 78600000.r5f
    [    8.527881] remoteproc remoteproc4: Booting fw image am64-main-r5f1_1-fw, size 91520
    [    8.543722] rproc-virtio rproc-virtio.5.auto: assigned reserved memory node r5f-dma-memory@a3000000
    [    8.557692] virtio_rpmsg_bus virtio4: rpmsg host is online
    [    8.564307] rproc-virtio rproc-virtio.5.auto: registered virtio4 (type 7)
    [    8.571282] remoteproc remoteproc4: remote processor 78600000.r5f is now up
    [    8.580943] virtio_rpmsg_bus virtio4: creating channel rpmsg_chrdev addr 0xe
    [*     ] A start job is running for Run pending postinsts (6s / no limit)
    
    [**    ] A start job is running for Run pending postinsts (7s / no limit)
    [   10.541233] remoteproc remoteproc5: 3000a000.txpru is available
    [   10.604026] remoteproc remoteproc6: 30034000.pru is available
    [   10.614199] remoteproc remoteproc7: 30004000.rtu is available
    [   10.661566] remoteproc remoteproc8: 30038000.pru is available
    [   10.713720] remoteproc remoteproc9: 30006000.rtu is available
    [   10.741624] remoteproc remoteproc10: 3000c000.txpru is available
    [   10.777643] remoteproc remoteproc11: 300b4000.pru is available
    
    [***   ] A start job is running for Run pending postinsts (7s / no limit)
    [   10.841567] remoteproc remoteproc12: 30084000.rtu is available
    [   10.891915] remoteproc remoteproc13: 3008a000.txpru is available
    [   10.917623] remoteproc remoteproc14: 300b8000.pru is available
    [   10.965328] remoteproc remoteproc15: 30086000.rtu is available
    [   10.991866] remoteproc remoteproc16: 3008c000.txpru is available
    
    [ ***  ] A start job is run[   11.344982] cfg80211: Loading compiled-in X.509 certificates for regulatory database
    ning for Run pending postinsts (8s / no limit)
    [   11.425902] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
    
    [  OK  ] Listening on Load/Save RF �itch Status /dev/rfkill Watch.
    [   11.592713] xhci-hcd xhci-hcd.6.auto: xHCI Host Controller
    [   11.662504] xhci-hcd xhci-hcd.6.auto: new USB bus registered, assigned bus number 1
    [   11.745473] xhci-hcd xhci-hcd.6.auto: hcc params 0x200073c9 hci version 0x100 quirks 0x0000002000018010
    [   11.809722] xhci-hcd xhci-hcd.6.auto: irq 519, io mem 0x0f410000
    [   11.832643] wl18xx_driver wl18xx.3.auto: Direct firmware load for ti-connectivity/wl1271-nvs.bin failed with error -2
    [   11.860386] xhci-hcd xhci-hcd.6.auto: xHCI Host Controller
    [   11.908937] xhci-hcd xhci-hcd.6.auto: new USB bus registered, assigned bus number 2
    [   11.939668] xhci-hcd xhci-hcd.6.auto: Host supports USB 3.0 SuperSpeed
    [   11.952446] hub 1-0:1.0: USB hub found
    [   11.957082] hub 1-0:1.0: 1 port detected
    [   11.971990] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
    [   11.983527] hub 2-0:1.0: USB hub found
    [   11.990056] hub 2-0:1.0: 1 port detected
    [   12.217553] wlcore: wl18xx HW: 183x or 180x, PG 2.2 (ROM 0x11)
    [   12.239917] wlcore: loaded
             Starting Load/Save RF Kill Switch Status...
    [  OK  ] Started Load/Save RF Kill Switch Status.
    [  OK  ] Created slice Slice /system/systemd-fsck.
    [  OK  ] Found device /dev/mmcblk1p1.
             Starting File System Check on /dev/mmcblk1p1...
    [  OK  ] Finished File System Check on /dev/mmcblk1p1.
             Mounting /run/media/boot-mmcblk1p1...
    [  OK  ] Mounted /run/media/boot-mmcblk1p1.
    [  *** ] A start job is running for Run pending postinsts (11s / no limit)
    
    [  OK  ] Finished Run pending postinsts.
    [  OK  ] Reached target System Initialization.
    [  OK  ] Started Daily rotation of log files.
    [  OK  ] Started Timer service to update the IP on OLED each 10s.
    [  OK  ] Started Daily Cleanup of Temporary Directories.
    [  OK  ] Reached target Timer Units.
    [  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
    [  OK  ] Listening on D-Bus System Message Bus Socket.
             Starting Docker Socket for the API...
    [  OK  ] Listening on dropbear.socket.
             Starting Weston socket...
             Starting D-Bus System Message Bus...
             Starting Reboot and dump vmcore via kexec...
    [  OK  ] Listening on Docker Socket for the API.
    [  OK  ] Listening on Weston socket.
    [  OK  ] Finished Reboot and dump vmcore via kexec.
    [  OK  ] Reached target Socket Units.
    [  OK  ] Started D-Bus System Message Bus.
    [  OK  ] Reached target Basic System.
    [  OK  ] Started Job spooling tools.
    [  OK  ] Started Periodic Command Scheduler.
             Starting Print notice about GPLv3 packages...
             Starting IPv6 Packet Filtering Framework...
             Starting IPv4 Packet Filtering Framework...
    [  OK  ] Started irqbalance daemon.
             Starting startwlanap...
             Starting startwlansta...
    [   15.909514] audit: type=1334 audit(1651167758.996:4): prog-id=7 op=LOAD
    [   15.921035] audit: type=1334 audit(1651167759.008:5): prog-id=8 op=LOAD
             Starting User Login Management...
    [  OK  ] Started TEE Supplicant.
             Starting telnetd.service...
    [  OK  ] Finished IPv6 Packet Filtering Framework.
    [  OK  ] Finished IPv4 Packet Filtering Framework.
    [  OK  ] Started startwlansta.
    [  OK  ] Started startwlanap.
    [  OK  ] Reached target Preparation for Network.
             Starting Network Configuration...
    [  OK  ] Started telnetd.service.
             Starting LSB: Expand Rootfs of boot device...
    [  OK  ] Started LSB: Expand Rootfs of boot device.
    [  OK  ] Started User Login Management.
    [  OK  ] Started Network Configuration.
             Starting Wait for Network to be Configured...
             Starting Network Name Resolution...
    [   17.177895] startwlansta.sh[480]: Wi-Fi user configuration file missing, exit
    [   17.371449] wlcore: using inverted interrupt logic: 2
    [   17.459005] wlcore: PHY firmware version: Rev 8.2.0.0.245
    [   17.572389] wlcore: firmware booted (Rev 8.9.0.0.86)
    [   17.602944] am65-cpsw-nuss 8000000.ethernet eth1: PHY [8000f00.mdio:01] driver [TI DP83867] (irq=POLL)
    [   17.612414] am65-cpsw-nuss 8000000.ethernet eth1: configuring for phy/rgmii-rxid link mode
    [   17.663726] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [TI DP83867] (irq=POLL)
    [   17.677396] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
    [  OK  ] Started Network Name Resolution.
    [  OK  ] Reached target Network.
    [  OK  ] Reached target Host and Network Name Lookups.
             Starting Avahi mDNS/DNS-SD Stack...
             Starting Enable and configure wl18xx bluetooth stack...
             Starting containerd container runtime...
    [  OK  ] Started Netperf Benchmark Server.
    [  OK  ] Started NFS status monitor for NFSv2/3 locking..
             Starting Simple Network Ma�ent Protocol (SNMP) Daemon....
             Starting Permit User Sessions...
    [  OK  ] Started Avahi mDNS/DNS-SD Stack.
    [  OK  ] Finished Enable and configure wl18xx bluetooth stack.
    [  OK  ] Finished Permit User Sessions.
    [  OK  ] Started Getty on tty1.
    [  OK  ] Started Serial Getty on ttyS2.
    [  OK  ] Reached target Login Prompts.
    [   17.929194] startwlanap.sh[547]: adding wlan1 interface
             Starting Synchronize System and HW clocks...
             Starting Weston, a Wayland�ositor, as a system service...
    [FAILED] Failed to start Synchronize System and HW clocks.
    See 'systemctl status sync-clocks.service' for details.
    [   18.412599] audit: type=1334 audit(1651167761.496:6): prog-id=9 op=LOAD
    [   18.290798] startwlanap.sh[555]: Line 499: unknown configurat[   18.425434] audit: type=1334 audit(1651167761.512:7): prog-id=10 op=LOAD
    ion item 'wep_rekey_period'
    [   18.291537] startwlanap.sh[555]: 1 errors found in configuration file '/usr/share/wl18xx/hostapd.conf'
    [   18.292548] startwlanap.sh[555]: Failed to set up interface with /usr/share/wl18xx/hostapd.conf
    [   18.293062] startwlanap.sh[555]: Failed to initialize interface
             Starting User Database Manager...
    [  OK  ] Started User Database Manager.
    [  OK  ] Created slice User Slice of UID 1000.
             Starting User Runtime Directory /run/user/1000...
    [  OK  ] Started Simple Network Man�ement Protocol (SNMP) Daemon..
    [  OK  ] Finished User Runtime Directory /run/user/1000.
             Starting User Manager for UID 1000...
    [   19.278343] audit: type=1006 audit(1651167762.364:8): pid=572 uid=0 old-auid=4294967295 auid=1000 tty=(none) old-ses=4294967295 ses=1 res=1
    [   19.302212] audit: type=1300 audit(1651167762.364:8): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=ffffc183be48 a2=4 a3=ffffb2c33020 items=0 ppid=1 pid=572 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" exe="/lib/systemd/systemd" key=(null)
    [   19.341336] audit: type=1327 audit(1651167762.364:8): proctitle="(systemd)"
    [   19.668811] audit: type=1325 audit(1651167762.732:9): table=nat family=2 entries=0 op=xt_register pid=584 comm="iptables"
    [   19.684918] audit: type=1300 audit(1651167762.732:9): arch=c00000b7 syscall=209 success=yes exit=0 a0=4 a1=0 a2=40 a3=ffffea13b078 items=0 ppid=547 pid=584 auid=4294967295 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=4294967295 comm="iptables" exe="/usr/sbin/xtables-legacy-multi" key=(null)
    [   19.723224] audit: type=1327 audit(1651167762.732:9): proctitle=69707461626C6573002D74006E6174002D4100504F5354524F5554494E47002D6F0065746830002D6A004D415351554552414445
    [  OK  ] Started User Manager for UID 1000.
    [  OK  ] Started Session c1 of User weston.
    [FAILED] Failed to start Weston, a �mpositor, as a system service.
    See 'systemctl status weston.service' for details.
    [DEPEND] Dependency failed for Matrix GUI.
    [  OK  ] Started containerd container runtime.
    [  OK  ] Finished Print notice about GPLv3 packages.
    [   22.123363] platform led-controller: deferred probe pending
    
    
     _____                    _____           _         _   
    |  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_ 
    |     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
    |__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|  
                  |___|                    |___|            
    
    Arago Project am64xx-evm -
    
    Arago 2023.04 am64xx-evm -
    
    am64xx-evm login: root
    
    [   71.965974] kauditd_printk_skb: 6 callbacks suppressed
    [   71.965993] audit: type=1006 audit(1651167815.052:12): pid=598 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=3 res=1
    [   71.984708] audit: type=1300 audit(1651167815.052:12): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=ffffc183be48 a2=1 a3=ffffb2c33020 items=0 ppid=1 pid=598 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=3 comm="(systemd)" exe="/lib/systemd/systemd" key=(null)
    [   72.012236] audit: type=1327 audit(1651167815.052:12): proctitle="(systemd)"
    [   72.020494] audit: type=1334 audit(1651167815.072:13): prog-id=11 op=LOAD
    [   72.028948] audit: type=1300 audit(1651167815.072:13): arch=c00000b7 syscall=280 success=yes exit=8 a0=5 a1=ffffdc5c66d0 a2=78 a3=0 items=0 ppid=1 pid=598 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=3 comm="systemd" exe="/lib/systemd/systemd" key=(null)
    [   72.054876] audit: type=1327 audit(1651167815.072:13): proctitle="(systemd)"
    [   72.063086] audit: type=1334 audit(1651167815.096:14): prog-id=11 op=UNLOAD
    [   72.071392] audit: type=1334 audit(1651167815.096:15): prog-id=12 op=LOAD
    [   72.079405] audit: type=1300 audit(1651167815.096:15): arch=c00000b7 syscall=280 success=yes exit=8 a0=5 a1=ffffdc5c6770 a2=78 a3=0 items=0 ppid=1 pid=598 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=3 comm="systemd" exe="/lib/systemd/systemd" key=(null)
    [   72.105518] audit: type=1327 audit(1651167815.096:15): proctitle="(systemd)"
    root@am64xx-evm:~# uname -a
    Linux am64xx-evm 6.1.33-g40c32565ca #1 SMP PREEMPT Thu Jul  6 14:17:24 UTC 2023 aarch64 aarch64 aarch64 GNU/Linux
    root@am64xx-evm:~# ls -l /dev/mmcblk*
    brw-rw---- 1 root disk 179, 0 Apr 28 17:42 /dev/mmcblk1
    brw-rw---- 1 root disk 179, 1 Apr 28 17:42 /dev/mmcblk1p1
    brw-rw---- 1 root disk 179, 2 Apr 28 17:42 /dev/mmcblk1p2
    root@am64xx-evm:~# 

  • Hi Hong:

    May you attach the AM64B SKEVM of your SW2/SW3 setting?

    BR Rio

  • If using the Kingstone 64, this booting will be stuck.

    If using another Sandisk 16G sd card, it works well.

    I will close this.

    Please check if the SD card issue is resolved on AM64!!

    I remember TI has the Jira for this issue, someone told me this is resolved.

    But, it seems not resolved on the SDK9.0 + AM64B SK EVM.

    BR Rio

  • MMC access issue is due to SK-AM64B errata ID#7
    www.ti.com/.../spruiy9
    Best,
    -Hong

  • Hi Hong:

    Sorry, I thought the new AM64B-SKEVM shall resolve the errrta ID#7.

    Okay, I will close this .

    Thanks.

    BR Rio