Part Number: TMS320C6671
Hi,
How can I change python version from python 27 to python 321 in CCS 1240?
from C:\Python27\python: No module named gitversionbuilder
to Python 321
thanks,
Chuan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320C6671
Hi,
How can I change python version from python 27 to python 321 in CCS 1240?
from C:\Python27\python: No module named gitversionbuilder
to Python 321
thanks,
Chuan
Chuan,
As this question is about CCS 12.4 and not about the processor device C6671,
moving to CCS forum - subgroup in TI.
Thanks for your patience.
Regards
Shankari G
Chuan,
How can I change python version from python 27 to python 321 in CCS 1240?
What is the context of this? Are you getting a build error for a project that uses python scripts?
Thanks
ki
Again, what is the context?
CCS itself does not have direct dependencies on python. There may be some utilities in CCS that does however. And many example projects have dependencies on Python.
Hence why it would be good if you can explain exactly what your scenario is with python and CCS.
do you have the example code?
I suggest try an existing SDK for your device.
For example: https://www.ti.com/tool/PROCESSOR-SDK-C667X
Chuan,
The latest processor SDK for C6671 is " PROCESSOR-SDK-RTOS-C667X — RTOS Processor SDK for C667X" - version 6.3.
There are approximately " 56 " PDK examples in it.
But none of them uses/depends on python.
I think, your customized software uses python. If it is not, point us the particular example among the list which I have provided in the above link.
Regards
Shankari G