This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62A-LP: How to set the opt mode in MCAN communication of MCU sides of AM62A7 soc

Part Number: SK-AM62A-LP
Other Parts Discussed in Thread: AM62A7

I've a question about how to set the opt mode in MCAN communication of MCU sides of AM62A7 soc. As well as we can see in the demo code "mcan_loopback_interrupt_am62ax-sk_mcu-r5fss0-0_nortos_ti-arm-clang", there're some opt mode to switch in the initial configuration as below:

int main()----->mcan_loopback_interrupt_main(NULL)----->App_mcanConfig(TRUE)

Firstly set the mode "MCAN_OPERATION_MODE_SW_INIT" in the API function "App_mcanConfig()"


Then set the MCAN_LPBK_MODE_INTERNAL mode enable status:

At last,set the mode "MCAN_OPERATION_MODE_NORMAL":

This is just the inernal loopback demo code, which is related closely to the mode configuration in the CANFD communication. My question is how to set the opt mode in MCAN communication of MCU sides if I could get the TX/RX signals or data in the CCS env. What's the mode configured process about it if am62a7 communicated with our ZLG tools or CANoe(VN1640) tools?

  • Hi Django,
    Thanks for your query!

    With reference to AM64x external loopback TX/RX example, you can pass False into App_mcanConfig() function here, so that external loopback method is enabled.

     

    Please give this a try on your setup and let us know.

    Regards,
    Aparna