This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
SDK: ti-processor-sdk-rtos-j721s2-evm-08_06_01_03.tar.gz and ti-processor-sdk-linux-j721s2-evm-08_06_01_02-Linux-x86-Install.bin
I'm working with a custom TDA4AL board that doesn't have a display port. Following guidance from [this link], I removed DSS_EDP in vision_apps/platform/j721s2/rtos/common/app_cfg_mcu2_0.h
#define ENABLE_CSI2RX #define ENABLE_CSI2TX //#undef ENABLE_CSI2TX /* IMPORANT NOTE: * - Only one of ENABLE_DSS_SINGLE or ENABLE_DSS_DUAL should be defined * - When ENABLE_DSS_SINGLE is defined, only one of ENABLE_DSS_HDMI or ENABLE_DSS_EDP should be defined * - When ENABLE_DSS_DUAL is defined, ENABLE_DSS_HDMI and ENABLE_DSS_EDP are not used, both EDP and HDMI ar\ e enabled unconditionally */ //Brandon for TDA4AL variant //#define ENABLE_DSS_SINGLE #undef ENABLE_DSS_SINGLE #undef ENABLE_DSS_DUAL /* define below to enable eDP display, make sure to undef ENABLE_DSS_HDMI & ENABLE_DSS_DSI as well */ //Brandon for TDA4AL variant //#define ENABLE_DSS_EDP #undef ENABLE_DSS_EDP /* define below to enable HDMI display, make sure to undef ENABLE_DSS_EDP & ENABLE_DSS_DSI as well */ #undef ENABLE_DSS_HDMI /* define below to enable DSI display, make sure to undef ENABLE_DSS_HDMI & ENABLE_DSS_EDP as well */ //#define ENABLE_DSS_DSI #undef ENABLE_DSS_DSI #define ENABLE_I2C #define ENABLE_BOARD
vision_apps log:
root@j721s2-evm:~# cd /opt/vision_apps/ root@j721s2-evm:/opt/vision_apps# source ./vision_apps_init.sh root@j721s2-evm:/opt/vision_apps# [MCU2_0] 3.815092 s: CIO: Init ... Done !!! [MCU2_0] 3.815143 s: ### CPU Frequency = 1000000000 Hz [MCU2_0] 3.815175 s: CPU is running FreeRTOS [MCU2_0] 3.815197 s: APP: Init ... !!! [MCU2_0] 3.815217 s: SCICLIENT: Init ... !!! [MCU2_0] 3.815353 s: SCICLIENT: DMSC FW version [8.6.3--1-g2249f (Chill Capybara] [MCU2_0] 3.815387 s: SCICLIENT: DMSC FW revision 0x8 [MCU2_0] 3.815417 s: SCICLIENT: DMSC FW ABI revision 3.1 [MCU2_0] 3.815449 s: SCICLIENT: Init ... Done !!! [MCU2_0] 3.815472 s: UDMA: Init ... !!! [MCU2_0] 3.816359 s: UDMA: Init ... Done !!! [MCU2_0] 3.816394 s: UDMA: Init ... !!! [MCU2_0] 3.816904 s: UDMA: Init for CSITX/CSIRX ... Done !!! [MCU2_0] 3.816959 s: MEM: Init ... !!! [MCU2_0] 3.816995 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ d9000000 of size 16777216 bytes !!! [MCU2_0] 3.817053 s: MEM: Created heap (L3_MEM, id=1, flags=0x00000000) @ 60000000 of size 524288 bytes !!! [MCU2_0] 3.817107 s: MEM: Init ... Done !!! [MCU2_0] 3.817128 s: IPC: Init ... !!! [MCU2_0] 3.817174 s: IPC: 5 CPUs participating in IPC !!! [MCU2_0] 3.817209 s: IPC: Waiting for HLOS to be ready ... !!! [MCU2_0] 11.818333 s: IPC: HLOS is ready !!! [MCU2_0] 11.827654 s: IPC: Init ... Done !!! [MCU2_0] 11.827696 s: APP: Syncing with 4 CPUs ... !!! [MCU2_0] 12.249918 s: APP: Syncing with 4 CPUs ... Done !!! [MCU2_0] 12.249952 s: REMOTE_SERVICE: Init ... !!! [MCU2_0] 12.251215 s: REMOTE_SERVICE: Init ... Done !!! [MCU2_0] 12.251258 s: FVID2: Init ... !!! [MCU2_0] 12.251315 s: FVID2: Init ... Done !!! [MCU2_0] 12.251381 s: SCICLIENT: Sciclient_pmSetModuleState module=214 state=2 [MCU2_0] 12.251588 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 12.251625 s: VHWA: VPAC Init ... !!! [MCU2_0] 12.251647 s: SCICLIENT: Sciclient_pmSetModuleState module=361 state=2 [MCU2_0] 12.251782 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 12.251810 s: VHWA: LDC Init ... !!! [MCU2_0] 12.254647 s: VHWA: LDC Init ... Done !!! [MCU2_0] 12.254687 s: VHWA: MSC Init ... !!! [MCU2_0] 12.263780 s: VHWA: MSC Init ... Done !!! [MCU2_0] 12.263819 s: VHWA: NF Init ... !!! [MCU2_0] 12.264797 s: VHWA: NF Init ... Done !!! [MCU2_0] 12.264831 s: VHWA: VISS Init ... !!! [MCU2_0] 12.271875 s: VHWA: VISS Init ... Done !!! [MCU2_0] 12.271919 s: VHWA: VPAC Init ... Done !!! [MCU2_0] 12.271955 s: VX_ZONE_INIT:Enabled [MCU2_0] 12.271982 s: VX_ZONE_ERROR:Enabled [MCU2_0] 12.272007 s: VX_ZONE_WARNING:Enabled [MCU2_0] 12.272870 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target MCU2-0 [MCU2_0] 12.273054 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target VPAC_NF [MCU2_0] 12.273228 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target VPAC_LDC1 [MCU2_0] 12.273396 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target VPAC_MSC1 [MCU2_0] 12.273566 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target VPAC_MSC2 [MCU2_0] 12.273791 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target VPAC_VISS1 [MCU2_0] 12.273977 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target CAPTURE1 [MCU2_0] 12.274152 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target CAPTURE2 [MCU2_0] 12.274327 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target DISPLAY1 [MCU2_0] 12.274496 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target DISPLAY2 [MCU2_0] 12.274662 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target CSITX [MCU2_0] 12.274850 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target CAPTURE3 [MCU2_0] 12.275034 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target CAPTURE4 [MCU2_0] 12.275222 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target CAPTURE5 [MCU2_0] 12.275405 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target CAPTURE6 [MCU2_0] 12.275585 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target CAPTURE7 [MCU2_0] 12.275758 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target CAPTURE8 [MCU2_0] 12.275918 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target DSS_M2M1 [MCU2_0] 12.276081 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target DSS_M2M2 [MCU2_0] 12.276256 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target DSS_M2M3 [MCU2_0] 12.276435 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target DSS_M2M4 [MCU2_0] 12.276601 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target CSITX2 [MCU2_0] 12.276646 s: VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!! [MCU2_0] 12.276677 s: APP: OpenVX Target kernel init ... !!! [MCU2_0] 12.302743 s: APP: OpenVX Target kernel init ... Done !!! [MCU2_0] 12.302777 s: CSI2RX: Init ... !!! [MCU2_0] 12.302798 s: SCICLIENT: Sciclient_pmSetModuleState module=136 state=2 [MCU2_0] 12.302894 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 12.302924 s: SCICLIENT: Sciclient_pmSetModuleState module=38 state=2 [MCU2_0] 12.303031 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 12.303057 s: SCICLIENT: Sciclient_pmSetModuleState module=39 state=2 [MCU2_0] 12.303139 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 12.303166 s: SCICLIENT: Sciclient_pmSetModuleState module=152 state=2 [MCU2_0] 12.303227 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 12.303254 s: SCICLIENT: Sciclient_pmSetModuleState module=153 state=2 [MCU2_0] 12.303311 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 12.303492 s: CSI2RX: Init ... Done !!! [MCU2_0] 12.303518 s: CSI2TX: Init ... !!! [MCU2_0] 12.303539 s: SCICLIENT: Sciclient_pmSetModuleState module=136 state=2 [MCU2_0] 12.303597 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 12.303624 s: SCICLIENT: Sciclient_pmSetModuleState module=40 state=2 [MCU2_0] 12.303706 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 12.303732 s: SCICLIENT: Sciclient_pmSetModuleState module=41 state=2 [MCU2_0] 12.303809 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 12.303837 s: SCICLIENT: Sciclient_pmSetModuleState module=363 state=2 [MCU2_0] 12.303899 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_0] 12.303963 s: CSI2TX: Init ... Done !!! [MCU2_0] 12.303989 s: ISS: Init ... !!! [MCU2_0] 12.304042 s: Found sensor IMX390-UB953_D3 at location 0 [MCU2_0] 12.304086 s: Found sensor AR0233-UB953_MARS at location 1 [MCU2_0] 12.304128 s: Found sensor AR0820-UB953_LI at location 2 [MCU2_0] 12.304170 s: Found sensor UB9xxx_RAW12_TESTPATTERN at location 3 [MCU2_0] 12.304206 s: AA55 IssSensor_OX03C_MAX9295_Init [MCU2_0] 12.304244 s: Found sensor OX03C-MAX9295E at location 4 [MCU2_0] 12.304273 s: IssSensor_OX03C_Init AA55 [MCU2_0] 12.304312 s: Found sensor MAX96712_RAW_TESTPAT at location 5 [MCU2_0] 12.304348 s: AA55 IssSensor_AR0233_MAX9295_Init [MCU2_0] 12.304385 s: Found sensor AR0233-MAX9295E at location 6 [MCU2_0] 12.304413 s: IssSensor_AR0233_Init AA55 [MCU2_0] 12.304451 s: Found sensor UB96x_UYVY_TESTPATTERN at location 7 [MCU2_0] 12.304492 s: Found sensor GW_AR0233_UYVY at location 8 [MCU2_0] 12.304517 s: IssSensor_Init ... Done !!! [MCU2_0] 12.304575 s: IttRemoteServer_Init ... Done !!! [MCU2_0] 12.304603 s: VISS REMOTE SERVICE: Init ... !!! [MCU2_0] 12.304654 s: VISS REMOTE SERVICE: Init ... Done !!! [MCU2_0] 12.304681 s: UDMA Copy: Init ... !!! [MCU2_0] 12.305735 s: UDMA Copy: Init ... Done !!! [MCU2_0] 12.305806 s: APP: Init ... Done !!! [MCU2_0] 12.305832 s: APP: Run ... !!! [MCU2_0] 12.305852 s: IPC: Starting echo test ... [MCU2_0] 12.307930 s: APP: Run ... Done !!! [MCU2_0] 12.308653 s: IPC: Echo status: mpu1_0[x] mcu2_0[s] mcu2_1[.] C7X_1[P] C7X_2[.] [MCU2_0] 12.308734 s: IPC: Echo status: mpu1_0[x] mcu2_0[s] mcu2_1[.] C7X_1[P] C7X_2[P] [MCU2_0] 12.308801 s: IPC: Echo status: mpu1_0[x] mcu2_0[s] mcu2_1[P] C7X_1[P] C7X_2[P] [MCU2_1] 3.806113 s: CIO: Init ... Done !!! [MCU2_1] 3.806165 s: ### CPU Frequency = 1000000000 Hz [MCU2_1] 3.806195 s: CPU is running FreeRTOS [MCU2_1] 3.806216 s: APP: Init ... !!! [MCU2_1] 3.806235 s: SCICLIENT: Init ... !!! [MCU2_1] 3.806366 s: SCICLIENT: DMSC FW version [8.6.3--1-g2249f (Chill Capybara] [MCU2_1] 3.806401 s: SCICLIENT: DMSC FW revision 0x8 [MCU2_1] 3.806427 s: SCICLIENT: DMSC FW ABI revision 3.1 [MCU2_1] 3.806457 s: SCICLIENT: Init ... Done !!! [MCU2_1] 3.806479 s: UDMA: Init ... !!! [MCU2_1] 3.807523 s: UDMA: Init ... Done !!! [MCU2_1] 3.807581 s: MEM: Init ... !!! [MCU2_1] 3.807614 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ da000000 of size 16777216 bytes !!! [MCU2_1] 3.807671 s: MEM: Created heap (L3_MEM, id=1, flags=0x00000001) @ 60080000 of size 524288 bytes !!! [MCU2_1] 3.807728 s: MEM: Init ... Done !!! [MCU2_1] 3.807750 s: IPC: Init ... !!! [MCU2_1] 3.807797 s: IPC: 5 CPUs participating in IPC !!! [MCU2_1] 3.807831 s: IPC: Waiting for HLOS to be ready ... !!! [MCU2_1] 12.240579 s: IPC: HLOS is ready !!! [MCU2_1] 12.249845 s: IPC: Init ... Done !!! [MCU2_1] 12.249884 s: APP: Syncing with 4 CPUs ... !!! [MCU2_1] 12.249917 s: APP: Syncing with 4 CPUs ... Done !!! [MCU2_1] 12.249945 s: REMOTE_SERVICE: Init ... !!! [MCU2_1] 12.251238 s: REMOTE_SERVICE: Init ... Done !!! [MCU2_1] 12.251275 s: FVID2: Init ... !!! [MCU2_1] 12.251326 s: FVID2: Init ... Done !!! [MCU2_1] 12.251389 s: VHWA: DMPAC: Init ... !!! [MCU2_1] 12.251411 s: SCICLIENT: Sciclient_pmSetModuleState module=58 state=2 [MCU2_1] 12.251649 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_1] 12.251678 s: SCICLIENT: Sciclient_pmSetModuleState module=62 state=2 [MCU2_1] 12.251807 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU2_1] 12.251833 s: VHWA: DOF Init ... !!! [MCU2_1] 12.256312 s: VHWA: DOF Init ... Done !!! [MCU2_1] 12.256351 s: VHWA: SDE Init ... !!! [MCU2_1] 12.258032 s: VHWA: SDE Init ... Done !!! [MCU2_1] 12.258066 s: VHWA: DMPAC: Init ... Done !!! [MCU2_1] 12.258101 s: VX_ZONE_INIT:Enabled [MCU2_1] 12.258124 s: VX_ZONE_ERROR:Enabled [MCU2_1] 12.258146 s: VX_ZONE_WARNING:Enabled [MCU2_1] 12.259018 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target MCU2-1 [MCU2_1] 12.259189 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target DMPAC_SDE [MCU2_1] 12.259356 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target DMPAC_DOF [MCU2_1] 12.259396 s: VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!! [MCU2_1] 12.259424 s: APP: OpenVX Target kernel init ... !!! [MCU2_1] 12.259646 s: APP: OpenVX Target kernel init ... Done !!! [MCU2_1] 12.259674 s: UDMA Copy: Init ... !!! [MCU2_1] 12.261184 s: UDMA Copy: Init ... Done !!! [MCU2_1] 12.261230 s: APP: Init ... Done !!! [MCU2_1] 12.261254 s: APP: Run ... !!! [MCU2_1] 12.261274 s: IPC: Starting echo test ... [MCU2_1] 12.263341 s: APP: Run ... Done !!! [MCU2_1] 12.263960 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[s] C7X_1[P] C7X_2[.] [MCU2_1] 12.264036 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[s] C7X_1[P] C7X_2[P] [MCU2_1] 12.308569 s: IPC: Echo status: mpu1_0[x] mcu2_0[P] mcu2_1[s] C7X_1[P] C7X_2[P] [C7x_1 ] 4.122181 s: CIO: Init ... Done !!! [C7x_1 ] 4.122196 s: ### CPU Frequency = 1000000000 Hz [C7x_1 ] 4.122208 s: CPU is running FreeRTOS [C7x_1 ] 4.122217 s: APP: Init ... !!! [C7x_1 ] 4.122224 s: SCICLIENT: Init ... !!! [C7x_1 ] 4.122335 s: SCICLIENT: DMSC FW version [8.6.3--1-g2249f (Chill Capybara] [C7x_1 ] 4.122350 s: SCICLIENT: DMSC FW revision 0x8 [C7x_1 ] 4.122360 s: SCICLIENT: DMSC FW ABI revision 3.1 [C7x_1 ] 4.122372 s: SCICLIENT: Init ... Done !!! [C7x_1 ] 4.122381 s: UDMA: Init ... !!! [C7x_1 ] 4.123248 s: UDMA: Init ... Done !!! [C7x_1 ] 4.123261 s: MEM: Init ... !!! [C7x_1 ] 4.123273 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ 117000000 of size 268435456 bytes !!! [C7x_1 ] 4.123294 s: MEM: Created heap (L3_MEM, id=1, flags=0x00000001) @ 70020000 of size 3964928 bytes !!! [C7x_1 ] 4.123312 s: MEM: Created heap (L2_MEM, id=2, flags=0x00000001) @ 64800000 of size 458752 bytes !!! [C7x_1 ] 4.123330 s: MEM: Created heap (L1_MEM, id=3, flags=0x00000001) @ 64e00000 of size 16384 bytes !!! [C7x_1 ] 4.123348 s: MEM: Created heap (DDR_SCRATCH_MEM, id=4, flags=0x00000001) @ 100000000 of size 385875968 bytes !!! [C7x_1 ] 4.123367 s: MEM: Init ... Done !!! [C7x_1 ] 4.123375 s: IPC: Init ... !!! [C7x_1 ] 4.123389 s: IPC: 5 CPUs participating in IPC !!! [C7x_1 ] 4.123403 s: IPC: Waiting for HLOS to be ready ... !!! [C7x_1 ] 11.053768 s: IPC: HLOS is ready !!! [C7x_1 ] 11.055593 s: IPC: Init ... Done !!! [C7x_1 ] 11.055607 s: APP: Syncing with 4 CPUs ... !!! [C7x_1 ] 12.249918 s: APP: Syncing with 4 CPUs ... Done !!! [C7x_1 ] 12.249936 s: REMOTE_SERVICE: Init ... !!! [C7x_1 ] 12.250107 s: REMOTE_SERVICE: Init ... Done !!! [C7x_1 ] 12.250159 s: VX_ZONE_INIT:Enabled [C7x_1 ] 12.250172 s: VX_ZONE_ERROR:Enabled [C7x_1 ] 12.250183 s: VX_ZONE_WARNING:Enabled [C7x_1 ] 12.250410 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1 [C7x_1 ] 12.250477 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_2 [C7x_1 ] 12.250542 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_3 [C7x_1 ] 12.250610 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_4 [C7x_1 ] 12.250677 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_5 [C7x_1 ] 12.250750 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_6 [C7x_1 ] 12.250817 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_7 [C7x_1 ] 12.250885 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_8 [C7x_1 ] 12.250909 s: VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!! [C7x_1 ] 12.250924 s: APP: OpenVX Target kernel init ... !!! [C7x_1 ] 12.251097 s: APP: OpenVX Target kernel init ... Done !!! [C7x_1 ] 12.251111 s: APP: Init ... Done !!! [C7x_1 ] 12.251120 s: APP: Run ... !!! [C7x_1 ] 12.251128 s: IPC: Starting echo test ... [C7x_1 ] 12.251265 s: APP: Run ... Done !!! [C7x_1 ] 12.252492 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] C7X_1[s] C7X_2[P] [C7x_1 ] 12.263849 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[P] C7X_1[s] C7X_2[P] [C7x_1 ] 12.308513 s: IPC: Echo status: mpu1_0[x] mcu2_0[P] mcu2_1[P] C7X_1[s] C7X_2[P] [C7x_2 ] 4.344116 s: CIO: Init ... Done !!! [C7x_2 ] 4.344132 s: ### CPU Frequency = 1000000000 Hz [C7x_2 ] 4.344145 s: CPU is running FreeRTOS [C7x_2 ] 4.344154 s: APP: Init ... !!! [C7x_2 ] 4.344163 s: SCICLIENT: Init ... !!! [C7x_2 ] 4.344274 s: SCICLIENT: DMSC FW version [8.6.3--1-g2249f (Chill Capybara] [C7x_2 ] 4.344289 s: SCICLIENT: DMSC FW revision 0x8 [C7x_2 ] 4.344300 s: SCICLIENT: DMSC FW ABI revision 3.1 [C7x_2 ] 4.344311 s: SCICLIENT: Init ... Done !!! [C7x_2 ] 4.344321 s: UDMA: Init ... !!! [C7x_2 ] 4.345195 s: UDMA: Init ... Done !!! [C7x_2 ] 4.345209 s: MEM: Init ... !!! [C7x_2 ] 4.345222 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ 127000000 of size 16777216 bytes !!! [C7x_2 ] 4.345243 s: MEM: Created heap (L2_MEM, id=2, flags=0x00000001) @ 65800000 of size 458752 bytes !!! [C7x_2 ] 4.345261 s: MEM: Created heap (L1_MEM, id=3, flags=0x00000001) @ 65e00000 of size 16384 bytes !!! [C7x_2 ] 4.345279 s: MEM: Created heap (DDR_SCRATCH_MEM, id=4, flags=0x00000001) @ 128000000 of size 67108864 bytes !!! [C7x_2 ] 4.345298 s: MEM: Init ... Done !!! [C7x_2 ] 4.345307 s: IPC: Init ... !!! [C7x_2 ] 4.345322 s: IPC: 5 CPUs participating in IPC !!! [C7x_2 ] 4.345336 s: IPC: Waiting for HLOS to be ready ... !!! [C7x_2 ] 11.279219 s: IPC: HLOS is ready !!! [C7x_2 ] 11.281040 s: IPC: Init ... Done !!! [C7x_2 ] 11.281055 s: APP: Syncing with 4 CPUs ... !!! [C7x_2 ] 12.249919 s: APP: Syncing with 4 CPUs ... Done !!! [C7x_2 ] 12.249937 s: REMOTE_SERVICE: Init ... !!! [C7x_2 ] 12.250110 s: REMOTE_SERVICE: Init ... Done !!! [C7x_2 ] 12.250133 s: VX_ZONE_INIT:Enabled [C7x_2 ] 12.250173 s: VX_ZONE_ERROR:Enabled [C7x_2 ] 12.250186 s: VX_ZONE_WARNING:Enabled [C7x_2 ] 12.250753 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP-1 [C7x_2 ] 12.250776 s: VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!! [C7x_2 ] 12.250790 s: APP: OpenVX Target kernel init ... !!! [C7x_2 ] 12.251108 s: APP: OpenVX Target kernel init ... Done !!! [C7x_2 ] 12.251123 s: UDMA Copy: Init ... !!! [C7x_2 ] 12.252024 s: UDMA Copy: Init ... Done !!! [C7x_2 ] 12.252040 s: APP: Init ... Done !!! [C7x_2 ] 12.252050 s: APP: Run ... !!! [C7x_2 ] 12.252059 s: IPC: Starting echo test ... [C7x_2 ] 12.252202 s: APP: Run ... Done !!! [C7x_2 ] 12.252500 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[x] C7X_1[P] C7X_2[s] [C7x_2 ] 12.263866 s: IPC: Echo status: mpu1_0[x] mcu2_0[x] mcu2_1[P] C7X_1[P] C7X_2[s] [C7x_2 ] 12.308536 s: IPC: Echo status: mpu1_0[x] mcu2_0[P] mcu2_1[P] C7X_1[P] C7X_2[s]
Now, I'm encountering errors when running vision apps,
[MCU2_0] 483.499744 s: VX_ZONE_WARNING:[tivxVpacVissCreate:377] VISS H3A output is not generated due to DCC not being enabled [MCU2_0] 483.505670 s: VX_ZONE_WARNING:[tivxAewbCreate:1074] No DCC buffer passed. Disabling 2A [MCU2_0] 483.510551 s: VX_ZONE_ERROR:[ownTargetKernelInstanceAlloc:116] kernel com.ti.hwa.display has not been registered on this CPU [MCU2_0] 483.510610 s: VX_ZONE_ERROR:[ownTargetKernelInstanceAlloc:117] Please register this kernel on the appropriate target core [MCU2_0] 483.510664 s: VX_ZONE_ERROR:[ownTargetNodeDescNodeCreate:761] target_kernel_instance is NULL [MCU2_0] 483.816610 s: ========================================================== [MCU2_0] 483.816670 s: Capture Status: Instance|0 [MCU2_0] 483.816705 s: ========================================================== [MCU2_0] 483.816745 s: overflowCount: 0 [MCU2_0] 483.816777 s: spuriousUdmaIntrCount: 0 [MCU2_0] 483.816809 s: frontFIFOOvflCount: 0 [MCU2_0] 483.816838 s: crcCount: 0 [MCU2_0] 483.816864 s: eccCount: 0 [MCU2_0] 483.816893 s: correctedEccCount: 0 [MCU2_0] 483.816921 s: dataIdErrorCount: 0 [MCU2_0] 483.816951 s: invalidAccessCount: 0 [MCU2_0] 483.816980 s: invalidSpCount: 0 [MCU2_0] 483.817014 s: strmFIFOOvflCount[0]: 0 [MCU2_0] 483.817049 s: strmFIFOOvflCount[1]: 0 [MCU2_0] 483.817074 s: Channel Num | Frame Queue Count | Frame De-queue Count | Frame Drop Count | Error Frame Count | [MCU2_0] 483.817139 s: 0 | 0 | 0 | 0 | 0 | [MCU2_0] 483.817498 s: ========================================================== [MCU2_0] 483.817556 s: Capture Status: Instance|1 [MCU2_0] 483.817583 s: ========================================================== [MCU2_0] 483.817621 s: overflowCount: 0 [MCU2_0] 483.817651 s: spuriousUdmaIntrCount: 0 [MCU2_0] 483.817682 s: frontFIFOOvflCount: 0 [MCU2_0] 483.817720 s: crcCount: 0 [MCU2_0] 483.817746 s: eccCount: 0 [MCU2_0] 483.817774 s: correctedEccCount: 0 [MCU2_0] 483.817803 s: dataIdErrorCount: 0 [MCU2_0] 483.817833 s: invalidAccessCount: 0 [MCU2_0] 483.817862 s: invalidSpCount: 0 [MCU2_0] 483.817896 s: strmFIFOOvflCount[0]: 0 [MCU2_0] 483.817930 s: strmFIFOOvflCount[1]: 0
My primary goal is capturing raw images.
Could anyone suggest a workaround or solution to run the program successfully?
Best,
Brandon
Hi Brandon,
But which example are you running? Have you removed usage of display node from this node? Since you have removed DSS from vision apps, you would also have to remove display node from this example. Most of the examples use display node for showing the output. So this needs to be removed, otherwise, display node create will fails, as display is removed from R5F.
Regards,
Brijesh
Hi Brijesh,
We are using ./run_app_single_cam.sh
for testing. Could you please provide guidance on how to remove the display node? Do you have any example code or steps to share?
Thank you,
Brandon
Hi Brandon,
Can you please check the single camera example and remove usage of display node from it?
You can find this example in vision_apps\apps\basic_demos\app_single_cam\ folder.
Regards,
Brijesh